Arrow Electronic Components Online

The heart of modern diagnostics: unpacking in vitro diagnostics technology and its benefits

Medical & Healthcare25 Apr 2025
A scientist in a white lab coat closely observes a sample through a microscope in a modern laboratory setting. The workspace features a computer monitor displaying data, laboratory glassware, and scientific equipment.
View all articles

In vitro diagnostic (IVD) devices execute precise analyses of biological samples - such as blood, urine, and tissue - to enable health care professionals (HCPs) with critical insights into disease detection, monitoring, and treatment. 

These devices operate externally to the human body, integrating sophisticated biosensors that detect molecular interactions with high specificity, which helps HCPs with sample analysis. Additionally, advanced signal processing units convert biochemical signals into quantifiable data, leveraging noise reduction and analog-to-digital converters (ADCs) for enhanced accuracy. Artificial intelligence (AI)-driven analytics process large datasets to identify biomarkers, detect anomalies, and provide predictive insights, which support HCPs with their clinical decisions. Modular microfluidic systems automate sample preparation and reagent delivery, ensuring precision and reproducibility to reduce human errors. Robust power management and medical-grade connectivity enable uninterrupted operation and secure data transmission of electronic health records to meet the evolving cybersecurity regulations in health care. These compact systems reduce diagnostic turnaround times, enhance workflow efficiency, and facilitate global access to personalized medicine. These features make them indispensable tools in clinical and decentralized health care settings.

Key Features

  • Rapid and accurate diagnostics

  • High sensitivity multiplex testing

  • Al-driver analytics

  • User-centric design

  • Integrated connectivity

A visual diagram categorizes various IVD devices into eight main types, including genetic testing, blood testing, clinical chemistry, cancer diagnostics, specialized devices, molecular diagnostics, immunoassay systems, and fertility testing. Each category lists specific device examples. The central graphic uses color-coded boxes and icons for clarity.

Examples of various IVD devices

Figure 1

System Block Diagram

The system architecture of an IVD device consists of several integrated modules that work together seamlessly to deliver reliable and accurate diagnostic results. Each module plays a critical role in ensuring the system’s overall functionality, performance, and precision. Below is a detailed explanation of the primary components in the system block diagram for a generalized IVD device, along with an example block diagram of an image-processing device.

  1. Sample Preparation Unit

  2. Biosensor Array

  3. Signal-Processing Module

  4. Data Analysis Engine (AI/Machine Learning (ML) Algorithms)

  5. User Interface (Display/Touchscreen)

  6. Power Management System

  7. Communication Interface (Wi-Fi/ Bluetooth)

  8. Data Storage Module

  9. Quality Control and Calibration Module

a detailed block diagram of a laboratory instrument system, illustrating the integration of hardware and software components. The diagram includes modules for power management, touchscreen display, barcode scanning, image processing, and sample handling.

System block diagram of an image-based IVD analyzer

Figure 2

Sample Preparation Unit

The user prepares the biological or chemical sample, often involving staining, reagent addition, or washing. The sample is then loaded into the analyzer’s cartridge. The microfluidic-based sample preparation unit is designed to automate essential tasks such as mixing reagents, separating components, and preparing samples. With the aid of precise actuators — including motors, pumps, and heaters — this unit handles liquids with great precision under controlled conditions. To efficiently manage small sample volumes, the unit incorporates microfluidic channels and chambers, ensuring optimal preparation for subsequent analysis.

Biosensor Array

The biosensor array is a central feature of the diagnostic system, housing multiple sensor technologies to detect and measure biochemical interactions. An imageprocessing camera sensor captures highresolution images of biological samples, which are essential for diagnostics that rely on morphological analysis. These images are processed in real time by the GPU. Electrochemical sensors are employed to monitor ionic or molecular interactions, while optical sensors capable of fluorescence, absorbance, or chemiluminescence detection offer versatile means of analyzing samples. Additionally, immunoassay-based sensors are used to identify specific antigens or antibodies. The sensors work in unison to convert biochemical reactions into measurable electrical, optical, or mechanical signals, forming the foundation for precise diagnostic interpretation.

Signal-Processing Module

After the sensors detect signals, the signal-processing module amplifies, filters, and digitizes these inputs to ensure they are accurately quantified. Using ADCs, this module ensures the precision of the signal readings. In addition, specialized noise reduction circuits are implemented to improve the clarity and fidelity of the data, mitigating any distortions that could compromise the accuracy of the diagnostic results. In the case of image-processing-based IVDs, the light source (LED, laser, or halogen lamp) illuminates the sample and the detector. The detectors can include charge coupled devices (CCDs) or complementary metal-oxide semiconductor (CMOS) sensors, which capture the image across an area. This captured data undergoes preprocessing to enhance quality, removing noise or artifacts. Images are then segmented to identify regions of interest.

Data Analysis Engine (AI/ML Algorithms)

The data analysis engine is equipped with advanced AI and ML algorithms that process and interpret the sensor data. These algorithms can recognize complex patterns, diagnose conditions, and identify any anomalies that may require further investigation. The system continuously refines its diagnostic models through cloudbased learning systems, which helps improve the accuracy of predictions and decision-making over time. This real-time and evolving process improves the support for HCPs.

User Interface (Display/Touchscreen)

The user interface serves as the point of interaction between the diagnostic device and its operator. Featuring a touch-screen display, it provides a graphical user interface (GUI) that allows users to select tests, monitor progress, and visualize results in a user-friendly format. The interface supports multiple languages and can be customized to fit specific workflows, enhancing the convenience and accessibility of the device for diverse user needs.

A laboratory technician wearing blue gloves handles a blood sample vial in a clinical setting. The technician is seated at a workstation with a modern hematology analyzer displaying data on its screen.

Power Management System

To ensure seamless and reliable operation, the power management system regulates the device’s power supply, whether from an AC source or battery. It is equipped with medical-grade transformers, voltage regulators, and backup systems to maintain continuous functionality. This system is optimized for low power consumption, especially when supporting portable device designs. It is also critical that the device remains operational for extended periods without interruption.

Communication Interface (Wi-Fi/Bluetooth)

The communication interface allows the device to connect with external systems and networks via wireless technologies such as Wi-Fi, Bluetooth, or near field communication (NFC). This connectivity ensures secure data transmission to electronic health records (EHR) systems or remote devices. Furthermore, the integration with cloud platforms facilitates remote diagnostics and telemedicine applications, enabling HCPs to monitor and manage patient data from a distance.

Data Storage Module

The data storage module is responsible for securely storing test results and patient information. This module supports both local storage options, such as flash memory, and cloud synchronization for efficient data management. Adherence to regulatory standards for medical data handling, such as HIPAA and GDPR, ensures that patient confidentiality is maintained, and the device operates within the boundaries of industry requirements.

Quality Control and Calibration Module

To ensure the reliability and accuracy of the device over time, the quality control and calibration module monitors the performance of the system through regular internal checks. It includes reference standards and control samples that validate the device’s testing capabilities. Automated calibration routines are incorporated to maintain the accuracy and consistency of results, guaranteeing the long-term performance of the device in diverse diagnostic scenarios. Each of these components plays an integral role in the functioning of an IVD device, ensuring that the device delivers accurate, reliable, and timely results for HCPs and patients alike. Below please find component recommendations that you should find useful. You can connect with our engineering support team via the contact box. We also have local field application engineers who can support your designs.

Download a complimentary copy of the In Vitro Diagnostics application brief by clicking below.

In Vitro Diagnostics Design Support

Please fill out the form below and an Arrow representative will reach out to support you with your design as soon as possible.

By submitting this form, you acknowledge that use of arrow.com is subject to Arrow’s Terms of Use and Privacy Policy.

Resources

 ProductsRelated Datasheets
BLE Module  
Microchip
STMicroelectronics
Silicon Labs
Fanstel
Wi-Fi Module  
Silicon Labs
Qualcomm
  • N/A
Murata
Memory  
Microchip
Micron
Infineon
USB Type-C Connectors  
Molex
Amphenol
onsemi
Display  
Displaytech
DFRobot
Phoenix Contact
Matrix Orbital
4D Systems
Advantech
Camera Module  
Sony
Omnivision
Leopard Imaging
Lantronix
onsemi
Input Protection  
Littelfuse
Antenna  
TE Connectivity
Motors  
DFRobot
Sanyo Denki
NMB Technologies Corporation
Motor Drivers & Sensors  
Melexis
Infineon
NXP Semiconductors
ams OSRAM
STMicroelectronics
onsemi
Honeywell
SOC/MCU  
NXP Semiconductors
Alif Semiconductor
Intel
eInfochips
STMicroelectronics
AC-DC Converter  
onsemi
Infineon
NXP Semiconductors
DC-DC Power IC  
Microchip
STMicroelectronics
onsemi

For more information conteact: EngineeringSupport@arrow.com

Connect with us

eInfochips, an Arrow Electronics company, is a leading engineering service provider for end-to-end medical product/software development life cycle (PDLC/ SDLC) with in-house ISO 13485-certified and FDA 21 CFR 820-ready quality management systems (QMS). eInfochips has deep technical expertise in IoT/IoMT, AI/ ML, security, sensors, silicon, wireless, cloud, and power design. Connect with us to discuss how we can accelerate your product development and time to market.

Article tags

Medical & Healthcare
Smart Health
Connectivity
Artificial Intelligence (AI)
Eloqua

Related news articles

View all