Skip to main content
Arrow Electronics, Inc.

HPE Morpheus VM Essentials: A modern hypervisor for SMB and Enterprise environments

huhtikuuta 20, 2026

Virtualization has long been a standard component of IT operations.

As the market landscape shifts, many businesses are proactively reviewing their virtualization strategy to ensure cost predictability, operational flexibility and long-term sustainability. 

 HPE Morpheus VM Essentials (HPE VME) is a commercial KVM-based hypervisor with an added enterprise management layer designed to make open virtualization easier to deploy and operate in both SMB and enterprise environments. 

 Technically, the solution is built on KVM, but the weakness of “raw” KVM has traditionally been the lack of centralized enterprise management. One of the key elements HPE has added in VME is a unified management platform that allows administrators to manage hosts, clusters and workloads from a single interface. 

For many administrators, the transition is not about missing functionality but about getting used to a new tool. 

 It can be compared to switching from Apple to Android: things may have different names, and the buttons may be placed differently, but the functions are largely the same. Features such as clustering, high availability, workload deployment and centralized administration are all present — just within a different interface. 

Parallel operation and unified management

One of the most interesting aspects of HPE VME is its ability to operate alongside existing virtualization environments. 

HPE VME supports centralized management that can handle both HPE VME clusters and VMware infrastructure within the same console. This means organizations do not have to make an immediate platform decision.

Administrators can: 

  • Manage VMware environments and HPE VME clusters from the same interface 

  • Deploy new workloads on HPE VME while existing environments remain unchanged 

  • Monitor resources and workloads across both platforms 

This provides important strategic flexibility. Several organizations are already evaluating HPE VME by running selected workloads or new projects on HPE VME while keeping their existing VMware infrastructure running in parallel. 

For many companies, HPE VME can initially be used as:

A B Testing

A test environment for new workloads

Virtual Instructor B

A supplement to existing virtualization platforms

Exponential Growth

A long-term strategic alternative

This allows organizations to evaluate the platform gradually without disrupting production systems.

 

 

What HPE VME delivers for customers

HPE Morpheus VM Essentials provides the core capabilities administrators expect from a modern virtualization platform. 

 Key capabilities include: 

  • Centralized cluster management for hosts, storage and workloads 

  • High availability and clustering to maintain workload uptime 

  • Live migration to move workloads between hosts without interruption 

  • Efficient resource utilization across modern high-core servers 

  • Rapid VM deployment through standardized templates 

For virtualization teams, these operational concepts will feel very familiar. The platform provides the same core virtualization capabilities administrators already rely on — delivered through a modern management layer built on open technology.

The licensing model is a major advantage

One of the most notable differences with HPE VME is its socket-based licensing model. Unlike core-based licensing used by many virtualization platforms, VME licenses are based on CPU sockets. 

 This means: 

  • Licensing cost is independent of the number of CPU cores 

  • High-core processors become economically attractive 

  • Infrastructure can be designed more efficiently 

 Modern servers frequently include 96, 128 or even 192 CPU cores, which can dramatically increase costs in core-based licensing models. With socket-based licensing, organizations can fully utilize modern hardware without increasing virtualization licensing costs. 

 This allows businesses to consolidate more workloads onto fewer hosts while maintaining predictable costs. 

An open ecosystem that continues to evolve

Another common topic in customer discussions is platform maturity. HPE VME is still evolving, and the ecosystem around the platform continues to expand rapidly. 

Several integrations are already available, and more are being added. 

For example:

Cloud Backup B

Backup integration with enterprise solutions such as Commvault

Integration B

Veeam integration now supported

Process_Control

Disaster recovery capabilities through integrations such as Zerto

The platform also supports APIs and plug-ins that allow networking, storage and infrastructure tools to integrate directly into the management console. For many organizations, this means HPE VME can be evaluated today while the ecosystem continues to mature. 

Some companies may prefer to wait until the ecosystem is fully mature before large-scale adoption. Others are already beginning to test the platform with selected workloads and gain operational experience. 

 For partners, this creates a clear opportunity. Customers are exploring alternatives now, and those who help them evaluate new platforms early often become the trusted advisors guiding broader modernization efforts later. 

How Arrow supports your HPE VME success

Arrow supports partners across the full lifecycle of virtualization modernization. 

 Partners working with Arrow gain access to: 

  • Decades of virtualization expertise and market knowledge 

  • Enablement to deliver CloudPhysics assessments for data-driven customer conversations 

  • Sales and technical guidance to position HPE VME confidently 

  • Support for proof-of-concepts, deployment planning and migrations 

  • Assistance building value-added services around HPE VME  

 As the virtualization market continues to evolve, partners who help customers evaluate modern alternatives today will be best positioned to lead the next wave of infrastructure modernization. 

 Curious how the broader virtualization shift is impacting customers? 

Curious how the broader virtualization shift is impacting customers?

 

Read our blog
Or explore the full campaign hub to see how Arrow supports partners with assessments, enablement, and migration guidance.
Visit the HPE VME page