APAC
Similar tags
Respiratory Rate Detection Using AI Motion Amplification Technology
With the continuous improvement of the quality of life, people are paying more and more attention to their own health status, so the demand for healthcare products is getting higher and higher, which provides great opportunities for the healthcare market. In particular, respiratory monitoring applications are one of the important functional requirements of elderly care and infant care, because these people especially need additional care to monitor their health status.
New Generation of Bluetooth Audio Technology - LE Audio
At present, with an increasing number of audio products using Bluetooth for communication, Bluetooth SIG has launched a new generation of Bluetooth audio technology - LE Audio, so as to minimize the power consumption of Bluetooth audio transmissions and offer more audio capabilities. The features and related applications of Bluetooth LE Audio technology are introduced here.
Reliable cables and connectors for robotic and radar applications
Robotics and phased array radars are some of the hottest and most critical technologies in industrial and military applications today. They both require reliable interconnect solutions for proper operation in extreme, rugged environments. This article will introduce you to Samtec's cable and connector solutions for robotics and radar applications.
Inertial measurement unit performs more accurate distance measurement by machine
In various technological applications, enabling a machine to accurately grasp position and distance is key to realizing autonomous operation and movement of the machine. Applications such as robots, drones, and autonomous driving need to accurately sense the distance. This article will introduce ADI’s Inertial Measurement Unit (IMU) to understand its application fields and product characteristics.
High energy efficiency traction inverters help electric vehicles drive farther
Battery electric vehicles have become the developing focus of the automobile industry. However, increasing the driving distance of electric vehicles is the key for the masses to widely accept electric vehicles. This text will introduce high energy efficiency traction inverters used power devices launched by ON Semiconductor and help you comprehend their important role in electric automobile applications.
Coin Manganese Dioxide Lithium Battery play an important role in Tire Pressure Monitoring Systems
Being one of the hottest applications in the transportation and automotive fields at present, a Tire Pressure Monitoring System (TPMS) must adopt Coin Manganese Dioxide Lithium Battery to provide the electric power required by the system operation and data transmission. This text will introduce the Coin Manganese Dioxide Lithium Battery product line promoted by Murata aiming at severe automotive environments.
Meeting the challenges of automotive electronic modular connectivity, is your connectivity solution ready?
Yesterday’s transportation applications were relatively straightforward. Today, a new technology paradigm is emerging. Vehicle systems are now connected with complex electronics that drive modularization, with a significant increase in the number of engine compartment systems, HMI, radars and cameras that require multiple printed circuit board (PCB) and flex assemblies. These assemblies require connectors with improved signal integrity for speed and robustness in harsh environments. The latest move in the market is toward integrated, connected sensors, and the need for interconnectivity is creating a massive opportunity for suppliers.
Intelligent Connected Vehicles are moving forward on the way to dreams
Being one of the hottest technological applications at present, Intelligent Connected Vehicles are still at the early development stage. This article will analyze the general situation of technological development and the solution launched by Beijing Ruiteng Zhongtian Technology Co., Ltd to help you have a further understanding of Intelligent Connected Vehicle applications and seize the market opportunities ASAP.
Automobile audio bus optimization for audio applications
While moving, automobiles can be influenced by high temperature, vibration, engine operation, etc, which creates a strict application environment that makes audio signals easily suffer from interference and increases the complexity of cable deployment. Because of this, ADI has launched automobile audio bus (A2B®) technology and products in order to help reduce the design complexity and cost of automobile audio systems. This text will introduce the details of A2B technology and products for you.
Miniature ultrasonic sensors make object detection easier
Ultrasonic sensors are most often used for object detection and perception, distance calculation and measurement, dynamic object detection and perception, and other applications. Because the object will reflect when detected by an ultrasonic wave, this sensor can be used as an alarm device for the detection of intruders, sensor for automatic doors, and other objects. In this paper, a new kind of subminiature open-type ultrasonic sensor from Murata is introduced.