Arrow Electronic Components Online

Architecture and Solutions for Building Automation and Control Systems

Building Automation and Control Systems12 Nov 2026
A rack-mounted laptop screen displays colorful analytics charts and graphs inside a data center server rack.
View all articles

As urbanization accelerates, energy costs rise, and people's requirements for the quality of living and working environments increase, the role of buildings has evolved from simple shelter spaces into intelligent systems with sensing, analysis, and response capabilities. Building Automation and Control Systems (BACS) are at the core of this transformation. BACS integrates sensors, actuators, controllers, and communication networks to automate the management of the environment, lighting, security, energy, and other facilities within a building, achieving the goals of improving operational efficiency, reducing energy consumption, and enhancing occupant safety and comfort. This article introduces the overall architecture and application scenarios of BACS, and explains the key enabling technologies provided by ADI, including analog IO, digital IO, isolation, and communication interfaces, to help engineers build smarter, more energy-efficient, and safer building automation systems.

Architecture and applications of building automation and control systems

Smart buildings and smart homes are contemporary terms used to describe built structures that employ automated control systems to manage their environmental, lighting, security, and other facilities. By extension, the term smart city is used to describe a larger metropolitan area comprising multiple smart buildings and smart homes, which may also use elements of these automated systems for larger-scale facilities management (traffic flow, electricity, water treatment, etc.).
 
The goal of BACS is to improve operational efficiency by reducing building energy consumption while also enhancing the safety and comfort of occupants. The architecture of BACS can generally be divided into three levels: the field level, the control level, and the management level. These three levels are interconnected through communication networks to form a complete automated control system.
 
The field level is the lowest level of BACS and directly interacts with various devices and the environment within the building. This level includes sensors used to monitor environmental variables such as temperature, humidity, pressure, illuminance, gas concentration, and occupant movement. Actuators are used to drive dampers, valves, solenoids, relays, motors, and other devices to adjust environmental conditions.
 
Digital and analog IO modules are responsible for converting sensor signals into digital data and outputting control signals to actuators. BACS are typically controlled using digital controllers, which closely resemble the programmable logic controllers (PLC) units found in industrial systems. Their realization is made possible through the recent convergence of smart sensors and actuators, networking protocols, and software configurability.
 
In BACS, analog input and output ICs are used to monitor and precisely control the state of continuously varying environmental variables, such as temperature, humidity, lighting, and gas concentration. Digital inputs and outputs can be used at multiple locations within a BACS, for example, in a security subsystem monitoring building entrances/exits or as part of a fire detection and sprinkler activation system. The field level is characterized by a large number of devices, wide distribution, and often harsh electromagnetic environments. Therefore, devices at the field level must have high immunity to interference, robust protection mechanisms, and low power consumption.
 
The control level is the core of BACS and is responsible for executing control logic, data processing, and device coordination. This level includes digital controllers, such as PLCs and DDCs (Direct Digital Controllers), which execute control algorithms and logic decisions. Communication interfaces such as BACnet, Profibus, Modbus, RS-485, CAN, and Home Bus are responsible for data transmission between the control level and the field level. The Controller Area Network (CAN) is a two-wire, half-duplex, high-speed serial network typically used to provide communication between network nodes that can operate independently of the main system microcontroller. CAN transceivers act as the interface between the controller and the physical wires of the CAN bus.
 
For safety reasons, double isolation is a regulatory requirement in systems that require direct human contact. Reinforced isolators have the same protective effect as double isolation, making them suitable for use in BACS. Isolation devices are used to protect low-voltage electronics from high field-side voltages and to ensure system safety. Controllers at the control level typically have a modular design and can be expanded according to the scale and needs of the building. Controllers can cooperate through the network to achieve cross-system integrated control.
 
The management level is the highest level of BACS and is responsible for overall system monitoring, management, and decision-making. This level includes central monitoring systems (SCADA/BMS), which provide graphical interfaces that allow managers to monitor the operating status of the building in real time. Data analysis and reporting are used to collect historical data for energy consumption analysis, trend prediction, and performance evaluation. Remote access and cloud integration support remote monitoring, mobile device access, and cloud data storage. The goal of the management level is to integrate the various subsystems within the building into a unified management platform to achieve information sharing and collaborative decision-making.

Diagram presents product families for digital IO, analog IO, communications, digital isolation, and isolation plus.

Key enabling technologies launched by ADI for BACS

ADI provides key enabling technologies to build a complete BACS

ADI provides key enabling technologies to build a complete BACS, including digital and analog inputs for monitoring a wide array of sensors (temperature, humidity, pressure, etc.); digital and analog outputs for driving a variety of actuators (damper controllers, solenoids, and valves); communication interfaces (RS-485, CAN, Home Bus) for data and control signaling; and isolators for safety and to protect low-voltage electronics from high field-side voltages. The following briefly introduces the solutions provided by ADI in the above applications.
 
In analog output technology, the MAX22007 launched by ADI is a 4-channel analog output device in which each channel can be independently configured using software to operate in either current or voltage mode. With factory-calibrated output with total unadjusted error of < 1% from -40°C to 85°C, this IC provides better accuracy in a smaller footprint than discrete solutions. Key benefits of the MAX22007 include support for 0 to 10.5V analog voltage or 0 to 21mA analog current output, an integrated comparator to determine load impedance, ±42Vpp protection on all output ports, ±1kV surge protection on input ports with a 5kΩ resistor, and integrated diagnostics including thermal monitoring and shutdown protection.
 
In analog input technology, the MAX22005 12-channel industrial-grade analog-input IC launched by ADI can operate in both voltage and current mode. It provides 12 single-ended inputs, 6 differential inputs, 4 configurable inputs, or any combination thereof. The MAX22005 supports software-configurable channels that function as ±12.5V voltage or ±25mA current mode analog inputs, with a choice of internal or external voltage reference, and robust ±36V protection on all ports.
 
The configurable digital IO single-channel MAX14914 and quad-channel MAX14906 launched by ADI can be configured to operate either as a digital input or as a digital output (high-side or push-pull). Both devices provide space and power savings while offering robust protection against ESD and surges. These ICs integrate several diagnostic features that enhance overall end system reliability. The MAX14914 and MAX14906 offer the flexibility to configure each channel independently as a digital input or digital output, and feature open-wire/open-load detection and supply monitoring, as well as thermal shutdown protection. SafeDemag™ enables controlled discharge of any size inductive load.

Technical diagram illustrating the MAX22530, MAX22531, and MAX22532 isolated analog-to-digital converter interface.

High DC voltage monitoring using MAX22530 isolated ADC

Protecting BACS from high voltage damage for safe operation

ADI has launched multiple galvanic isolators. The MAX22344, MAX22345, and MAX22346 are 4-channel, 3.75kVRMS reinforced, low-power digital galvanic isolators which use ADI's proprietary process technology to provide data transfer rates up to 200Mbps. Two independent voltage supplies operate between 1.71V and 5.5V, providing logic level translation in addition to the required galvanic isolation for safety.
 
ADI has launched a dry contact/relay monitor for relays. The MAX22518 is a dual-channel isolator with an integrated DC-DC converter. Requiring only a single 3.0-5.5V logic-side supply, it eliminates the need for a bulky and expensive field-side power supply. The MAX22518 simplifies design with no requirement for a field-side supply. The field side operates up to 24VAC with an external resistor, making it ideal for monitoring low-voltage AC or DC (including relay contacts). The basic isolation rating is 3.5kVRMS.
 
ADI's MAX4896 is an 8-channel relay and load driver designed for medium voltage applications up to 50V, which can drive either latching/non-latching or dual-coil relays. It provides open-load and short-circuit fault detection and also protects against inductive kickback and overcurrent conditions. Each independent open-drain output features a 3Ω (typical) on-resistance and is guaranteed to sink 200mA of load current (VS ≥ 4.5V) when all channels are active or 410mA for each individual channel.
 
For high DC voltage monitoring, the MAX22530 family from ADI are galvanically isolated, 4-channel, multiplexed, 12-bit analog-to-digital converters (ADC) from the MAXSafe™ family product line. An integrated, isolated, DC-DC converter powers all field-side circuitry enabling field-side diagnostics even in the absence of an input signal. The MAX22530 provides robust detection of multi-channel inputs with integrated data and power isolation. High integration eliminates the requirement for a field-side supply, reducing board space and BOM, and provides flexible control and interface with programmable comparator thresholds.
 
ADI's MAX14919 is an industrial quad-channel low-side switch with 140mΩ (typical) on-resistance per channel and with integrated ±1kV/42Ω surge protection. It has resistor-settable current limiting that provides operating currents in the range of 100mA to 800mA. The outputs can be connected in parallel for higher load currents. The four switches are pin controlled to allow for simple and fast switching of up to 200kHz. Reverse-current detection prevents damage against load-supply miswiring faults, while the switches are short circuit and overload protected. Inductive loads can be rapidly discharged using the internal high-voltage clamps.

Block diagram illustrating an isolated RS-485 transceiver module labeled MAXM22510 and MAXM22511.

Isolated RS-485 device MAXM22511 in full-duplex configuration

Meeting BACS communication application requirements and maintaining robust performance

For BACS communication applications, ADI's range of RS-485 products includes half duplex, full duplex, isolated-data, and fully integrated modules like the MAXM22511 that provide full data and power isolation in a single package. All transceivers integrate high levels of ESD protection to help reduce board space while maintaining robust performance.
 
ADI's portfolio of CAN transceivers includes the MAX14883E, which provides high ESD and fault protection. It also features polarity selection to reduce down-time caused by installation errors. The MAX14878 includes integrated isolation for enhanced robustness.
 
The MAX22088 is a Home Bus System (HBS) compatible transceiver which uses a single pair of wires for data and power. This IC eliminates the need for the bulky external AC-blocking inductor typically required in bus-powered applications. It also improves signal quality, enabling longer cable runs.
 
For analog switch/multiplexer applications, the MAX14777 quad Beyond-the-Rails® (BTR) switch supports analog signals above and below the rails with a single 3.0V to 5.5V supply. It has a selectable -15V/+35V or -15V/+15V analog signal range for all switches. Each independent switch is controlled separately, making the device an alternative to opto-relays in applications that do not need galvanic isolation. Alternatively, the MAX14777 can be quickly configured as a single-supply analog input module that supports both ±15V voltages and 4mA-20mA current measurements.

Conclusion

The development of BACS symbolizes the transformation of buildings from passive shelter structures into intelligent platforms with sensing, analysis, and response capabilities. With the continuous evolution of sensing technology, communication protocols, edge computing, and cloud platforms, BACS is no longer just an automated control system within a single building, but is gradually integrating into the overall context of smart cities, energy management, and sustainable development. In the future, the value of BACS will not only lie in reducing energy consumption and improving operational efficiency, but also in creating people-oriented living and working environments with resilience and sustainability. ADI's industrial communication products can provide building automation engineers with a broad range of analog IO, digital IO, isolation, and communication interfaces that combine low power, robust performance, and improved diagnostics in the smallest possible form factors, helping us build smarter, safer, more energy-efficient, and more comfortable building environments.

Article tags

Global
Article
Analog Devices

Related Content