As Time of Flight (ToF) technology matures, there will be further opportunities to expand the use of Time of Flight cameras in a broad array of commercial and industrial applications. Analog Devices’ collaboration with Arrow simplifies the process and supports rapid prototyping of ToF solutions that can help customers quickly get to market.
Arrow and Analog Devices’ have partnered together to deliver a complete 3D ToF evaluation platform that customers can use for prototyping and product development activities. The evaluation kit includes the AD-96TOF1-EBZ mezzanine card, a complete analog front end (AFE) from Analog Devices, along with a Qualcomm DragonBoard 410c. The AD-96TOF1-EBZ mezzanine card is also compatible with the Raspberry Pi single-board computers with which it can be interfaced through the Raspberry Pi camera connector.
Learn more about the 3D Imaging Time of Flight Development Platform here.
Proof of Concept - Cutting Edge Baby Monitor:
Watch this video to see how Arrow and Analog Devices' 3DToF technology can be used to impact the next generation of technology in this use case scenario.
参阅相关产品