Skip to main content
Arrow Electronics, Inc.
Stockage Dell Technologies
Article

Meet Bob. It's already at work.

October 14, 2026

Every development team knows about AI coding assistants. Most are already using them, whether leadership has approved it or not. The challenge isn't convincing developers that AI can help. The challenge is everything that comes next.


Who's managing token consumption? Who's choosing the right models? Who's making sure AI-generated code meets security, compliance and quality standards before it reaches production? And who owns the process when that code becomes part of an application customers depend on?

 

That's where IBM Bob is different.


IBM Bob was built to support the full lifecycle of professional software development, helping organizations adopt AI in a way that's governed, scalable and cost effective. And IBM didn't start with customers. Bob spent nearly a year as IBM's own "client zero," operating inside real development teams before it was released. The result was a reported 45% average productivity gain across IBM developers.


Bob isn't just helping teams write code faster. It's helping organizations build better software, with the controls, visibility and accountability enterprise customers expect.

What is Bob?

Serveurs Dell Technologies
Bob focuses on delivering software.

Most AI coding tools focus on one part of the job: writing code.

IBM Bob is designed to support the entire software development lifecycle, helping teams build better products faster, with greater consistency, governance and cost control. That starts long before a developer opens an IDE.

 
Bob can help product owners refine and prioritize backlogs. It can help architects evaluate technologies, frameworks and dependencies to support secure and stable designs. It works alongside developers to generate and improve code, while helping front-end teams accelerate user experience design and implementation.

Exterior Of Multistory Building
Bob helps testers identify defects earlier.

The value doesn't stop when the code is written.

It supports the creation of test cases and quality checks, and assists DevOps teams with deployment automation and release workflows. Then it helps teams repeat that process for every sprint, release and iteration.

 
Think of Bob less as a coding assistant and more as a software delivery partner. Under the hood, Bob routes work to the model best suited for each task, whether that's IBM Granite, Claude, Mistral or another specialized model. At the same time, governance remains built into the workflow through capabilities such as prompt validation, sensitive-data protection, auditability and policy enforcement.

The result is simple: Bob helps teams plan better, build faster, test smarter, deploy safely and continuously improve the products they deliver.



Proven before it ever shipped

IBM didn't just tell developers Bob was ready. They proved it first, on real IBM teams:

Blue Pearl:

A Java upgrade that normally takes 30 days, done in 3, saving 160+ engineering hours with zero post-deployment defects.

IBM Instana team:

A 70% reduction in time spent on selected tasks, roughly 10 hours saved per developer, every week

APIS IT:

Decades-old government systems analyzed 10x faster, with .NET services migrated in hours instead of weeks.

That's the track record behind the tool your clients would be adopting.

Bob at work: an IBM Consulting team


One IBM Consulting delivery team didn't pilot Bob on a side project. They put it directly into daily work across two production platforms, with more than ten 

developers depending on it.

Three things changed fast.

The result: faster delivery, and engineering judgment spent where it counts.

 

 

Room_Monitoring_Multiple_CCTV_Cameras

Bob at work: IBM I developers

Bob's second act reaches a platform many assumed AI tooling would never truly understand: IBM. With Bob 2.0 and the new Premium Package for i, Bob now reads and writes source directly in QSYS and the IFS. It runs CL commands, SQL statements and PASE scripts. It compiles code, reads the errors and keeps iterating until the build is clean. It even generates and runs RPGUnit test suites.


It knows RPG, CL, DDS, and Db2 for i, not as general concepts, but with 40+ built-in skills and a direct line into official IBM documentation to ground its answers in fact, not guesswork. For teams who've spent decades hearing "AI doesn't understand legacy systems," that's the story worth telling.

Bob at work: Inside Arrow’s experience center


Our own IBM champion engineering team put Bob to the test too, not on a client project, but on our own house.


Frank Welder, of Arrow ECS, had a workspace for the Arrow experience center that had grown the way most workspaces do: organically, and without much structure. Programs, websites, scripts and documentation were scattered across folders with no version control and no consistent plan.


Bob's first move wasn't to write code. It was to look at what already existed, then propose a clean structure before touching a single file: separate folders for programs, development, infrastructure and documentation, all under one source-of-truth repository. Frank approved it. Bob executed it, moved every file, set up version control, and connected it to GitHub, in one sitting.


With a clean foundation in place, the team turned to the Arrow experience center's public showcase site. The existing setup had one page doing the job of two separate sites, with no way to add new programs without more workarounds. Bob spotted the underlying problem in the hosting setup, laid out two options with clear trade-offs, and once Frank picked a direction, built and deployed the fix itself, catching and fixing two live configuration errors along the way.


By the end of the evening: a single, organized repository, a rebuilt showcase site now covering seven Arrow Experience Center programs, and a one-command script the team can use to deploy future changes.


Why it matters: Bob wasn't just generating code snippets here. It reasoned through the trade-offs, made a recommendation and carried that decision all the way to a live, working deployment, on its own team's infrastructure, not just a demo environment.

Why Bob wins the harder conversation

Plenty of tools can write good code. GitHub Copilot, Cursor, Claude Code, and OpenAI Codex all do that well, often on the very same underlying models Bob uses.


But enterprise clients aren't just asking "can AI write code faster?" anymore. They're asking harder questions. Will this hold up under audit? Does it reach our mainframe and our COBOL, PL/I, and RPG estates, not just our modern stack? Who approves what it changes before it ships?


That's the ground the other tools don't cover. Bob's argument isn't raw coding skill, it's everything around the model: full lifecycle scope, governance and audit built in, real modernisation reach, and the flexibility to deploy in a regulated environment.

Where this opens revenue for you

Business_Meeting_at_Trendy_Startup_Company

For your clients running IBM Z, IBM i, Power, or watsonx, Bob isn't a bolt-on tool.

It's a reason to open a bigger conversation, and the attach points are concrete, not hypothetical:

  • IBM Z: a dedicated Premium Package built on watsonx Code Assistant for Z, with modes tuned for system-level reasoning and for COBOL, PL/I, JCL and z/OS generation.
  • watsonx Orchestrate: Bob is already the IDE-side tool for building and deploying agents, available now for any account running or evaluating Orchestrate.
  • IBM i and Power: in active use today for modernization work, exactly where many of your legacy-heavy clients already sit.
African_American_Male_Working

Each of those maps to a real services opportunity

Modernization work for clients sitting on years of technical debt, governance advisory for regulated industries, platform attach into existing IBM accounts and managed AI development services for clients who want this running, not just piloted.


The clients who need this most are the ones with the most legacy risk: heavy technical debt, mainframe or IBM i systems, regulated compliance requirements or leadership asking for AI adoption they can actually govern.

Why this matters for you

If you sell IBM solutions, Bob gives you something concrete to bring to the table. Not a promise about the future of AI. A working track record, real customer stories and a clear path to new services revenue on top of it.


Every client conversation about AI coding tools eventually asks the same question: does this actually hold up outside the demo? Now you have proof from IBM's own client-zero results, an enterprise consulting team, an IBM i shop and our own champion engineering team. Bob isn't a concept. It's already building.


We've put the full detail, including how Bob compares against the field and where it fits across the IBM portfolio, into a Partner Guide. 

Download it or talk to your Arrow IBM to bring this into your next modernization conversation.
Get in touch