For channel partners, the conversation is changing. Commvault and NetApp offer a way to help customers move beyond protecting data to demonstrating that they can recover it when it matters.
Most organizations have a backup strategy. They replicate data, maintain recovery copies and invest in tools designed to protect critical information. But there's an important question that traditional backup conversations don't always answer: What happens when it's time to recover?
As ransomware and AI-driven cyber threats become more sophisticated, having a backup is only part of the equation. Organizations also need to know whether their recovery points are clean, how quickly they can restore operations and whether their recovery processes will work under pressure.
For channel partners, this creates an opportunity to shift the discussion from backup infrastructure to something customers increasingly need: greater certainty about their ability to recover.
Backup isn't the same as recovery readiness
An immutable backup can help protect data against unauthorized changes or deletion. But immutability alone doesn't establish whether the information is free from compromise or ready to restore.
Consider a customer whose environment has been affected by ransomware. They may have multiple backup copies available, but determining which recovery point is safe to use can still be a challenge. Restoring compromised data could introduce additional risk, while uncertainty about the recovery process can extend downtime.
This is where a more comprehensive approach to cyber resilience becomes important.
NetApp and Commvault bring together threat detection, immutable data protection, recovery capabilities and validation tools to help organizations prepare for incidents before they happen.
Rather than treating backup and recovery as separate activities, partners can help customers think about the entire process, from identifying suspicious behavior to testing whether critical systems can be restored.
From detecting threats to validating recovery
The value of the Commvault and NetApp approach becomes clearer when viewed across five connected capabilities.
Detect suspicious activity earlier. NetApp Autonomous Ransomware Protection with AI (ARP/AI) helps identify unusual file activity and can create snapshots in response to suspected ransomware behavior. Earlier detection gives organizations another opportunity to limit the impact of an attack.
Protect critical recovery data. NetApp SnapLock provides immutable storage capabilities designed to help safeguard data from alteration or deletion. Protecting recovery copies is an important part of maintaining options after an incident.
Recover from available snapshots. Commvault can use NetApp snapshots to support recovery workflows, helping organizations access recovery points and restore protected data. The objective is to reduce the time and complexity involved in getting critical systems back into operation.
Validate recovery before an incident. Commvault Cleanroom provides an isolated environment for recovery testing, forensic analysis and recovery operations. This allows organizations to examine and test recovery points without immediately introducing them into production.
Orchestrate the process. Commvault brings centralized management and threat-aware recovery orchestration into the picture, helping IT teams coordinate recovery activities across their environments.
Together, these capabilities support a more complete recovery strategy. The goal isn't simply to have protected data available. It's to help organizations establish a repeatable process for determining what can be recovered and how.
Three customer conversations worth having
For partners, cyber resilience doesn't have to begin with a discussion about replacing a customer's existing backup solution.
Often, the most productive starting point is a business or operational challenge the customer already recognizes.
1. Cyber recovery and ransomware readiness
A customer may have invested heavily in cybersecurity and backup but have limited experience testing recovery after a serious incident.
This is an opportunity to ask:
How confident are you that your current recovery points are clean and ready to restore?
The answer can reveal gaps in recovery validation, isolation, orchestration or testing. With Commvault and NetApp, partners can explore how earlier threat detection, immutable protection and recovery validation could help customers strengthen their response to ransomware and reduce the potential impact of downtime.
2. Backup infrastructure modernization
Many organizations are also reconsidering the infrastructure supporting their backup operations.
Legacy backup appliances, growing capacity requirements and changing workload demands can make traditional architectures harder to manage and scale.
A useful question is:
Is your current backup architecture giving you the flexibility and scalability you need?
For customers facing these challenges, the conversation can extend beyond cyber recovery into infrastructure modernization.
One option is Commvault Flex with NetApp StorageGRID, which combines a disaggregated backup architecture with scalable, immutable S3 object storage.
By separating compute from storage, this approach gives organizations greater flexibility in how they scale their backup environments while maintaining a simplified operational model.
For partners, it offers another way to engage customers evaluating their existing backup appliances and long-term infrastructure requirements.
3. Archiving and long-term retention
Not every data protection challenge is driven by an immediate security concern.
As data volumes grow, organizations must also manage retention requirements, storage costs and access to information that may be needed months or years later.
Partners can start by asking:
How are you balancing long-term retention requirements with storage costs and accessibility?
This opens a discussion about moving infrequently accessed data to cost-efficient object storage while maintaining appropriate governance and access.
It's also an opportunity to look more broadly at how the customer's data protection strategy supports both operational and financial priorities.
A broader approach to data protection
The appeal of an integrated Commvault and NetApp strategy extends beyond any single recovery feature.
Customers are balancing multiple requirements at once: protecting critical information, reducing downtime, supporting hybrid and multicloud environments, simplifying management and keeping infrastructure costs under control.
An approach that connects storage and data protection capabilities can help address these priorities together.
For example, snapshot-based recovery can support faster restoration, while immutable storage and threat detection strengthen the protection of critical data. Centralized management and orchestration can help simplify recovery processes across environments.
The architecture also gives partners room to discuss different deployment requirements, from on-premises infrastructure to hybrid, multicloud and SaaS workloads.
Importantly, the right approach will depend on the customer's existing environment, recovery objectives and operational requirements. The opportunity is to understand those needs first, rather than lead with a predetermined product configuration.
What this means for channel partners
Customers don't necessarily want another conversation about backup features. They want to understand whether their business can withstand an attack and how quickly essential operations can resume.
That creates room for partners to play a more consultative role. Instead of beginning with storage capacity or backup licensing, start with the customer's recovery expectations. Ask when they last tested a full recovery, how they identify trustworthy recovery points and what their current process would look like during a ransomware incident.
Those discussions can reveal opportunities for assessments, solution design, recovery planning and ongoing services. They can also help partners build stronger relationships by connecting technology decisions to the customer's operational priorities.
Arrow can support partners as they explore the Commvault and NetApp portfolio, evaluate customer requirements and identify opportunities to develop their cyber resilience business.
Change the recovery conversation
Backup remains essential. But the real test of a data protection strategy comes when an organization needs to restore its systems and resume operations.
With Commvault and NetApp, partners can help customers look beyond whether their data is backed up and focus on whether their recovery processes are ready to perform.
It's a more meaningful conversation about cyber resilience, and one worth having before an incident occurs. Strengthen your customers' recovery readiness.
Contact your Arrow Channel Manager or email commvaultecs@arrow.com to explore Commvault and NetApp opportunities.
Connect with Arrow