Top 10 Gifts for Engineers 2016

게시자

Click Here for the 2017 Engineer's Gift Guide!

Even around the holidays, engineers can more often than not be found tucked away in their labs or workspaces hammering out the details of a new project or scratching their heads at the one that never seems to end. If you, on the other hand, are scratching your head as to what kind of a gift to give them this season, why not pick out something that makes their workspace a little more complete? To help you out, we’ve compiled a list of tools and toys perfect for the electronics engineer on your shopping list. 

1. LoRaWAN 868 Extreme Range Starter Kit               ~ $122

Get a little more connected this holiday season. With the world becoming more connected (and our projects too), there is a need to send data and respond to commands no matter where a system is. The LoRaWAN 868 Starter Kit from Libelium lets you experiment with the LoRaWAN standard, which allows for better range than cellular modems at extremely low power consumption. To give you an idea of the range, Amsterdam managed to cover the entire city using only 10 gateways. Now systems can stay connected everywhere without sacrificing battery power. How’s that for a holiday treat?

관련 상품 참조

10681

Libelium 보기

2. Solar Powered BLE Kit ~ $46

There’s no need to be blue this time of year when you’ve got the gift of Bluetooth low energy – it has the ability to help us connect lots of little sensors without needing a ton of power. This CYALKIT-E02 kit from Cypress lets you play with a sensor sending temperature and humidity data broadcasting over BLE – it is powered only by a small solar cell and is an excellent way to learn about keeping power profiles small while sending the data you need.

3. ICE40HX1K-BLINK-EVN ~ $37

Learning new tech is always fun, and now is a great time to experience the world of FPGAs, which are becoming more popular for extreme high performance computing like Machine Learning and Image Recognition. The Lattice Semi iCEblink40 HX1K is a small introduction to this world – it comes on a ready to go dev-board with 1024 Logic Cells, 68 3.3V I/Os, and a pinout that allows you to add some Arduino Shields onto it to get started. The HX1K is a great way to learn about these technologies that are making their way into many modern engineering projects from AI and Machine Learning to Quad Copters and Cameras.

관련 상품 참조

ICE40HX1K-BLINK-EVN

Lattice Semiconductor Programmable Logic Development Boards and Kits 보기

4. X NUCLEO IKS01A1 ~ $15

Being able to sense the environment around you is the first step to having a project that can react to external stimulus. The ST IKS01A1 is a full featured sensor add on board that can give you 9 degrees of freedom sensing with its accelerometer, gyroscope, and magnetometer as well as providing barometric pressure, humidity, and temperature. Being pinned out for the Arduino layout means you can get started quickly and have high quality sensing data for whatever project you may be undertaking, be it the next warehouse sorting robot or a package delivery drone.

관련 상품 참조

Motion and Evironment Sensor | X NUCLEO IKS01A1

STMicroelectronics Sensor Development Boards and Kits 보기

5. Intel JOULE Kit ~ $373

So you have had a chance to play with the Raspberry Pi, the Arduino, and many other hobbyist boards, but now it is time to step it up. The Intel Joule has a ton of power and can handle encoding and displaying 4K video with a whole set of tools for understanding and reacting to that video, making it an excellent foundation for robotics or self-navigating systems. All this power comes in an incredibly small package with a breakout board that lets you get started quickly. 

관련 상품 참조

GT.PDKW

Intel Embedded System Development Boards and Kits 보기

6. Kinetis K66 Freedomboard ~ $63

Embedded electronics are getting more powerful at a quick pace, and it seems that many things nowadays are somehow related to the various ARM architectures. This Kinetis K66 Freedomboard from NXP gets you started with an ARM M4 processor quickly while allowing you to use Arduino compatible shields and has onboard Gyroscope, Magnetometer, and Accelerometers to let you experiment. The Freedom board is an excellent gift to get started with higher powered embedded electronics. 

관련 상품 참조

FRDM-K66F

NXP Semiconductors Embedded System Development Boards and Kits 보기

7. Weller Solder Stations ~ $326 and $112

As you get into making your own systems, prototyping your dreams, and seeing ideas come to life, it is nice to have a tool that can keep up. The Weller WD1003 soldering station gives you digital control over your temperatures, so you just tell it the temp you want and that is what you get. It also has three memory slots, so as you change component types it is quick to get to the temperature you need. This is a soldering station that can keep up with the needs of your projects and is an excellent workbench upgrade.

The entry point to an electronics obsession is the humble pen soldering iron that plugs right into the wall, but as you get more involved it is nice to have fine temperature control. The Weller WES51 is a great upgrade to the electronics workbench, giving you fine control over the soldering temperature and letting you work with more components like microcontrollers. In addition, having the ability to change out tips lets you have the right tool for each soldering job. It’s a gift any engineer would love.

8. Weller WSB80 Solder Bath ~ $222

If you already have a Weller WD or WR series soldering station, this WSB80 Solder Bath can help speed up your timeline for those projects you’ve got sitting on the workbench. Using a solder bath, you can quickly tin wires and component leads, resulting in better solder joints and more reliable systems.

9. Weller RTW 1 Tweezers ~ $67

Moving from through hole to surface mount can present a new challenge when soldering components. Tweezers like these RTW 1’s from Weller make it easy to get chip resistors and other pieces onto the board and get your holiday project out the door.

10. Adafruit PCB Ruler ~ $4

This PCB ruler from Adafruit is an excellent stocking stuffer for the engineer in your life, giving them lots of useful information from basic measuring to wire gauge sizes and surface mount component layouts. 

관련 상품 참조

1554

Adafruit Industries Development Kits and Tools 보기

The holidays are fast approaching, but with this handy list, you won’t have any trouble finding that one special gift sure to make your favorite engineer smile. Happy holidays, from all of us at Arrow.

*Prices subject to change.

 

관련 동영상

최신 동영상

죄송합니다. 선택한 필터와 일치하는 결과가 없습니다.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.