Increasing solid-state drive reliability with intelligent data protection

Solid-state drives bring inherently high reliability to applications from entry-level consumer equipment to mission-critical systems. Proper data protection mechanisms can maximize the lifetime of the drive by taking preventative measures when needed and anticipating causes of data loss such as excessive access behavior, overtemperature, power instability, and malicious attacks. This article explores how Silicon Motion solid-state drives, coupled with intelligent data protection technology, are a great choice for modern system designs.

SSD reliability

Solid-state drives (SSDs) provide high-performing and compact mass storage for embedded computing applications that make today’s digital lifestyles possible. They are found in equipment such as car computing and navigation systems, thin clients, point-of-sale terminals, multifunction printers, telecommunications equipment, factory automation tools, and server systems of all types and sizes, from small data centers to cloud-level facilities.

The typical SSD lifetime is heavily dependent on the NAND Flash technology used. QLC (Quad-level cell) and TLC (Triple-level cell) NAND have a lifetime between 1,000 to 3,000 program/erase cycles per cell, while the expected lifetime for MLC (multi-layer cell) is 3,000 to 10,000 cycles. SLC (single-layer cell) NAND has the longest lifetime, up to 100,000 cycles. These known limitations help system designers choose the optimum SSD technology for their application, depending on the required endurance, price, and mission criticality. TLC NAND, with the lowest endurance, typically comes at a lower price than the others and is usually sought for use in cost-conscious consumer products.

Although the typical lifetime range for any given technology can be predicted, the actual lifetime of any given drive cannot be known. Unexpected failure can cause data loss, system downtime, and repair costs. The consequences can range from inconvenient to catastrophic. System designers need tools to help avoid these problems by managing and protecting the SSD to maximize its lifetime and taking preventative measures before any drive failure occurs.

A failing SSD can significantly degrade system performance. Slow read/write speeds, increased access times, and frequent error handling can lead to a sluggish response and decreased overall system efficiency.

After failure, recovery and repair can involve replacing the faulty SSD, restoring data from backups, and reconfiguring the system, all of which can be time-consuming and result in additional costs. Professional assistance may be needed to diagnose and resolve the issue. Sometimes, the entire embedded system might need to be replaced if the SSD failure cannot be easily rectified.

To mitigate the consequences of SSD failure, it is essential to have proper backup strategies, redundancy measures, and monitoring systems in place.

Silicon Motion intelligent data protection series

Among the tools available for managing SSDs safely and securely, built-in data protection mechanisms can both prevent and mitigate expected lifetime-based failures. Additionally, they can provide protection against hazards such as prolonged time duration, excessive read access, cross temperature, overtemperature, power instability, hacking, and all of which can shorten the life of the drive.

FerriSSDs come with a set of intelligent data protection mechanisms that meet the storage needs of different application systems and can be effectively activated in various environments where data loss may occur.

0924-FerriSSD-Intelligent-Series-Tiles

These mechanisms include IntelligentLog™, which comprehensively records the health status of the SSD to let system developers understand its current condition and take appropriate measures. When the SSD approaches its usage limit, it is possible to proactively inform the host of any potential danger regarding read and write cycles; data migration is initiated to ensure data integrity and prevent any loss. It also records major event logs for faster and more efficient debugging. In addition, IntelligentScan™ performs automatic scanning and repairs, ensuring that data stored in the secure area can be read and written correctly. It increases the duration of data storage and extends the lifespan of the SSD (see figure 1).

0924-FerriSSD-Intelligent-Series-chart

Figure 1. IntelligentScan & DataRefresh functions can detect high-risk factors before the data is lost

Overtemperature protection

Exposure to high temperatures can present a number of hazards to SSDs, including accelerating the degradation of the NAND flash memory cells, which, over time, can shorten the lifespan of the drive. Excessive heat can also affect the integrity of the stored data and increase the risk of read or write errors. Performance degradation can also occur, including slower access times, decreased transfer rates, and latency issues, resulting in decreased overall system performance and responsiveness. To prevent such problems, FerriSSD IntelligentThermal™ monitors the drive’s temperature and activates cooling mechanisms if a certain threshold is exceeded. It effectively chooses between host-controlled thermal management (HCTM) and drive-controlled thermal management (DCTM) to control temperature and prevent SSD damage in high-temperature conditions.

Power loss

Power loss can affect data protection in several ways. If power is suddenly lost during a write operation, the SSD may not have enough time to complete the data writing process. This can result in partially written data or metadata inconsistencies, causing the stored information to be corrupted or inaccessible. Also, power loss during remapping processes such as wear leveling, which is performed regularly to distribute write operations across memory cells evenly, can lead to data mapping errors or incorrect tracking of data locations. This can cause data loss or fragmentation, affecting the overall reliability and accessibility of the stored data.

In addition, data temporarily stored in the cache can be lost if a power outage occurs before the cached data is written into the main storage, resulting in data inconsistencies or file system corruption. Also, power loss can interrupt the updating or synchronization of metadata used for organizing and managing the stored data, leading to corruption or inconsistencies that can cause issues during boot-up or result in the loss of file system integrity.

To protect against power disruptions, FerriSSD IntelligentShield™ ensures that all data being transmitted is securely stored in a designated safe area, preventing data loss caused by power outages. The drive initiates this mechanism as soon as instability in the power supply is detected and also activates FerriSSD’s IntelligentFlush™. This enables instant data migration at a consistent speed, allowing data to be swiftly moved to a secure storage block (see figure 2).

0924-FerriSSD-Intelligent-Series-charts

Figure 2: IntelligentFlush™ enables instant data migration at a consistent speed, allowing data to be swiftly moved to a secure storage block.

Completing protection for drives

The data protection features also include preventing hacker attacks that could compromise the SSD's management functionality. Because all data transmission and protection mechanisms within the SSD are managed by the firmware, safeguarding these against attacks is critical. Ferri’s IntelligentGuard™ technology achieves this by enhancing the authentication and protection mechanisms of the SSD's firmware (see figure 3).

0924-FerriSSD-Intelligent-Series-Whitepaper

Figure 3: IntelligentGuard™ technology maintains boot security by enhancing authentication and protection mechanisms of the SSD's firmware.

Additional features include IntelligentImage™, a preloading mechanism for embedded systems that allows data to be loaded onto a safe block before surface-mount assembly. This protects the data against manufacturing hazards such as damage by high reflow soldering temperatures and significantly enhances production line efficiency. Finally, IntelligentZones™ supports a multi-Name Space design, allowing the SSD to be tailored according to the requirements of different system designers. The SSD is divided into different storage blocks, and data is placed in the appropriate block based on the design. This ensures data integrity as well as effective utilization of SSD capacity, thereby maximizing economic benefits.

Conclusion

Intelligent data protection series provide an effective solution to data loss in various environments and ensure the safekeeping of all data stored on the drive. With these advanced protective measures in place, users can prolong the life of their drives and ensure their data is secure at all times.


Articles de presse apparentés

Actualité

Sorry, your filter selection returned no results.

Nous avons mis à jour notre politique de confidentialité. Prenez un moment pour lire les changements. En cliquant sur "J'accepte", vous acceptez la clause de confidentialité d'Arrow Electronics ainsi que les conditions d'utilisation.

Notre site Internet place des cookies sur votre appareil pour améliorer votre expérience et pour améliorer notre site. Pour en savoir plus sur les cookies que nous utilisons et la façon de les désactiver, cliquez ici. Des cookies et des technologies de suivi peuvent être utilisés à des fins de marketing. En cliquant sur « Accepter », vous consentez au placement de cookies sur votre appareil et à notre utilisation de technologies de suivi. Cliquez sur « En savoir plus » pour de plus amples informations et instructions sur la façon de désactiver les cookies et les technologies de suivi. Même si l'acceptation des cookies et technologies de suivi est volontaire, leur désactivation peut entraîner un mauvais fonctionnement du site Internet et certaines publicités peuvent être moins pertinentes pour vous. Nous respectons votre confidentialité. Lisez notre politique de confidentialité ici.