Virtual power plants (VPPs) and the future of the smart grid
By Jeremy Cook
Most conversations about the transition from fossil fuel power generation to solar and wind lean toward replacing existing power plants with renewable power plants. However, the modular nature of renewable generation—plus new options for energy storage systems—means there’s another option: the Virtual Power Plant, or VPP.
What is a virtual power plant?
The virtual power plant concept aggregates distributed energy resources (DER) to act as a coordinated power supply, supplementing or even replacing traditional centralized generation. Solar and wind production from residential and commercial generators can become the primary or supplemental energy provider for a network of users.
Traditionally, electric power is supplied to homes and businesses by centralized power plants, distributed through the electrical grid. While there are many twists and turns along the way, it’s ultimately a plant-to-user affair. Emerging smart grid technology and infrastructure, including two-way metering equipment, means that consumers can sell power back to the grid, lightening the load for dedicated power producers while earning monetary rebates. Consumers can also store power on-site to purchase and sell when expedient. On the remote Isle of Eigg in Scotland, VPP smart grid systems are already in use with homes and businesses coordinating their usage to avoid strain on the grid.
Why do we need virtual power plants?
When you consider home solar and battery backup, one ideal is total energy independence, with a $0 monthly bill. In extreme cases, you might envision being disconnected from the grid entirely, living off the land—or, more accurately, the sun’s rays.
The cost for such an off-grid setup can be extreme, and if your personal equipment breaks you have to fix it to restore power. From a user perspective, VPPs offer most of the personal benefits of such an off-grid setup at a potentially much lower price as well as backup power from the grid. VPPs also present several benefits on a societal level versus a centralized fuel-fired or even solar-powered facility.
Consider the VPP concept’s modularity and that generation can take place near consumption. In the traditional grid model if there is a problem with power transmission in one area, it can easily affect another geographic location. The VPP concept provides more localized options for re-routing power to keep the lights on, and it could even result in lower transmission losses as power is typically consumed closer to where it’s produced.
On a personal level, if your equipment malfunctions the grid and other DER can provide backup power, enabling a very robust energy supply.
Physical power plants (coal-fired, solar, nuclear, or otherwise) take up land that could otherwise be used for managed forests, farms, and parks. However, VPPs take advantage of otherwise unused rooftop space for solar panels. Solar can also be installed over existing parking areas creating the dual benefit of power production, plus shaded automobile storage. Adding in EV energy storage systems and charging in such a scenario further sweetens the parking/DER scenario.
When you consider home solar and battery backup, one ideal is total energy independence, with a $0 monthly bill. In extreme cases, you might envision being disconnected from the grid entirely, living off the land—or, more accurately, the sun’s rays.
The cost for such an off-grid setup can be extreme, and if your personal equipment breaks you have to fix it to restore power. From a user perspective, VPPs offer most of the personal benefits of such an off-grid setup at a potentially much lower price as well as backup power from the grid. VPPs also present several benefits on a societal level versus a centralized fuel-fired or even solar-powered facility.
Consider the VPP concept’s modularity and that generation can take place near consumption. In the traditional grid model if there is a problem with power transmission in one area, it can easily affect another geographic location. The VPP concept provides more localized options for re-routing power to keep the lights on, and it could even result in lower transmission losses as power is typically consumed closer to where it’s produced.
On a personal level, if your equipment malfunctions the grid and other DER can provide backup power, enabling a very robust energy supply.
Physical power plants (coal-fired, solar, nuclear, or otherwise) take up land that could otherwise be used for managed forests, farms, and parks. However, VPPs take advantage of otherwise unused rooftop space for solar panels. Solar can also be installed over existing parking areas creating the dual benefit of power production, plus shaded automobile storage. Adding in EV energy storage systems and charging in such a scenario further sweetens the parking/DER scenario.
Virtual power plants: Coordinating resources
In a VPP scenario consider that coordination between sources is also needed on a very low level, down to ensuring that line frequencies match up properly. Long-range transmission and overall grid maintenance are also necessary, which is beyond the scope of individual homeowners.
Efficiency will be paramount for this future VPP concept to work well, potentially taking advantage of SiC transistors, current sensors, and power-line communication to keep everything coordinated. Given future requirements it’s safe to say that power companies aren’t going anywhere soon, they may simply take on a different form in the coming decades.
Article tags