Inertial sensing boosts precision and productivity in smart farming
With the global population continuing to grow, modern smart farming is actively embracing technological innovation and automation to ensure food supply under sustainable conditions. Inertial sensors play a vital role in various application scenarios. Precision inertial measurement units provide navigation and stability control for the increasing number of robots in agriculture, including self-steering tractors, picking robots, drones, and more. Furthermore, wideband inertial sensors can be used for predictive maintenance of all such complex machinery. Additionally, inertial sensors enable various edge sensing modalities, such as animal tracking, heat detection in dairy animals, and vital sign monitoring. This article introduces the trends in smart farming and relevant solutions offered by ADI.
AI, machine learning, robotics, and IoT make smart farming more cost-effective
The world's population is projected to approach 10 billion by 2050, requiring a 70% increase in global food production to meet rising living standards. However, the agricultural market faces unprecedented challenges. In many developed and developing nations, the agricultural workforce continues to decline. Younger generations are moving away from traditional farming, leading to rising labor costs. Climate change exacerbates these challenges, with unpredictable weather patterns, soil degradation, and water scarcity posing serious threats to farmers worldwide. Agribusinesses must increase yields, reduce waste, and optimize costs to meet demand and remain competitive. Technological advancements provide crucial support here. The rise of Artificial Intelligence (AI), Machine Learning (ML), robotics, and the Internet of Things (IoT) has made automation in smart farming more feasible and cost-effective. Today, farmers can utilize data-driven analytics to improve decision-making.
The introduction of automated systems such as robotic harvesting and drone-assisted monitoring has made farming operations faster and more efficient, reducing reliance on manual labor. Precision farming techniques improve soil health, seeding accuracy, and crop growth, increasing yield per acre. Smart irrigation and fertilization systems effectively reduce water and fertilizer waste, achieving cost savings and resource conservation.
In the realm of smart farming, inertial sensors perform multiple critical functions. Firstly, inertial sensors provide real-time data on acceleration, orientation, and position, thereby enhancing the operational efficiency of autonomous and semi-autonomous farming vehicles. With the aid of GPS, Inertial Measurement Units (IMUs) are widely used for the navigation of ground and aerial vehicles like tractors, robots, and drones, as well as for monitoring their attitude and other inertial states. This enables these vehicles to accurately follow predetermined paths for seeding, tilling, and spraying, effectively reducing costs and promoting sustainable agricultural development. Secondly, in livestock management, inertial sensors can track animal movement and behavior, allowing farmers to monitor herd health and detect anomalies in activity patterns. Finally, the integration of inertial sensors with AI further strengthens the predictive maintenance capabilities of agricultural equipment, effectively reducing downtime and maintenance costs.
Advancements in Micro-Electro-Mechanical Systems (MEMS) technology have led to enhanced performance, making MEMS IMUs key components for scalable autonomous vehicle (AV) platforms. MEMS IMUs are typically used as feedback sensing elements in motion control systems, with common applications including Guidance Navigation Control (GNC) in autonomous vehicles and pointing control for smart implements (like sprayers, seeders, buckets, blades). When employed as feedback sensing element, the performance of MEMS IMUs directly impacts system accuracy.
ADIS16576 inertial frame of reference
MEMS inertial measurement units enhance system stability and maneuverability
The ADIS16576 from ADI is a MEMS IMU that represents a significant breakthrough in both functional integration and core sensor performance, with particularly notable improvements in Vibration Rectification Error (VRE) - a 10x improvement for the gyroscope and a 50x improvement for the accelerometer. The fundamental function of a MEMS IMU is to provide triaxial angular rate sensing around three mutually orthogonal axes (roll, pitch, yaw) and triaxial linear acceleration sensing along the same three axes.
The accelerometer provides mean (or static) angle estimation, while integrated gyroscope measurements provide real-time angular displacement. The system processor combine these two angle estimation sources to generate reliable feedback control information for GNC or pointing control systems. Operating in this manner, an accelerometer VRE of 1.3 mg under 4 g of vibration means the GNC platform can maintain an attitude angle better than 0.1° without assistance from any other sensing function. This is particularly beneficial for UAVs, especially those whose vibration levels vary significantly with thrust.
In gyroscopes, VRE can cause rapid and persistent changes in bias, leading to erroneous motion correction and, in the worst case, platform instability. Previous-generation devices could exhibit VRE responses exceeding 300°/h under 8 g rms, whereas the ADIS16576 offers a response of 12°/h, significantly reducing the estimation/correction burden on other system sensing modes. One of the most important functional improvements of this MEMS IMU is its scalable external synchronization. By incorporating a user-programmable clock scaling function, system developers can now drive 4000 Hz IMU data sampling using slower system-level references, such as GPS or video sync. This achieves tight coupling with Pulse Per Second (PPS) or perception sensing references while preserving the various digital processing options afforded by higher data sampling rates.
Take an autonomous vehicle platform as an example; it can use a 20 Hz GPS reference and a 200x scale factor to generate an internal sampling rate of 4000 Hz. Furthermore, the system can employ an on-board decimation filter to reduce the output data rate by a factor of 20x (to 200 Hz). In more dynamic scenarios, such as a crop inspection drone operating in windy conditions, the system processor may need to read and process data at the maximum sampling rate to ensure stability and maneuverability.
ADXL366 configured as a motion switch in an IoT system
Inertial sensors play a key role in IoT systems
Inertial sensors also play a pivotal role in IoT systems, which can be used for continuous monitoring of animal location and physiological conditions. Typical embodiments include tags affixed to the ear, tail, or body, or smart collars worn around the neck. These tags not only help manage herd location but, more importantly, continuously provide animal health data such as activity levels, feeding times, and respiration rates. Furthermore, newer tags possess the capability to track heart rate and other vital signs. Neck-worn collars have become invaluable tools for detecting estrus, rumination, lameness, and other conditions in cattle. One of the core requirements for such IoT systems is low power consumption, as maintaining batteries (rechargeable or primary) for large herds is a tedious and challenging task.
ADI's ADXL366 offers exceptional low-power advantages. This triaxial accelerometer incorporates internal voltage regulation, allowing it to be connected directly to a battery. Its minimum operating voltage is 1.1 V, and it can provide motion data at 100 Hz with a power consumption of only about 1 µW. This energy consumption level is lower than the self-discharge rate of a coin cell battery. When used in a neck-worn collar, this accelerometer can adjust between low-power and low-noise modes, providing a minimum signal between 3 mg and 8 mg rms, sufficient to distinguish chewing, rumination, and respiration rate (RR). The ADXL380 offers enhanced vital sign monitoring capability, with operational noise levels nearly two orders of magnitude lower across a 4 kHz bandwidth. For an equivalent bandwidth comparison at 200 Hz, the equivalent noise for this accelerometer is 0.4 mg rms. The high Signal-to-Noise Ratio (SNR) combined with wide bandwidth allows this triaxial accelerometer to function as a "stethoscope," collecting heart rate information via ballistocardiograms or capturing various noises associated with breathing, digestion, and other physiological functions.
Another core capability of ultra-low-power inertial sensors is supporting system-level power management for IoT nodes. The ADXL366 provides a dedicated wake-up mode that can issue interrupts based on detected motion profiles to manage the power cycle of electronic systems. The accelerometer offers a rich set of programmable parameters to configure the desired motion profile and, most importantly, to wake and sample at full bandwidth. This capability is crucial for avoiding aliasing and false detection. In wake-up mode, the ADXL366 consumes an astonishingly low 180 nA. Leveraging this feature, high-power sensors, radios, and other components can be powered down when not needed, thereby extending the useful lifetime of the sensor node.
Integrated inertial sensing and AI analytics enable predictive maintenance in smart farming
Finally, the discussion turns to the integration of inertial sensing and AI analytics, aimed at achieving predictive maintenance in smart farming. As modern farms expand in scale, they increasingly rely on high capital expense machinery for production. Such equipment must not only operate with precision but also withstand the harsh environments and intensive demands of seasonal farming tasks. Equipment failure during the short planting or harvesting season can lead to significant economic losses.
For example, precision equipment like seeders or harvesters often must operate in adverse conditions such as rain, wind, dust, mud, and rock fragments . In these environments, changes in key vibration signatures can be used to predict equipment issues in advance, allowing for maintenance during periods that minimally impact peak-demand production times. Mechanical vibration analysis (similar to vital sign monitoring in livestock) can precisely identify the failure modes and timing of various problems in mechanical elements, such as bearing faults, axle misalignment, imbalance, looseness, gear faults, and other issues. Consider a bearing defect, such as spalling or deviation from an ideal spherical shape. Each time this defect contacts the machine surface, it creates an impulse on the platform, triggering a complex vibration response containing both fundamental and broadband content.
Therefore, to achieve predictive maintenance, accelerometers need to meet three important performance criteria: low noise (for early prediction), high bandwidth (to detect all spectral contents and support fault classification), and a sufficiently high measurement range. However, the last requirement is often overlooked because the magnitude of acceleration is proportional to the square of the frequency (ω²). If not considered, high-frequency spectral content can saturate the sensor. ADI's new ADXL382 triaxial digital accelerometer in a compact package meets all three requirements. This product supports measurement ranges of ±15 g, ±30 g, and ±60 g, offers an 8 kHz bandwidth, and features ultra-low noise of less than 55 μg/√Hz.
The ADXL382 boasts industry-leading noise performance, enabling high-precision applications with minimal calibration. Its low noise and low power characteristics allow for accurate measurement of audio signals or heart sounds even in high-vibration environments. Furthermore, the ADXL382 enables true system-level performance, including a built-in micropower temperature sensor, single-, double-, or triple-tap detection, and a state machine to prevent false triggering.
Conclusion
Automation and technological advancement in agriculture are key forces in addressing critical global challenges such as food security, labor shortages, and environmental sustainability. By adopting innovations like AI, robotics, and precision farming, agricultural production can enhance efficiency, reduce costs, and ensure a more sustainable future for food production. Within the agricultural technology ecosystem, inertial sensors provide core sensing capabilities and play a pivotal role. However, careful consideration must be given when selecting sensors to ensure their performance and functionality align with the specific application. The relevant solutions offered by ADI will accelerate the development of smart farming and stand as one of the optimal choices for related applications.
Article tags