LEDs, Heat, and You

发布人是

When it comes to replacing or redesigning a light fixture, many people turn to LEDs for their efficiency benefits over traditional sources. While LEDs are significantly more efficient than a filament bulb, they still generate heat that must be considered in the overall design. What does heat do to your LEDs, and what can you do about it?

How Much Heat?

A 100W tungsten filament bulb is about 10% efficient, meaning it only generates 10W of light energy for every 90W of heat energy.  That “light energy” is what designers need to match with other sources to get an equivalent amount of light, which is why high-efficiency bulbs can call themselves equivalent to a 100W bulb while only actually consuming a fraction of that energy.  While LEDs themselves can be extremely efficient, other components of the system like the driver or lens tend to reduce the efficiency of an LED light bulb to about 70%.  That is an incredibly energy saving over the 10% efficient filament bulb, but still means that about 30% of the power consumed by the bulb gets emitted as heat rather than light. 

 

Light Source

Input Power

Light Energy

Heat Energy

Tungsten Bulb

100W

10W

90W

LED Bulb

100W

70W

30W

LED Bulb

15W

10.5W

4.5W

 

How Does That Matter?

When a filament bulb generates heat, that heat aids the efficiency of the bulb by lowering the electrical power required to heat the filament to the point of emitting light.  LEDs emit light (and heat) based on the PN junction of the diode, which becomes less efficient as heat is introduced.  The forward voltage of the LED is indicative of the size of the energy gap an electron must achieve before it can be absorbed into the other side of the diode junction and emit light.  When heat is introduced, the electrons start at a higher energy level, and the voltage of the LED decreases.  LEDs are constant current devices and are not (typically) driven in a way that allows them to compensate for this voltage drop by drawing more current.  The LEDs just fall backwards along their V-I curve and emit less light as the temperature increases.

Why Not Use Constant Voltage?

Most LED drivers are constant current and limit the LEDs as described above.  It seems like a good solution would be to move to constant voltage control, which would allow the LEDs to draw more current as the voltage decreases.  This works mathematically, but actually creates a positive feedback loop in the diode junction that causes the LED to draw more and more current, generating more and more heat until it burns up. Even if the power supply has a current limit, constant voltage supplies are not designed to actually regulate at that limit and will likely stop functioning once their limit is exceeded.  One way or another, something in your system will fail. 

Can We Compensate?

The compromise between a thermal runaway situation and dimming LEDs is to use temperature-sensitive driver chips.

参阅相关产品

CL25N8-G

Microchip Technology LED 驱动器 查看

These drivers are often placed in series with each string of LEDs in a fixture to balance parallel strings and compensate the allowed current based on fixture temperature.  These chips will limit the current to a range that is deemed safe for the LEDs to prevent runaway but also appropriately increase the current to compensate for lower voltages.  While some power supplies claim to compensate for temperature, that is only valuable in a situation where the ambient temperature fluctuates.  The temperature of concern is typically very localized to the LEDs and can only be properly regulated by a chip that is on the same board and in the same situation as the LEDs themselves. 

The easiest answer is usually to allow proper heat sinking for the LED board and not allow the junction temperature to reach the point where LED dimming is noticeable. 

Without a comparison point, our eyes typically do not detect dimming until the light source is at 50% of the original brightness, so things have to get pretty hot for the average application to be affected by the dimming effect.  If you use thermal vias, generous copper pours, metal heat sinks, and fans where appropriate, the typical temperature rise of an LED system should not practically affect your output.  If you do notice the fixture dimming, be sure to let it cool down before grabbing it to investigate – it will be hot!

相关新闻文章

最新消息

Sorry, your filter selection returned no results.

请仔细阅读我们近期更改的隐私政策。当按下确认键时,您已了解并同意艾睿电子的隐私政策和用户协议。

本网站需使用cookies以改善用户您的体验并进一步改进我们的网站。此处阅读了解关于网站cookies的使用以及如何禁用cookies。网页cookies和追踪功能或許用于市场分析。当您按下同意按钮,您已经了解并同意在您的设备上接受cookies,并给予网站追踪权限。更多关于如何取消网站cookies及追踪的信息,请点击下方“阅读更多”。尽管同意启用cookies追踪与否取决用户意愿,取消网页cookies及追踪可能导致网站运作或显示异常,亦或导致相关推荐广告减少。

我们尊重您的隐私。请在此阅读我们的隐私政策。