FPGA basics: Architecture, applications and uses

The Field Programmable Gate Array (FPGA) is an integrated circuit that consists of internal hardware blocks with user-programmable interconnects to customize operation for a specific application.

What is FPGA?

Field Programmable Gate Array (FPGA) is an integrated circuit that consists of internal hardware blocks with user-programmable interconnects to customize operation for a specific application. The interconnects can readily be reprogrammed, allowing an FPGA to accommodate changes to a design or even support a new application during the lifetime of the part.

The FPGA has its roots in earlier devices such as programmable read-only memories (PROMs) and programmable logic devices (PLDs). These devices could be programmed either at the factory or in the field, but they used fuse technology (hence, the expression “burning a PROM”) and could not be changed once programmed. In contrast, FPGA stores its configuration information in a re-programmable medium such as static RAM (SRAM) or flash memory. FPGA manufacturers include Intel, Lattice SemiconductorMicrochip Technology and Microsemi.

FPGA architecture

A basic FPGA architecture (Figure 1) consists of thousands of fundamental elements called configurable logic blocks (CLBs) surrounded by a system of programmable interconnects, called a fabric, that routes signals between CLBs. Input/output (I/O) blocks interface between the FPGA and external devices.

Depending on the manufacturer, the CLB may also be referred to as a logic block (LB), a logic element (LE) or a logic cell (LC).

Body Image 1-FPGA-Basics-architecture-applications-and-uses
Figure 1: The fundamental FPGA architecture (Image Source: National Instruments)

An individual CLB (Figure 2) is made up of several logic blocks. A lookup table (LUT) is a characteristic feature of an FPGA. An LUT stores a predefined list of logic outputs for any combination of inputs: LUTs with four to six input bits are widely used. Standard logic functions such as multiplexers (mux), full adders (FAs) and flip-flops are also common.

Body Image 2-FPGA-Basics-architecture-applications-and-uses
Figure 2: A simplified CLB: The four-input LUT is formed from two three-input units. (Image source: Wikipedia)

The number and arrangement of components in the CLB varies by device; the simplified example in Figure 2 contains two three-input LUTs (1), an FA (3) and a D-type flip-flop (5), plus a standard mux (2) and two muxes, (4) and (6), that are configured during FPGA programming.

This simplified CLB has two modes of operation. In normal mode, the LUTs are combined with Mux 2 to form a four-input LUT; in arithmetic mode, the LUT outputs are fed as inputs to the FA together with a carry input from another CLB. Mux 4 selects between the FA output or the LUT output. Mux 6 determines whether the operation is asynchronous or synchronized to the FPGA clock via the D flip-flop.

Current-generation FPGAs include more complex CLBs capable of multiple operations with a single block; CLBs can combine for more complex operations such as multipliers, registers, counters and even digital signal processing (DSP) functions.

CPLD vs FPGA

Originally, FPGAs included the blocks in Figure 1 and little else, but now designers can choose from products with a large range of features. Less complex devices such as simple programmable logic devices (SPLDs) and complex programmable logic devices (CPLDs) bridge the gap between discrete logic devices and entry-level FPGAs.

Entry-level FPGAs emphasize low power consumption, low logic density and low complexity per chip. Higher-function devices add functional blocks dedicated to specific functions: Examples include clock management components, phase-locked loops (PLLs), high-speed serializers and deserializers, Ethernet MACs, PCI express controllers and high-speed transceivers. These blocks can either be implemented with CLBs—termed soft IP—or designed as separate circuits; i.e., hard IP. Hard IP blocks gain performance at the expense of reconfigurability.

At the high end, the FPGA product family includes complex system-on-chip (SoC) parts that integrate the FPGA architecture, hard IP and a microprocessor CPU core into a single component. Compared to separate devices, a SoC FPGA provides higher integration, lower power, smaller board size and higher-bandwidth communication between the core and other blocks.

SoC FPGAs

SoC FPGAs include a wide range of processing capabilities to suit different applications. A low-cost, low-power SoC FPGA such as Intel’s Cyclone V, for example, targets high-volume applications such as industrial motor control drives, protocol bridging, video processing cards and handheld devices. The device (Figure 3) has two distinct parts: the FPGA portion and a hard processor system (HPS) based around a single- or dual-core 32-bit Arm Cortex-A9 MPCORE running at 925 MHz. Each part contains its own set of peripherals, which includes hard IP from third-party vendors.

Body Image 3-FPGA-Basics-architecture-applications-and-uses
Figure 3: The Cyclone V SoC internal block diagram (Image Source: Cornell University)

At the other end of the scale, the Stratix 10 SX targets high-performance applications in communications, data center acceleration, high-performance computing (HPC), radar processing and ASIC prototyping; that FPGA includes a quad-core 64-bit Arm Cortex-A53 running at up to 1.5 GHz.

FPGA design

How do we transform this collection of thousands of hardware blocks into the correct configuration to execute the application? An FPGA-based design begins by defining the required computing tasks in the development tool, then compiling them into a configuration file that contains information on how to hook up the CLBs and other modules. The process is similar to a software development cycle except that the goal is to architect the hardware itself rather than a set of instructions to run on a predefined hardware platform.

Designers have traditionally used a hardware description language (HDL) such as VHDL (Figure 4) or Verilog to design the FPGA configuration.

Body Image 4-FPGA-Basics-architecture-applications-and-uses
Figure 4: Sample VHDL code for a signed adder (Image Source: Wikipedia)

Once the FPGA design has been created and verified using HDL, the compiler takes the text-based file and generates a configuration file that contains information on how the components should be wired together. Even if the HDL code has no errors, choosing the wrong FPGA may still cause the compilation to failfor example, the FPGA runs out of a specific resource type or the compiler cannot create the required routes between components.

One challenge with an HDL approach is that configuring an FPGA requires both coding skills and a detailed knowledge of the underlying hardware, and the required expertise is not widely available.

As a result, vendors are offering software development kits (SDKs) that allow designers to develop FPGA solutions in popular high-level languages such as C/C++, Python and OpenCL. High-level synthesis (HLS) design tools are also available; these run on a framework such as National Instrument’s LabVIEW and feature graphical block diagrams instead of lines of code.

FPGA uses: An attractive choice for certain applications

The ability to configure the hardware of the FPGA, reconfigure it when needed and optimize it for a particular set of functions makes the FPGA an attractive option in many applications.

FPGAs are often used to provide a custom solution in situations in which developing an ASIC would be too expensive or time-consuming. An FPGA application can be configured in hours or days instead of months. Of course, the flexibility of the FPGA comes at a price: An FPGA is likely to be slower, require more PCB area and consume more power than an equivalent ASIC.

Even when an ASIC will be designed for high-volume production, FPGAs are widely used for system validation, including pre-silicon validation, post-silicon validation and firmware development. This allows manufacturers to validate their design before the chip is produced in the factory.

FPGA applications

Many applications rely on the parallel execution of identical operations; the ability to configure the FPGA’s CLBs into hundreds or thousands of identical processing blocks has applications in image processing, artificial intelligence (AI), data center hardware accelerators, enterprise networking and automotive advanced driver assistance systems (ADAS).

Many of these application areas are changing very quickly as requirements evolve and new protocols and standards are adopted. FPGAs enable manufacturers to implement systems that can be updated when necessary.

A good example of FPGA use is high-speed search: Microsoft is using FPGAs in its data centers to run Bing search algorithms. The FPGA can change to support new algorithms as they are created. If needs change, the design can be repurposed to run simulation or modeling routines in an HPC application. This flexibility is difficult or impossible to achieve with an ASIC.

Other FPGA uses include aerospace and defense, medical electronics, digital television, consumer electronics, industrial motor control, scientific instruments, cybersecurity systems and wireless communications.

FPGA history: What comes next?

With these emerging applications, the FPGA market is growing at a healthy clip: It was valued at $5.34 billion in 2016 and is expected to grow to $9.50 billion in 2023, according to industry researchers MarketsandMarkets. That’s a compound annual growth rate (CAGR) of 8.5 percent, compared to a CAGR of about 2 percent for the much larger ($74 billion) general microprocessor market.

The exponential growth of data, and the emergence of fast-changing fields such as AI, machine learning, HPC and genomics, require architectures that are fast, flexible and adaptable. FPGAs are well-positioned to take advantage of these new opportunities.


相关新闻文章

最新消息

Sorry, your filter selection returned no results.

请仔细阅读我们近期更改的隐私政策。当按下确认键时,您已了解并同意艾睿电子的隐私政策和用户协议。

本网站需使用cookies以改善用户您的体验并进一步改进我们的网站。此处阅读了解关于网站cookies的使用以及如何禁用cookies。网页cookies和追踪功能或許用于市场分析。当您按下同意按钮,您已经了解并同意在您的设备上接受cookies,并给予网站追踪权限。更多关于如何取消网站cookies及追踪的信息,请点击下方“阅读更多”。尽管同意启用cookies追踪与否取决用户意愿,取消网页cookies及追踪可能导致网站运作或显示异常,亦或导致相关推荐广告减少。

我们尊重您的隐私。请在此阅读我们的隐私政策。