RECOM Demo: R-78 Series

As an alternative to a legacy linear regulator, RECOM has introduced a series of low cost, high performance switching regulators with an identical footprint for drop-in implementation. Specifically, the R-78 series is universal for any application and is even ready for use in the IoT where power loss is a substantial concern. To learn more about the advantages of RECOM’s switching regulator, watch the above video that highlights the capabilities of the R-78 series.

To evaluate the difference of the R-78 series, over the outdated LM78 linear regulator series, this demonstration specifically compares the input and output voltages and currents between the two different components, as well as points out some of the key operational differences. Right away, you can see that the part count of the LM78 is several components including a heat sink, thermal paste, nuts and bolts and, of course, the extra labor – while the R-78 solution’s part count is a single part number.

관련 상품 참조

R-78E5.0-0.5

RECOM Power GmbH DC to DC Converter and Switching Regulator Module 보기

It’s important to understand what’s going on here and how a linear regulator actually works. A linear regulator is simply a voltage regulator, so the input current and output current are always the same. A switching regulator, on the other hand, is a power converter. So as the input voltage increases, the input current will decrease. This has the advantage of significantly reducing power losses resulting in excessive heat in the application. Our switching regulators run at efficiencies above 90% regardless of the input voltage.

관련 상품 참조

R-78E5.0-1.0

RECOM Power GmbH DC to DC Converter and Switching Regulator Module 보기

Let’s have a look at what that really means in practice. If I configure the linear regulator to produce 5V out, you see that the input and output current are the same, meaning that the power loss is quite high. You can see in the thermal images that this will result in a significant amount of heat generated, reducing the lifetime of the entire application. When replacing the linear regulator with one of RECOM’s R-78 switching regulators with the same load, you can see that the input voltage is still the same, but the input current drawn is much less. This results in a greater amount of power being transferred to the load as opposed to being dissipated as heat. Taking a look at the thermal image, we can see that the solution is running much cooler.

관련 상품 참조

R-78E3.3-1.0

RECOM Power GmbH DC to DC Converter and Switching Regulator Module 보기

The Total Cost of Ownership of a design has to be considered in this case. While the initial BOM of the linear regulator may be slightly cheaper than an R-78, other life-long factors play a role in overall cost. The heat dissipation that reduces the lifetime of the nearby components needs to be considered. Plus, the part count is reduced, which simplifies sourcing and BOM management. Finally, as the modules are pre-certified and EMC tested, time-to-market is greatly improved over creating a discrete solution with thermal management integrated.

관련 상품 참조

R-78E3.3-0.5

RECOM Power GmbH DC to DC Converter and Switching Regulator Module 보기

관련 동영상

최신 동영상

죄송합니다. 선택한 필터와 일치하는 결과가 없습니다.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.