What is an op-amp? Operations amplifier circuits explained

What is an op-amp?

You’ve probably heard the term “op-amp” thrown around in electronics jargon, but what are these components? Operations amplifiers — op-amps for short, are integrated circuits, constructed mostly out of transistors and resistors. These integrated circuits multiply an input signal to a larger output. You can use these components with voltage and current in both DC and AC circuits.

Karl D. Swartzel Jr. invented the first op-amp in 1967, and he originally conceived them to do mathematical operations in analog computers — thus the “operation” part of their name. We now use op-amps in many other applications, and they form the basis of many modern analog electronic circuits.

What does an op-amp do?

At their most basic, an op-amp takes a differential signal — the voltage difference between the V+ and V- pins — and outputs a voltage proportional to this difference through the Vs+ and Vs- power supply. You can see the Vs+ and Vs- power supply in the image below. Many simplified representations of this component omit the Vs+ and Vs- nodes and only show the V+, V-, and Vout pins.

0918_Opamp2_3

Fig 1: Op-amp circuit diagram symbol

This open loop operation typically results in a device gain (known as the open loop gain or AOL) of 100,000 or more. Even a tiny difference in the voltage on the non-inverting (+) and inverting (-) pins works out to an output of nearly the supply voltage when the + input voltage is greater than the — input. This configuration acts as a comparator, turning a potentially varying input signal to a steady on/off output.

Closed-loop op-amps

We usually use op-amps in a closed-loop configuration, with the output voltage feeding back (as feedback) into the inverting input to form a more controllable signal amplification. The simplest way to accomplish this is to use a buffer circuit, where the output feeds back into the inverting input with no resistors or other components.

To understand how this operation works, here are the two op-amp golden rules:

1. The output attempts to make the voltage difference between the inputs zero

2. The inputs draw no current

Here’s how to construct a closed-loop op-amp:

1. Feed the input voltage into the + input

2. Connect the – to the amplifier’s output

3. The output should go to the same value as the + input to keep both equal

This configuration can be useful for weak signals that require an amplified current before triggering another device.

0918_Opamp3_2

Fig 2: Op-amp with a feedback loop and voltage divider

In the image above, we took the closed-loop configuration concept further. If you want the output voltage to be a different value than the input, add a pair of resistors to form a voltage divider for the feedback loop. Amplification is thus based on the voltage we see at the node between these two resistors, calculated by the following formula:

Vin- = Vout * Rg / (Rg + Rf)

By this formula’s logic, we can state the following:

Vout = Vin- * (Rg + Rf)/Rg

Vout = Vin- *(1 + Rf/Rg)

The 1 + Rf/Rg term is the closed-loop gain (ACL) of the circuit. If the resistors stay the same as Vin increases or decreases, Vout will vary proportionally by a factor of ACL up to the supply voltage.

Other configurations are also available, including feedback to the inverting pin, and using a voltage divider circuit to allow an op-amp to provide negative and positive voltage.

Op-amp differences

Beyond being able to connect and use op-amps in different ways, you can select op-amps with a variety of specifications to fit your application, including variations on:

- Offset voltage

- Maxim supply voltage

- Gain-bandwidth product

You can find a wide variety of other op-amps available in different packages and with different specifications. Take, for example, the LTC2063 from Analog Devices, a low-supply current op-amp available in a variety of packages -- great for a variety of applications.


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.