Active vs. Passive Components in Electronics

One key factor that differentiates types of electronic components from each other is whether they are passive or active. However, many people are unsure of exactly what that difference entails.

Difference Between Active and Passive Components

What are active components? These components are parts of a circuit that rely on an external power source to control or modify electrical signals. Active components such as transistors and silicon-controlled rectifiers (SCRs) use electricity to control electricity.

What are passive components? Like resistors, transformers, and diodes don’t need an external power source to function. These components use some other property to control the electrical signal. As a result, they only require the current traveling through the connected circuit. Resistors impede the flow of electrons without introducing more electricity into the system.

Browse Arrow.com's featured passive components for sale.

Active and Passive Components in Electronics

While their superficial differences are easy to articulate, active and passive components tap into a more fundamental premise of electronics design: the conservation of energy. Because energy cannot be created or destroyed, and real-world machines cannot operate at 100% efficiency, all real-world passive circuits will lose some amount of power in use. We witness this net loss through the decline in power between the input and output signals and a decrease in amplification.

In practical terms, active components are useful because they often enable a small amount of electricity to control a larger quantity. In other words, one of the major benefits of active devices like transistors, tunnel diodes, and vacuum tubes is that they allow amplification. Whether they influence the flow of electricity by using voltage or current as the control, active components allow a small input to generate a matching, larger output.

Electronic Components Explained

Active components such as amplifiers, vacuum tubes, and transistors make use of an external power source to add power to a system. They use one electrical signal to control another and are required for the circuit to be considered “electronic.” Technically, we don’t define circuits without active components as “electronics,” but in practice, virtually all electronic circuits have passive components as well. Passive components like resistors, inductors, and capacitors influence the flow of power but do not require an external power source to function.

You will likely find both kinds of components in every electronic device.

 

Overstock AV Page Footer 560x140 2 1 1

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.