Bluetooth® Low Energy (BLE) Technology Development Trends

With the integration of the Mesh and Beacon application technologies, the application of BLE technology is promising. Learn more about how the MBN52832 Bluetooth® low energy module by Murata can offer an energy-efficient option for your IoT products.

Bluetooth Low Energy Technology allows for longer operation time for battery-powered products 

Bluetooth ®Low Energy, also known as Bluetooth® LE, or BLE, is a Wireless PAN or WPAN technology designed and sold by Bluetooth SIG, which is a new mode of application suitable for medical and health care, sports and health, Beacon, security, family entertainment and other areas. As compared with the Classic Bluetooth, the BLE yields the same performance in communication within the same range with efficient use of energy and low cost at significant level. The low energy feature of BLE allows an application to wearables and IoT devices. With the use of a button cell, it allows for operation for months and even years. It is compact in size and low cost, and is compatible with most cell phones, tablet PCs or even PCs. According to the forecast of Bluetooth SIG, there will be more than 90% of the smart phones with Bluetooth feature support BLE in 2018.

BLE technology starts to support the Mesh network. The function of the brand new Mesh provides many-to-many (m:n) device communications and specifically upgrades the communication performance for the installation of wide range network. As compared with the P2P communications of the Bluetooth in the past, which is a communication network connecting 2 single node points, Mesh could make all devices in the network as a single node point so that each node point could connect with one another and the range of transmission broadened. In addition, each device can connect to one another to make it possible for using in the automation of building and sensor network, which requires many or even thousands of devices as a solution for the IoT for transmission in a stable and secure environment. 

Furthermore, the BLE also supports the micro positioning technology of Beacon. In other words, Beacon is just like a lighthouse broadcasting signals without a pause. When a cell phone enters the lighting range of the lighthouse, Beacon will transmit series of codes for the cell phone. After detecting the codes by the App, the cell phone will trigger series of actions. It may be information downloaded from the cloud or the activation of other Apps or interlock devices. Beacon features micro positioning function in higher precision than GPS and could be used indoor for identifying any cell phone entering the transmission range explicitly. This could be used in digital marketing, electronic payment, and indoor positioning. 

The MBN52832 Bluetooth® low energy module presented by Murata is a product that can provide ultra-low energy interconnection in the course of data transmission. This module put a Nordic BLE chip, R/F front end and crystal into a compact shape with a built-in 64KM RAM and 512KB flash ARM Cortex M4 core, which provides a high performance engine and abundance of ports for various IoT, such as sensor network and device control. With accredited R/F, this module significantly helps to reduce the burden of the system designer and condense the time to market, and is an ideal solution for many smart devices, medical and health care devices, and M2M application. 

The MBN52832 Bluetooth® BLE module supports the Bluetooth® v5, ANT, and NFC Tag. The built-in Nordic nRF52832 Bluetooth Smart® chip is sealed with LGA and the dimension is only 7.4 x 7.0 x 0.9 mm, which supports PCB antennae on board, and also connects to external antennae through a connection point. Under the LDO mode for connection with the connector of antennae, the maximum transmission capacity is +4.0dBm, and the sensitivity for receiving could be as high as -93dBm @ 1Mbps (LDO mode), and the power is 7mA @ 3.5dBm during transmission (DCDC mode), and 6mA at receiving (DCDC mode). The main control connector supports UART and SPI and also 20 GPIO, 5 ADC, UART, SPI, I2C, and PWM and Debug SWD. This is suitable for home automation, proximity service, building automation, medical/health care, and Beacon application. 

Murata also launched the MBN52832 development kit and the Nordic nRF52 software development kit could be used for improving the speed of development of the application. The evaluation board could support the same J-Link USB-SWD and USB-UART as provided by the nRF52 development kit to simplify debugging and development process. 

The business opportunity for the wide range of application of the IoT is promising. With the integration of the Mesh and Beacon application technologies, the application of the BLE technology will thrive. The MBN52832 Bluetooth® low energy module presented by Murata provides full function and compact size that make it the excellent choice in your development of IoT related products.
 

관련 상품 참조

WSM-BL241-ADA-008DK

Murata Manufacturing 보기

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.