Bel Power Solutions: The Future of Fuses

When is a Fuse Not a Fuse?

This article by Bel Power Solutions explores how a fuse is traditionally used within an electronic design and how it will need to change in a world of ever-increasing miniaturization. Learn more about the positive temperature coefficient (PTC) fuses offered by Bel and how they will improve the future of fuse design.

A traditional fuse consists of a piece of wire or other conductive link with a known current-carrying capacity placed in series with an electric circuit. The fuse functions solely as a safety device that is designed to melt and permanently interrupt further current flow.  By operating, fuses protect circuits from damage caused by overload or short circuit current, thereby preventing overheating and even fire if a fault condition should occur.
0818_BEL_Article_VI_Circuit Protection_When is a Fuse Not a Fuse
Depending on the circuit being protected, fuses can be rated from a few mA in small consumer electronic products to hundreds of Amps in industrial applications.  Current rating alone is not sufficient to specify a fuse for a particular application; fuses are also rated for voltage, AC and/or DC.  The voltage rating is a maximum and cannot be exceeded.  Once the fuse operates, there is no chance of arcing across the fuse.  Depending on whether the load is resistive or reactive, fuses are available that are designed to blow “fast” in the event of a current overload, or designed to allow a brief overload for a defined short time period before blowing, often called “time delay” or “slow” fuses.  Fuses also need to be selected according to circuit parameters.  Certain semiconductor circuits require a fuse to clear very quickly to avoid possible significant/expensive component damage. Conversely, highly inductive or capacitive circuits such as power supplies may generate brief inrush surges at “power-up”, where the circuit current is well above a fuse’s rating for a very short time. Circuits like this require a “Time Lag” or “Slow Blow” type fuse to allow it to ride out these brief but normal surges without causing what’s known as “nuisance clearing”.  This is also true for motor and transformer in-rush currents.

One thing all fuses have in common is that they are “one-time” devices. When any conventional fuse is forced to clear, installing an exact replacement after repairing the underlying fault is the only way to repower the protected circuit. But as electronic systems continue to shrink and evolve, the single use nature of the fuse has come under increasing pressure.

0818_BEL_VI_Article_When is a Fuse Not a Fuse

Apart from USB interfaces, other applications that benefit from PTC protection include:

-- IEEE 1394 Firewire
-- Power over Ethernet (PoE)
-- Lithium Ion Battery Packs
-- Battery Charger Circuits
-- PC Peripherals
-- Disk Drive Interface
-- Transformer
-- Telecom Line Interface
-- Motors
-- Power Supplies
-- Heaters
-- Toys

READ FULL WHITE PAPER

SHOP BEL'S RANGE OF FUSES

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.