Electrical Connector Reliability: Connector Types & Concerns

게시자

Reliability is a term that's commonly used in our daily lives. Some cars are sought after for their high reliability; others avoided for the opposite reason. Reliability is a desired quality in a friend, a boss, a paycheck; yet its precise meaning can vary depending on the context.

When it comes to electrical connectors, though, reliability has a precise definition. In plain language: Reliability is “the probability that a connector will perform as required for a desired period of time during which it is subjected to a given set of environmental and/or mechanical stresses.”

This definition states that there is a defined set of performance levels that must be maintained for a defined time while the connector is operating under the defined set of conditions. Since any or all of these can change with the application, a connector reliability specification is a function of all three.

What is a Connector? Construction Basics

So what exactly is a connector, anyway? One general definition of a connector is that a connector “provides a separable connection between two elements of an electronic system without unacceptable signal distortion or power loss.”

The two key parts to this definition are “separable” and “unacceptable” performance loss, both of which depend on the connector application and its electrical and environmental requirements.

Below is a simplified drawing of a connector, showing the main components together with a close-up of the contact finish and interface.

 0715_Basics of Connector Reliability_inarticle

Figure 1:  Connector Electrical Components. (Source: TE Connectivity)

The electrical portion for each connection consists of a connector pin and a mating contact spring, which exerts a mechanical force on its associated pin to maintain electrical continuity.  The pins and springs are each contained within a rigid shell; the two shells mate together, typically with a key mechanism to ensure correct orientation.

Electrical Connector Failure Modes and Mechanisms

If nothing ever failed, connector reliability would be a non-issue. When looking at what can go wrong in a connector, though, we can distinguish between failure modes and failure mechanisms. A failure mode is the particular way that the connector could fail functionally compared to the application requirements—for example, contact resistance that exceeds the specification or unacceptably high insertion force are both failure modes. A failure mechanism is a cause of a failure mode—for example, mechanical vibration and electrical overstress are both mechanisms that may lead to failure.

Here are some common failure mechanisms and their typical failure modes:

Failure Mechanism

Typical Failure Mode

Mechanical stress: vibration, shock, sustained bending stresses, repeated mating and un-mating

Damage to connector shell and key; mis-mating and circuit damage; excessive wear leading to intermittent or open connections

Excessive high temperatures

Insulation breakdown; increased contact resistance

Excessive low temperatures

Damage to non-metallic components

High humidity

Increased contact resistance, corrosion

Determining the Best Electrical Connectors: Measuring Connector Reliability

How do we develop reliability metrics for connectors? In most fields, reliability is determined using one of three available methods:

1)      Actual use: monitors the performance of the product in service.

2)      Predictive: predicts the reliability based on a model developed through empirical studies and/or testing.

3)      Physics-of-failure: identifies potential failure mechanisms and develops an accelerated failure-testing program to induce failures and hence predict real-world performance.

For a number of reasons, though, these techniques are not suitable for connectors. Standard statistical metrics such as MTTF and MTBF (Mean Time To Failure and Mean Time Between Failures, respectively) are difficult to obtain. Instead, connector manufacturers give a set of guaranteed electrical and mechanical operating specifications and a set of qualification tests that sample products have passed.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.