Rev Up Your Motor Control with Current Sensing

0324-Picture-of-electronic-components-from-Analog-Devices-Header-820x410

The efficiency of electric drive motors in industrial applications is only as good as the circuits that control them. Critical to motor control is a power electronics block, and critical to the power electronics block are sensors that gauge current, voltage and position. In this article from Analog Devices, explore how current feedback and DC bus voltage measurement can become part of your electric motor control circuit.

Power inverters and power electronics blocks sit at the heart of every motor drive. They provide the controllable power element that enables modulation of the power to the motor in order that its speed and torque can be precisely controlled. Control of the inverter is thus critical to the whole operation of the drive.

For any closed loop control system we generally need a set point (e.g. the desired operating point) and a measured variable (known as feedback) to compare it with, in order that the control loop can respond to any difference between these. In drives, the key measured variables are typically motor current and motor position. Other variables such as DC bus voltage are helpful to the operation of the control loop. Let’s examine the current feedback and the DC bus voltage measurement as these occur within the inverter stage, as indicated again in our architecture diagram below.


0324- Servo-drive-architecture-diagram
Figure 1: Servo drive architecture diagram

What is important in the current feedback path is that the measurement is synchronized with the PWM cycle in order that no high-frequency switching current ripple is introduced into the feedback path. This requires precise timing of the current sampling in order that it is sampled at the midpoint of the waveform. At this point in the waveform, the instantaneous current is equal to the PWM cycle average, and the measurement will not include any of the PWM switching ripple current.

This is illustrated in Figure 2 in a simplified fashion – where the sampling point on the phase current waveform is shown, along with its relative alignment to the PWM high-side switching waveform, and the switching period Tsw. The PWM_SYNC pulse indicates the point at which sampling of the current must be triggered in this scenario (this can also be understood as the center-point of the digital filter in the case where sigma-delta ADC type sampling is used which is not a single-point sample, see [1]).


0324-Motor-current-mid-point-sampling
Figure 2: Motor current mid-point sampling

Simultaneous sampling of at least two phases is also required, and usually 14-16 bit measurement resolution is sufficient, with microsecond-level latency so that the control loop can respond within the PWM cycle time (Tsw) or in half the cycle time for higher performance control loops.

There are a few different ways to implement the current measurement – these are shown in Figure 3, and described in the table below, along with some example part numbers to implement the scheme for a 20A application. The most accurate location to measure the motor current is in the actual motor phases, i.e the output lines of the inverter – but this usually requires galvanic isolation, due to the high voltage present at these nodes. Motor current measurements can be inferred from other locations such as inverter leg, and DC bus positive or negative rail – however these measurement locations, while potentially cheaper to implement have other disadvantages associated with them.


0324-Current-feedback-options
Figure 3: Current feedback options

Description Comments Example Parts (20A)
1 Series shunt resistor + high common mode voltage (CMV) op-amp + simultaneous sampling ADC (SSADC) Usually used in < 100V applications, as high CMV op-amps are usually rated for this range CFN1206AFXR010 (Bourns)
AD8410 (ADI)
MAX11195(ADI)
2 Series shunt resistor + isolated ADC Best solution for noise immunity, size and performance. Bitstream output – needs digital filter CFN1206AFXR010 (Bourns)
ADuM7701-8
3 Isolated current sensor + opamp + SSADC Good solution for higher current levels where shunt resistors become too inefficient HMSR 20-SMS (LEM)
AD8515 (ADI)
AD7380 (ADI)
4 Leg shunt resistor + opamp + SSADC Cheapest solution as no isolation needed if controller is DC bus grounded. Less accurate than in-phase shunt CFN1206AFXR010 (Bourns)
MAX4477 (ADI)
MAX11195 (ADI)

High fidelity, precision, current feedback is important to the overall control loop of the inverter. It has a big impact on the overall control bandwidth and torque ripple. Bandwidth translates into faster transient performance of the motor control – which can be very important in applications like pick-and-place machines. Torque ripple translates into effects such as machining quality and finish tolerance in applications like grinding, cutting and polishing.

While current feedback is the most important feedback variable from the inverter to the controller, DC bus voltage can also be valuable as a control feedforward variable. It is not used as a controlled quantity, but because variation in the DC bus voltage impacts the dynamics of the current control loop it can be used as a feedforward variable, which improves the dynamics of the overall current controller. The end result of this is as shown in Figure 4.


0324-Current-Controller-Block-Diagram
Figure 4: Current controller block diagram

The DC bus voltage sense signal can be derived directly from a voltage divider across the DC bus if the controller ground is at the DC bus negative, or else by using an isolated amplifier or ADC (such as the ADuM7701 mentioned previously) connected to the voltage divider output.



See related product

AD7380BCPZ-RL7

Analog Devices Analog to Digital Converters - ADCs View

See related product

MAX11192EVKIT#

Analog Devices Data Conversion Development Boards and Kits View

See related product

MAX11192ATE+T

Analog Devices Analog to Digital Converters - ADCs View

See related product

MAX11195EVKIT#

Analog Devices Data Conversion Development Boards and Kits View

See related product

MAX11195ATE+T

Analog Devices Analog to Digital Converters - ADCs View

See related product

MAX11198EVKIT#

Analog Devices Data Conversion Development Boards and Kits View

See related product

MAX11198ATE+T

Analog Devices Analog to Digital Converters - ADCs View

AD8410

CFN1206AFXR010

MAX11195

ADuM7701-8

AD8515

MAX4477


Related news articles

Latest News

Sorry, your filter selection returned no results.

We've updated our privacy policy. Please take a moment to review these changes. By clicking I Agree to Arrow Electronics Terms Of Use  and have read and understand the Privacy Policy and Cookie Policy.

Our website places cookies on your device to improve your experience and to improve our site. Read more about the cookies we use and how to disable them here. Cookies and tracking technologies may be used for marketing purposes.
By clicking “Accept”, you are consenting to placement of cookies on your device and to our use of tracking technologies. Click “Read More” below for more information and instructions on how to disable cookies and tracking technologies. While acceptance of cookies and tracking technologies is voluntary, disabling them may result in the website not working properly, and certain advertisements may be less relevant to you.
We respect your privacy. Read our privacy policy here