Arrow Electronic Components Online

Saving the planet one motor at a time

Energy Management26 Mar 2024
A row of blue industrial motors is displayed in a manufacturing setting
View all articles

Electric motors have been commonplace in manufacturing applications since at least the late 1800s. Compared to prior methods, they offered numerous advantages, including instantaneous torque, higher controllability and lower maintenance. While motor technology has certainly improved over the years, there are still large advances yet to be made. This article from Analog Devices explores how the process of making electric motors more efficient can aid in reducing the emissions contributing to climate change.

The Paris Agreement in 2015 set out a plan to limit global warming to 1.5°C by 2050. Meeting the 1.5°C target in 2050 requires an approximately 70% reduction in CO2 emissions from 2018 levels. The current trajectory of global warming has the potential to cause major economic, societal, and environmental disruptions. The world has already warmed by 1.1°C and experts say that it is likely to breach 1.5°C in the 2030s.

Figure 1 outlines a path to the 1.5°C target by reducing CO2 emissions to under 10 Gt CO2, as covered in World Energy Outlook 2019. In that report, the International Energy Agency (IEA) looks at two scenarios for the trajectory of global emissions. The first is the Stated Policies Scenario, which estimates emissions based on publicly announced government policies. The second is the Sustainable Development Scenario, which looks at additional paths to mitigating emissions. The largest opportunity to reduce CO2 emissions as part of the IEA’s Sustainable Development Scenario is gains in energy efficiency, accounting for 37% of the Sustainable Development Scenario’s reductions when compared to the Stated Policies scenario With 25% of CO2 emissions coming from industry in 2022 [2], accelerating industrial energy efficiency investments will be an important part of the path to net zero emissions in 2050.

Figure 1 outlines a path to the 1.5°C target by reducing CO2 emissions to under 10 Gt CO2, as covered in World Energy Outlook 2019. In that report, the International Energy Agency (IEA) looks at two scenarios for the trajectory of global emissions.

Figure 1: Path to CO2 emissions reductions

Why industrial motors matter

The global electricity supply in 2022 was 28,642 terawatt-hours, contributing 13.2 Gt of carbon emissions. Industry consumes an estimated 30% of global electricity and within industry, electric motors make up approximately 70% of electricity consumption. Clearly, the efficiency of these components is a potentially critical contribution to the efficiency savings identified in Figure 1. The most basic and lowest efficiency motion solutions are based on direct AC grid-connected 3-phase motors that use switchgear to provide on/off control and basic protection. These motion solutions run at a relatively fixed speed, independent of any load variation. Adjustments in output variables (such as fluid flow in pumps and fans) are implemented with mechanical controls such as throttles, dampers, and valves, whereas significant speed changes are implemented with gears.

The addition of a rectifier, DC bus, and a 3-phase inverter stage, as illustrated in Figure 3(b) creates an inverter with variable frequency and a variable voltage output that is applied to the motor to enable variable speed control.

Figure 2: The part played by Industrial Motors in global energy usage

The addition of a rectifier, DC bus, and a 3-phase inverter stage, as illustrated in Figure 3(b) creates an inverter with variable frequency and a variable voltage output that is applied to the motor to enable variable speed control. This inverter-driven motor significantly reduces system energy consumption by running the motor at the optimum speed for the load and application. Examples include higher-efficiency pumps and fans. When added to the existing motor of a pump, fan, or compressor, an inverter can potentially reduce power consumption between 25% and 60%, depending on the motor and application. For higher-performance motion control applications, a VSD (Figure 3(c)) enables accurate torque, velocity, and position control.

It is estimated that only about 1-in-6 of all deployed motors in the industry are inverter driven or connected to a VSD. By moving more deployed motion assets from grid-connected motors to inverter-driven or VSDs, it is possible to significantly reduce energy consumption and CO emissions. These reductions in energy consumption would enable more sustainable manufacturing with reduced CO2 emissions. It has been estimated that if all deployed motor-driven systems were operated at maximum efficiency, it would reduce global electricity demand by 10% and remove 2490 Mt of CO2 emission in 2030.

Figure 3: (a) Grid-connected AC motor (b) Inverter fed motor (c) Variable speed motor drive

It is estimated that only about 1-in-6 of all deployed motors in the industry are inverter driven or connected to a VSD. By moving more deployed motion assets from grid-connected motors to inverter-driven or VSDs, it is possible to significantly reduce energy consumption and CO emissions. These reductions in energy consumption would enable more sustainable manufacturing with reduced CO2 emissions. It has been estimated that if all deployed motor-driven systems were operated at maximum efficiency, it would reduce global electricity demand by 10% and remove 2490 Mt of CO2 emission in 2030.

Motor efficiency standards

To accelerate the deployment of higher efficiency motor driven systems, the International Electrotechnical Commission (IEC) has contributed to the definition of energy efficient electric motor standards. This includes the IEC 60034-2-1 test standard for electric motors and the IEC 60034-30-1 classification scheme comprised of four levels of motor efficiency (IE1 through IE4), with the IE5 level due to be introduced in the future. The higher-level standards can be achieved either through more efficient motor design or through the addition of an inverter or VSD to a standard motor design. As the efficiency classes become more stringent, meeting them by improved motor design alone is becoming more and more challenging, and costly. Alongside the additional benefits provided by variable speed control in the application, the case for VSD-attach to most industrial motors is becoming more compelling.

Article Tags

Safety

Related Content