As the IoT grows, and hardware demands increase, the development platform at the heart of your project needs more power, more IOs, and more connectivity. That’s where the DragonBoard 410c comes in.
The DragonBoard 410c is the latest player in the development platform landscape and is built by Arrow and powered by Qualcomm. Here’s a run-down of some of the specs behind this exciting new piece of hardware.
See related product
Qualcomm Snapdragon Processor
At the center of the DragonBoard 410c is the Qualcomm Snapdragon Processor – a 1.2Ghz Quad Core workhorse that has made a name for itself as the brains behind mobile devices from HTC and Motorola. The DragonBoard 410c also features 1GB of low-power DDR3 Ram and 8GB of flash storage (with additional microSD expansion on board).
What really sets the DragonBoard 410c apart are its on-board connectivity features. The DragonBoard 410c comes with built in WiFi, Bluetooth, and GPS. It also has 12 GPIO pins, as well as SPI, I2C and UART connectivity.
DragonBoard 410c: Android, Linux & More
The DragonBoard 410c is also versatile. It ships with Android 5.1 pre-loaded, but can also run Linux Ubuntu and even Windows 10, and because the board is capable of both 32 and 64-bit operation, the DragonBoard 410c is capable of playing nice in many different applications

Finally, the DragonBoard 410c is well-equipped for handling graphics. The board includes a 400MHz graphic processor capable of handling 1080 HD video (and has a built-in HDMI port). The DragonBoard 410c is also set up to integrate with Amazon Web Services (AWS), making it a solid choice for IoT, smarthome, and other connected applications.
Arrow.com is the exclusive home of the DragonBoard 410c. Grab one today and start making your next project idea a reality!