The Role of Audio in Modern Building Safety and Security Systems
Modern building safety and security systems continue to evolve, but the role of audio within them is not new. Audible signaling has been a foundational part of alarm and communication systems for over a century, from early centralized fire alarm panels to building-wide intercom systems introduced in the late 19th and early 20th centuries. This article will introduce the role of audio in modern building safety and security systems, as well as the related solutions launched by Same Sky and their product features.
Audio design considerations should be made at the system level
Audio is already a ubiquitous signal in daily life. In modern society, what has truly changed is not the importance of audio, but the way it is implemented. Advances in digital electronics, connectivity, and system integration have expanded the functions of audio and improved its reliability in complex building environments. Today, audio can be used to support user interaction, system communication, recording, and event detection. For engineers, this reinforces an important point: audio design considerations should be made at the system level, rather than simply selecting components.
Audio supports multiple functions in building safety and security systems. Although specific requirements vary by application, the fundamental goal is the same: audio must be clear, reliable, and appropriate for the environment. For example, in access control systems, audio provides real-time feedback to users, including confirmation tones for access granted or denied, as well as voice communication through intercom-enabled entry points.
In video surveillance systems, audio is used not only for real-time communication and deterrence, but also for recording and playback. Audio recordings can provide additional context for incidents and are often integrated with video streams for review and analysis. In addition, in fire and life safety systems, audio becomes mission critical. It is responsible for delivering alarms and voice evacuation instructions, and its intelligibility and reliability directly affect occupant safety. These applications have different requirements for audio performance, which is why audio design must be carried out at the system level, rather than as a one-size-fits-all solution.
When determining the audio output required for a device, the needs of the application environment must first be considered
Audio output design fundamentals
When carrying out system-level design, one of the first design decisions is to choose the appropriate audio output device. The most common options include piezo buzzers, magnetic buzzers, and speakers. Piezo and magnetic buzzers are generally used for narrowband frequency output, making them suitable for alarms and status indications rather than voice reproduction. Piezo buzzers are highly efficient and well suited for low-power applications where a clear single or multi-tone frequency signal is sufficient, while magnetic buzzers are less efficient than piezo devices but can operate at lower voltages and often deliver strong audio output in more compact designs, making them suitable for applications with limited space and limited driving voltage.
Speakers support a wideband frequency response and can reproduce voice and more complex audio signals, making them essential components for intercom systems, voice evacuation systems, and advanced surveillance applications. However, the tradeoff is increased power consumption and more complex system requirements, including amplification and signal processing. Rather than viewing these audio devices as competing options, it is more accurate to see them as tools suited to different roles. The correct choice depends on whether the application requires simple signaling or clear communication, allowing designers to flexibly balance acoustic performance with power consumption, space, and system complexity.
Same Sky's speaker product line
A key basis for selection is understanding sound pressure level and coverage. Sound pressure level (SPL) determines the audibility of a signal in a specific environment. Indoor applications such as access control readers typically operate in controlled environments with moderate background noise. Outdoor or industrial environments have higher ambient noise and require greater output. Fire and life safety systems have the strictest requirements. Audio must remain audible and intelligible during emergency conditions when noise levels may increase significantly.
Placement is also critical to achieving effective coverage. Speaker orientation, mounting location, and grille design all affect how sound propagates through a space. Poor placement can result in uneven coverage, dead zones, or excessive reflections that reduce intelligibility. On the other hand, enclosure design primarily affects the speaker's internal performance, such as resonance and frequency response. Effective design ultimately requires looking beyond SPL alone and considering how the system will perform under real-world conditions.
Microphones have long been part of communication systems such as intercoms. However, microphones are now used not only for communication but also as part of the sensing layer. In access control, microphones support intercom and voice-assisted entry. In surveillance systems, they capture audio for recordings and enable communication with remote operators. Microphones can also support acoustic event detection in more advanced systems, including identifying sounds such as breaking glass or other abnormal conditions. As systems continue to incorporate AI and edge processing, audio input will play an even larger role in event detection and system response.
System integration considerations for audio
Even with the right components selected, audio performance ultimately depends on how well it is integrated into the overall system. Electrical, mechanical, and environmental factors all influence the final result, and small design decisions can also have a noticeable impact in the field.
From an electrical perspective, audio can place unexpected demands on the system. Speakers and amplifiers can quickly become higher power consumers, especially in PoE or battery-backed designs. On the input side, the challenge shifts to signal integrity rather than power. Microphone sensitivity to noise depends on the output type, with analog microphones being more susceptible to interference and requiring careful layout and grounding practices to maintain signal integrity. Key considerations include managing power budget and peak current during playback, maintaining signal integrity through proper layout, grounding, and shielding, and selecting and matching amplifiers to achieve the desired output.
In addition, mechanical design is equally important. The enclosure directly affects how sound is produced and captured, while component placement determines how effectively audio reaches the user or the environment. In practice, this comes down to designing enclosures that support the intended acoustic performance, placing speakers and microphones to avoid obstruction or uneven coverage, and minimizing interference between components. Environmental conditions add another layer of complexity, particularly in outdoor or industrial deployments. Long-term performance depends on designing for moisture and dust protection through the use of appropriately IP-rated audio components, supporting extreme temperatures across the operating range, and accounting for contaminants that can obstruct acoustic pathways over time.
At the system level, architecture decisions also shape audio behavior. Whether audio is always active or event-driven, where processing occurs, and how it interacts with other subsystems all affect performance, power consumption, and responsiveness.
Audio systems in building safety applications must meet strict reliability expectations. In many cases, devices must also comply with safety standards such as UL certifications and regional regulatory requirements. These standards define how systems must perform under real-world conditions, including requirements for alarm audibility, system uptime, and fault handling.
Audio must also function during power transitions and system faults, making fail-safe design key to ensuring that critical alerts are still delivered even if other parts of the system are compromised. In some designs, redundancy is introduced to improve reliability, which may include multiple alert paths or backup power systems. The challenge is finding the right balance between reliability, cost, and complexity.
Same Sky's audio product line
A diverse audio product line
Same Sky's audio products cover buzzers, microphones, speakers, and audio sample kits. Among them, the buzzer product line is quite diverse and can be divided into four major categories by product type, including audio indicators with built-in drive circuits that emit sound when DC voltage is applied and audio transducers that require an external drive circuit.
Same Sky's buzzers support sound pressure levels (SPL) ranging from 65 dB to 115 dB. Most transducers fall within 65-90 dB, while indicators can reach 100 -115 dB, making them suitable for noisy environments. Voltage ratings include Vdc (direct current) for indicators with built-in drive circuits, while Vp-p (peak-to-peak) is used for transducers requiring external drive, ranging from 1.5 V to 220 V. Current consumption is as low as 1 mA and as high as 600 mA. Low-power models are suitable for battery-backed or PoE designs. Mounting methods include through-hole, SMT, wire, and solder, with round and square shapes, and sizes from 3.2 x 3.2 x 0.12 mm to 130 x 130 x 150 mm. Included in Same Sky’s buzzers line is a range of siren models, which are ideal for security systems and alerts.
Same Sky also offers MEMS microphones and electret condenser microphone options, allowing engineers to choose the best solution based on size, performance, and environmental requirements. MEMS microphones use semiconductor processes and offer compact packaging and high consistency. Electret condenser microphones use a traditional diaphragm-based analog design and offer IP57, IP65, and IP67 protection options. Most ECM and MEMS models use analog output with output impedance of 100 - 2200 Ω, requiring an analog signal chain. Digital PDM (pulse density modulation) MEMS mics directly output digital signals, providing strong anti-interference capability and making them suitable for dense PCB layouts.
Same Sky's microphone products include noise cancelling, omnidirectional, and unidirectional directivity. Models offer top or bottom ports, making them suitable for specific mechanical design requirements. Sensitivity ranges from -24 dB to -54 dB with sensitivity tolerance from ±1 dB to ±3 dB. In terms of current consumption, models consume from 80 - 1120 μA, while operating voltages span 1.3 to 3.6 Vdc. Most MEMS models support 20 - 10,000 Hz operating frequencies, while electret condenser models can reach 100 - 20,000 Hz.
Same Sky's speaker products range from miniature speakers to larger frame speakers. These speakers feature sound pressure levels (SPL) ranging from 75 dB to 135 dB, nominal inputs from 0.003 to 20 W, and max inputs from 0.005 to 40 W.
Same Sky's speaker impedance ranges from 3 - 50 Ω and features a resonance frequency range from 100 Hz to 1700 Hz. Lower resonance frequencies are suitable for fuller low-frequency performance, while higher resonance frequencies are suitable for applications where voice intelligibility is prioritized. Some enclosed speakers already include enclosures for direct integration, making it easier for designers to build them into their system. Mounting methods include PCB, solder eyelets, solder pads, solder pins, spring contact, surface mount, through hole, wire leads, and wire leads with connector.
Same Sky also offers the CSK-AUDIO-001 IP-rated audio sample kit, which contains 70 waterproof buzzers, microphones, and speakers, all from its top waterproof product series. The models in the kit all have IP67 protection and cover a variety of termination methods, sound pressure levels, and form factors, making it easy for designers to find the ideal solution for harsh environments. Designers can quickly compare and test to shorten development cycles.
Please visit the following Arrow Electronics website to search for related audio components launched by Same Sky.
Conclusion
Audio has long been a foundational element of building safety and security systems. Its role has not fundamentally changed, but the way it is implemented continues to evolve with advances in digital electronics, connectivity, and system integration. Modern systems place greater emphasis on integration, flexibility, and performance, which increases the importance of thoughtful audio design. Engineers who take a system-level approach to audio design will be better equipped to meet the demands of modern safety, security, and user experience. Same Sky's range of audio components as well as audio design services can help customers optimize solutions for specific system needs.
Article tags