Arrow Electronic Components Online

Encoder technology is the core of intelligent motion control in modern motor drives

Industrial Automation05 May 2026
Autonomous mobile robots carry cardboard boxes across the floor of a large warehouse.
View all articles

In today's factory automation systems, encoders are no longer just sensing devices, they represent the starting point for truly "intelligent" drive systems. Whether the goal is achieving micron-level positioning accuracy, maintaining stable speeds under variable loads, or running reliably over long periods in harsh environments filled with dust and oil mist, everything begins with real-time, precise feedback from an encoder. If the motor drive acts as the system's brain and muscles, then the encoder serves as the nerve endings that sense the system's actual position. Without an encoder, precision motion control becomes guesswork. This article explores the critical role of encoder technology in industrial automation, the growing trend toward absolute encoders, and how Same Sky's AMT capacitive encoders use innovative technology to address the pain points of traditional encoder designs.

The role and importance of encoders in industrial automation

Early automation systems often relied on open-loop control, where the controller issued commands and assumed the motor would execute them. However, when load changes, belt stretching, mechanical wear, or temperature drift occur, deviations between commanded and actual outcomes become inevitable, making it difficult to maintain precision. Closed-loop control continuously measures motor position and speed via an encoder, and the drive adjusts its output in real time to keep actual motion aligned with the commanded profile. This feedback loop delivers high positioning accuracy, repeatable motion trajectories, stable speed regulation, faster settling times, and reduced mechanical stress. The data provided by encoders allows the controller to close the loop, including position data (confirming the actual location of the rotor and load), velocity information (stabilizing speed under varying loads), direction detection (ensuring deterministic motion logic and safety behavior), and index referencing (establishing a repeatable reference point).
 
Within industrial automation, encoders are used across a broad range of applications, including multi-axis coordination for robotic arms, which depends on accurate position feedback to ensure smooth and repeatable motion. When payload and reach change, the control system needs trustworthy feedback to maintain path accuracy and stable movement. In conveyor and material handling systems, speed synchronization and load compensation require consistent velocity measurement; encoder feedback helps maintain predictable timing, directly boosting throughput and reducing jams or mis-indexing.
 
Additionally, accurate odometry readings for autonomous mobile robots (AMRs) rely on dependable wheel rotation feedback for navigation and positioning. When the system can trust the encoder signal, mapping and motion planning become more stable. For CNC machines, gantries, and machining systems, tight tolerances depend on stable feedback, especially as the system warms up over long runs. Encoder consistency influences repeatability, surface finish, and the ability to hold targets without constant retuning.
 
A controller can only correct what it can measure. If encoder feedback is noisy, inconsistent, or susceptible to environmental conditions, the drive may still "work," but machine precision will degrade, tuning margins will shrink, and nuisance faults will become more frequent. In many designs, improving the encoder feedback channel is the fastest way to enhance motion quality without changing the motor or power stage.

Characteristics and advantages of absolute encoders

Incremental encoders measure relative motion and require a homing or referencing procedure after power-up. Absolute encoders, by contrast, provide a unique position value immediately at startup, eliminating the need for homing sequences. In today's interconnected, data-driven industrial environments, this feature is extremely valuable. It reduces startup time, simplifies system design, and delivers greater noise immunity and signal integrity through serial communication protocols.
 
Traditional quadrature encoding is relatively sensitive to electrical noise and signal degradation, whereas many absolute encoders use serial communications that incorporate error detection mechanisms such as checksums or CRC. Compared to analog signals, they are less susceptible to electrical noise interference,  simplify wiring through serial communication interfaces, and provide more deterministic communication in networked control systems.
 
These advantages align well with broader trends in factory automation, where motion systems are increasingly being integrated into industrial networks and expected to operate as part of coordinated, data-driven environments. While incremental encoders still have a place in cost-sensitive or simpler applications, absolute encoders have become the default choice for high-end designs as performance expectations and system complexity continue to rise.

Functional features of Same Sky’s AMT capacitive encoders

Same Sky's AMT modular encoder series use patented capacitive sensing technology and are available in incremental, absolute, and commutation versions. These models offer a rugged, high-precision encoder solution with excellent environmental tolerance. Unlike traditional optical encoders that rely on an LED and line-of-sight, capacitive technology is less susceptible to common industrial contaminants such as dust, dirt, and oil. It can operate without additional covers or seals and supports a temperature range from -40°C to +125°C, making it suitable for vacuum and high-pressure environments.
 
In addition, AMT encoders support programmable resolutions to enhance design flexibility. The AMT series offers up to 22 programmable resolution options, with incremental versions reaching up to 5120 PPR and absolute versions providing 12-bit or 14-bit resolution. Engineers can adjust resolution during prototyping without ordering different part numbers, and procurement teams can significantly reduce the number of SKUs in production, thereby simplifying BOM management.
 
Absolute AMT encoders also feature diverse interfaces, supporting SPI, SSI, or RS-485 communication protocols, with single-turn or multi-turn output options. Taking the AMT24 series as an example, it uses a high-speed RS-485 communication protocol, delivering 4096 positions per revolution at 12-bit resolution or 16,384 positions per revolution at 14-bit resolution. Power consumption at 5 V is only 16 mA, with an accuracy of ±0.2 mechanical degrees.
 
The AMT series simplifies installation and alignment, reducing setup time to just seconds and significantly cutting the labor-intensive assembly processes traditionally associated with encoders. Users can set the zero position using the AMT Viewpoint™ graphical interface or the encoder's protocol. Furthermore, thanks to its low-mass internal rotor design, the AMT encoder draws low current and requires minimal power for rotation, while its compact package helps reduce overall design size. These features are especially critical for weight- and power-sensitive applications such as drone payloads and portable devices.
 
For brushless motor applications, AMT commutation encoders offer flexible configuration with programmable incremental resolution (up to 4096 PPR) and support commutation signals for 2, 4, 6, 8, 10, 12, and 20-pole brushless motors, greatly simplifying integration into motor drive systems.
 
In the industrial automation field, AMT encoders are widely used in robotics, drone payload systems, agricultural spraying equipment, and renewable energy, among other applications. For example, in drone gimbals, AMT encoders provide high-resolution digital feedback that enables the control system to compensate for vibrations in real time, achieving smooth image stabilization. In agricultural drone spraying systems, the high-resolution feedback from AMT encoders, combined with intelligent control, can adapt in real time to changes in terrain and wind speed, enabling precise application and reducing waste.

Driving data automation and serving as the intelligent foundation for the industry 4.0 era

As the waves of Industry 4.0 and smart manufacturing sweep across the globe, factory automation has evolved from simple motion control into data-driven, highly interconnected intelligent systems. In this context, encoders are no longer just sensors that provide position and velocity feedback, they have become critical data sources within the Industrial Internet of Things (IIoT) architecture. From machine diagnostics and predictive maintenance to system-level optimization, the data generated by encoders is playing an increasingly central role.
 
With the advancement of Industry 4.0, the high resolution and reliable data transmission capabilities of capacitive encoders have become essential for improving production efficiency and equipment safety. By integrating bus communications such as EtherCAT and PROFINET along with advanced sensing technologies, companies can achieve more flexible control architectures and predictive maintenance, thereby maintaining the stability and competitiveness of their automation systems in highly competitive environments. In IIoT applications, encoders help realize more autonomous, efficient, optimized, and cost-effective industrial processes by integrating industrial tools, sensors, and monitoring equipment. Traditional encoder systems use sensors with fixed device arrays, whereas next-generation encoders integrate more intelligent functions through digital technology.
 
Same Sky's AMT encoder series is a pioneer in this digital transformation. Designed with digital ASIC technology, AMT encoders provide engineers with valuable diagnostic and programming tools that accelerate time-to-market and reduce field machine downtime. Integrating diagnostic capabilities into rotary encoders allows designers to obtain valuable system data that was previously unavailable in pure analog solutions. This data can be used to quickly determine whether an encoder is functioning correctly, has failed or become inoperable, or is misaligned. The system can then use this information to alert operators to potential issues, or to make informed decisions before starting the motor and potentially causing catastrophic damage.
 
This diagnostic data can also be monitored over time via industrial communication networks, providing valuable performance trends that can be analyzed and used to predict failures before they occur within the motion control system. Because the encoder is mounted directly on the motor in a critical location, its diagnostic data is not limited to the performance of the individual encoder. It can also serve as an early indicator of other problems within the motion control system, such as shaft misalignment, bearing wear, or thermal degradation. By carefully examining this data, preventive maintenance can be performed on the machine in a controlled manner before catastrophic failure occurs, limiting severe downtime, extending machine life, and increasing the overall intelligence of the system.
 
In practical applications, the diagnostic capabilities of AMT encoders deliver multi-level value. First, in terms of predictive maintenance, the system can use encoder data to detect anomalies early and schedule repairs before problems escalate. Second, if a fault does occur in the field, diagnostic data can speed up the troubleshooting process. Service technicians can access the encoder's diagnostic functions to quickly confirm whether the encoder is the root cause, eliminating the time-consuming and expensive trial of removing and replacing the encoder and motor from the system. This is especially important in industrial environments where downtime costs are high due to lost productivity. Furthermore, during product development, encoder diagnostic data also provides significant time benefits. When problems arise during testing, diagnostic data can quickly point to design areas needing improvement, potentially eliminating days or weeks of investigation. This shortens design cycles, leads to more robust products, and accelerates time-to-market.

Conclusion

The starting point and the end point of intelligent motion control both depend on encoders. A motor drive converts electrical energy into motion, while encoder feedback transforms that motion into a measurable, correctable, and optimizable closed-loop system. From precise positioning and stable velocity to data-driven diagnostics, encoder technology forms the backbone of modern automation platforms. As factory systems demand ever-higher precision, longer uptime, and greater intelligence, encoder performance will remain a decisive factor in motor design. Same Sky's AMT capacitive encoders, with their ruggedness, programmability, low power consumption, and easy installation, offer engineers an ideal solution that balances performance and reliability, helping industrial automation move toward higher levels of intelligent control.

Article Tags

Same Sky (formerly CUI Devices)
Encoders
Robotics
Arrow Times
Motion Control and Fluid Power

Related Content