Using configurable ultra-small clocks to reduce space, power and EMI in consumer electronics designs

The electronics we use every day, from phones and tablets to cameras and gaming consoles, have rapidly shrunk in size and increased in power, based on market demands. This change has been driven by advances in circuit design, among other things. In this article, learn how ultra-small timing clocks from Skyworks are enabling new generations of more compact, more powerful consumer electronics.

Saving space with ultra-small clocks

Space constraints are a major concern for system board designers focused on consumer products. Any possible reduction in used printed circuit board (PCB) space allows more room for routing signals, bypassing noise on power supplies, or simply reducing PCB cost. Numerous timing device vendors support small-outline clock generators optimized for the consumer electronics industry. Although very critical for system operation, the clock generator is generally not considered a key component on the board; therefore, it is occasionally overlooked when it comes to space savings. If that is the case, the embedded designer should reconsider the options and realize the significant space savings that a silicon clock generator can offer.

Consider a digital camera that requires three crystals or oscillators in the system to provide the necessary clocking for a USB controller operating at 24 MHz, for the high-speed analog-to-digital converter (ADC) (also at 24 MHz), and for the image processor at 27 MHz. Although it carries a higher cost than other larger crystals, the popular small surface-mount crystal has a standard size of 2 mm x 1.6 mm. This crystal runs fundamental frequencies typically ranging from 24 MHz to 54 MHz and is packaged in a ceramic housing available from many major industry suppliers.

If one or two of these three crystals were replaced by a Skyworks Si51210 clock generator with an ultra-small 1.4 mm x 1.2 mm package size, the digital camera designer would be able to reduce the system’s clock space usage by a considerable 47 to 73 percent. CMOS-based clock generators are mixed-signal semiconductor devices that employ a phase-locked loop (PLL) architecture typically used to generate output frequencies that are different from the input. If the device is configurable, the designer will be able to generate any frequency that best fits the system requirements.

Minimizing power consumption

System designers have many choices to make when it comes to selecting a clock generator. Since market trends favor greener, more power-efficient systems, it is important to consider certain factors impacting power consumption when making the clock selection. Understanding the silicon gate geometry, the core power supply and the ability to configure output drive are key factors in determining how “low-power-friendly” a clock generator will be. Power consumption in CMOS depends on the switching speed, the power supply level, and the load capacitance that the device is driving based on the following formula: P = CL * V2 * F.

CL is a representation of the load capacitance, which is relative to the gate size and thus dependent on the submicron CMOS technology being implemented. Making the device affordable at a smaller gate width technology, such as 0.18 micron, is critical. The device’s ability to support a lower supply voltage (V) has an exponential impact on power consumption as can be seen in the above formula. It is important, however, to consider the availability of the power supply in the system. For example, 1.8 V is a widely-used power supply across multiple handheld and AC-powered applications.

Reducing EMI

EMI reduction remains an important consideration when bringing electronic systems to market. Regardless of the system’s performance, features and other innovations, if the system cannot pass government regulations for electromagnetic emissions, the manufacturer may not be able to launch the product. This barrier to production heavily burdens system designers as well as EMI compliance engineers. In particular, the emission compliance test takes place after the board has been designed and just as the system is reaching the last phase of pre-production. Therefore, it is important to address EMI issues during the design stage or risk delays in launching the product to the market. This is no easy task, considering that unpredictable real-life noise models may be difficult to identify during board simulation. Conventional techniques for EMI reduction including shielding and localized filtering are relatively simple but can be costly.

To reduce the need to place passive components across the board to control potential noise and EMI behavior, the designer should consider choosing a clock generator that integrates a frequency modulation technique referred to as spread spectrum or spectrum spread. As the name suggests, spread spectrum technology distributes the energy that is typically concentrated at the center frequency over a wider bandwidth, consequently attenuating the peak energy. The configurable clock generator supports various configurable settings of the spread bandwidth and gives the EMI engineer more options for optimizing the system setting.

Configurability benefits

Using the signal integrity tuning features of an advanced configurable clock generator, the designer can reduce the budgeted amount of several of these timing errors. In addition, confidence in a sufficient timing margin can be increased by artificially introducing errors to validate the error modeling. For example, the highly programmable Skyworks Si51210 clock generator enables fine-tuning of the output drive strength, operating frequency, spread spectrum profile and modulation rate to minimize timing errors and validate the amount of time needed for the system timing margin. These programmable features can also be used to determine system response to intentional timing errors. This is a very useful debugging tool during development to measure the system’s sensitivity to various timing parameters.

Programming the clock to set all timing error deltas (Tr/Tf, period, spread spectrum magnitude, etc.) to the maximum allowed by specification and then running the system to the point of failure can prove the actual frequency limit. Of course, some small margin is still retained for safety, and the timing specifications of the other components remain unaffected.

Ultimately, the advantages of configurability allow the designer to adapt to any changes in frequency or drive requirements of the receiver devices even in if the changes occur in the middle of the design cycle. In addition, the ability to quickly reconfigure frequency, drive levels, and spread spectrum parameters while maintaining the same device pinout enables the designer to port the layout to the next project, thereby reducing the development time for the timing system.

READ MORE


Featured Products:


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.