The importance of safe and reliable operation

EMC measurement at SCHURTER

Cooperating with SCHURTER as EMC specialist. As an innovation and knowledge partner, SCHURTER is closely involved in the development of input systems for machines and devices used all over the world, often under demanding or complex conditions. Operating those devices must be done safely and reliably at all times. After all, a malfunction can have far-reaching consequences.

In today's high-tech equipment, electromagnetic radiation is one of the main risk factors for reliable operation. It is therefore not surprising that Electromagnetic Compatibility, or EMC for short, is one of the main areas of focus at SCHURTER when developing and integrating input systems. The required EMC certification guarantees safe and reliable operation over the lifetime of the application.

With specific expertise in this field, SCHURTER engineers help develop EMC-certified applications. 

Collaborative thinking in the design phase

Taking electromagnetic emission and immunity into account as early as the concept and design phase avoids having to make major design modifications afterwards. After all, discovering EMC deficiencies only in the final phase often means a costly and time-consuming trip back to the drawing board. Before the actual engineering begins, SCHURTER therefore already makes an inventory of possible failure-sensitive components or processes. Environmental factors for the intended practical use are also taken into consideration.

By choosing high-immunity materials and components in the design, electromagnetic interference can be reduced to a large extent. Insulated cables and suppression components can play a crucial role in achieving the desired EMC level. The enclosure and the way it is integrated also influence the final EMC score.

Testing during the development process

As an EMC specialist, SCHURTER is able to simulate and assess EMC conditions in-house. In a radiation-free test room, special software is used to measure how the application reacts to interference. 

Based on the findings, the application can be specifically adapted to limit or prevent electromagnetic influences. The test room is also used to measure the radiation levels of the application itself.

All signals around predefined critical frequencies are recorded by an antenna in the test room and transmitted via a coaxial cable to a spectrum analyser outside the room. From this, an algorithm determines an average, which must lie between certain values for EMC approval.

In SCHURTER's engineering lab, pre-compliance tests can be done during the design phase and with the first prototypes. A successful pre-compliance test offers a good indication of official CE certification.

0926-Conducted-test

0926-EMC-test

Co-engineering as success factor for efficient product development

Developing and producing machines and devices that need to comply with strict EMC requirements requires specific knowledge and expertise. By opting for co-engineering with SCHURTER, this expertise is guaranteed. SCHURTER specialists consult together in the design process and provide tailor-made advice.

SCHURTER helps select the most suitable materials, software and the various components. Development partners can thus rely on making the right choices for a reliable end product and an efficient production process. With very little extra cost, high-quality, user-friendly and EMC-certified input systems can be integrated into your application in a way that fits perfectly with the production process.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.