Power line noise countermeasures using common mode choke coils from Murata

Common mode choke coils (CMCC) are filters that reduce common mode noise that is problematic in differential transmission lines (non-automotive use: USB, HDMI, Mipi, etc.; automotive use: CAN, CAN-FD, 100Base-T1, 1000Base-T1, SerDes, A2B®, etc.), power lines, and audio lines.

Explore some countermeasure examples for using a common mode choke coil to deal with power supply noise in this article from Murata’s Tadashi Tanaka,Product Engineering Section 3, Product Engineering Department, EMI Filter Division.

Electronic devices are generally made up of multiple semiconductor and functional blocks and both must be supplied with power at their designated voltage. In many cases, the required voltages are all different. When this occurs, the voltage needs to be converted using a DC-DC converter. This is a circuit that converts the power supply to the voltage required for the operation of electronic components.

When working with different required voltages, size and electrical performance are two main considerations. Switching DC-DC converters are often used in such cases. However, it’s important to pay attention to the noise caused by switching. If the noise regulation standards aren’t met, then some type of noise countermeasure is required.

An example of a power line noise countermeasure

This noise countermeasure example was prepared with a typical non-isolated, step-down type (5 V to 1.8 V, Pout = 27 W) DC-DC converter with a switching frequency of 500 kHz.

The goal here is to support the CISPR22 class B general device standard (devices used in ordinary homes and light industrial environments). Effective noise countermeasures were implemented after determining whether the noise mode was primarily differential mode or common mode.

(1) Noise terminal voltage (150 kHz to 30 MHz)

The common mode voltage (noise terminal voltage) was measured for one line with respect to ground using an artificial mains network (AMN). When the noise terminal voltage is measured under the initial conditions, we can see that a noise spectrum occurs at multiples (frequency is converted to n multiples) of the 500 kHz switching frequency.

1221 Murata Power line noise - image 1

Figure 1. Initial noise terminal voltage levels

Before proceeding with the noise countermeasure, mode separation was performed using Delta-LISN (Line Impedance Stabilization Network) in order to determine whether the noise mode was primarily differential mode or common mode. As shown in Figure 2, it is clear that the noise in this case is primarily differential mode noise.

1221 Murata Power line noise - image 2

Figure 2. Noise mode separation

As a result, the noise level was significantly decreased when the EMIFIL® BNX029-01 block-type filter was used, due to its highly effective countermeasures for differential mode noise.

1221 Murata Power line noise - image 3

Figure 3. Noise countering effects of the block type EMIFIL®

Radiation noise (30 MHz to 6 GHz)

After implementing the countermeasure described above, the radiation noise was evaluated at 10 m to measure the intensity of the field emitted into the space, and discovered radiation noise that significantly exceeded the CISPR22 class B noise tolerance (Figure 4).

When the radiation path was investigated, it was discovered that the input power supply cable of the DC-DC converter was acting as an antenna and radiating noise into the surrounding space.

1221 Murata Power line noise - image 4

Figure 4. Initial radiation noise levels

The BNX029-01 is able to remove differential mode noise across a wide frequency band from 100 kHz to 1 GHz, so the remaining noise was presumed to be common mode noise.

When a PLT10HH9016R0PN common mode choke coil was inserted to deal with the common mode noise, the level of radiation noise significantly improved to meet the CISPR22 class B noise tolerance. As a result, it was learned that the radiation noise was primarily common mode noise (Figure 5).

1221 Murata Power line noise - image 5

Figure 5. Noise countering effects of a common mode choke coil

Lineup of common mode choke coils for power lines

Murata Manufacturing Co., Ltd. Maintains a wide variety of component sizes and characteristics to provide the optimal components for customer applications (Table 1).

Product name Size Common mode impedance Rated current *1 Rated voltage
DLW5BTM***TQ2
1221-Murata-Power-line-noise---produc-DLW5BTM
5.0x5.0mm
T=2.5mm max.
100Ω to 1400Ω
@100MHz
6A to 2A 50Vdc
PLT5BPH******SN
1221-Murata-Power-line-noise---produc-PLT5BPH
5.0x5.0mm
T=5.0mm max.
100Ω to 500Ω
@100MHz
5.6A to 3.1A 80Vdc
PLT10HH******PN
1221-Murata-Power-line-noise---produc-PLT10HH
12.9x6.6mm
T=9.3mm max.
45Ω to 100Ω
@10MHz
18A to 15A 300Vdc
400Ω to 1000Ω @10MHz 10A to 6A 100Vdc

 

Table 1. Lineup of common mode choke coils

*1 With regard to the rated current, derating is configured, so please see the detailed specifications for each product.

*2 The operating temperature range differs for each product type, so please see the detailed specifications for each product.

Summary

When implementing noise countermeasures, it is extremely important to determine whether the noise mode is common mode or differential mode. Murata has maintained common mode choke coils for power lines in every size, and these have the high rated current and high insertion loss to provide the optimal noise suppression products for your power supply circuits.

관련 상품 참조

PLT5BPH3013R7SNL

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 상품 참조

PLT10HH1026R0PNB

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 상품 참조

PLT10HH401100PNB

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 상품 참조

PLT10HH9016R0PNB

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 상품 참조

DLW5BTM142TQ2L

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 상품 참조

DLW5BTM251TQ2L

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 상품 참조

DLW5BTM501TQ2L

Murata Manufacturing Common Mode Chokes - CMCs 보기

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.