Capacitor Codes: Capacitor Markings and Tolerance Code Chart

Learn about the various markings on capacitors and the properties that these codes represent.

When you’re working with circuits, it’s essential to know and understand each of your components’ specs. Unfortunately, many parts, like capacitors, are too small to have all their relevant information written out in full. As a result, many manufacturers mark capacitors with essential data in shorthand or use visual markings that take up less space. The markings and data they’re able to write depend on the capacitor’s size.

Before we look at the markings themselves, let’s review some important terminology that will help us learn how to read capacitors:

  • Capacitance: The amount of charge that the capacitor can store.
  • Breakdown Voltage: The point at which the capacitor short circuits and can no longer hold a charge.
  • Tolerance: The expected variations around the given capacitance – in other words, how close the real capacitance will stay to the designated capacitance.
  • Polarization: By design, some capacitors can accept voltage in only one polarity (otherwise you risk destroying the device). In polarized capacitors, therefore, it is important to know which lead is positive and which is negative.

Common Capacitor Numerical Markings

Because capacitance is the most important marking on a capacitor, it may be the only marking you see on the device. Larger capacitors usually display at least two values written directly on the component:
  • Capacitance
  • Breakdown voltage
Manufacturers may express capacitance as either a number followed by “μF,” such as “150μF.” (the μF symbols designates microfarads) They may also use a series of three digits. These numbers tell you the picofarad rating’s value (leading digits) and power (final digit).
 
For example, in the image below, “224” indicates 22 x 104, or 220,000 picofarads.
 
0918_Capacitor_marking_200

In this marking formula, it is important to note that the final digit may indicate a few different things: 

  • 1-6 indicate powers of 10
  • Seven is not used
  • The numbers eight and nine refer not to an exponential power of eight and nine, but to a multiplier of .01 (x 10-2) and .1 (x 10-1) respectively

Note that tiny capacitors – under 1000μF – will indicate the capacitance directly in picofarads. You may see a number between 1 and 999 written directly on them. It’s important to know the general range of capacitance to understand how to read the numbers. You’ll need to know the difference between 134μF written directly or at 130,000μF written in an exponential coding.

After capacitance, the next most important spec is the breakdown voltage. If the capacitor bears a second value, it will typically be its breakdown voltage, expressed as a number followed by V, such as “25V” or “100V.”

Finally, in the case of a capacitor with polarized leads, you’ll typically see a colored stripe on the negative side. Usually the line is white, but below you can see a capacitor with a black stripe marking the negative pole. Also note the indications for the breakdown voltage and operating temperature.

0918_Capacitor_markings_1 

Capacitor Color Codes

Modern capacitors use the numerical markings we outlined above, but older capacitors employed a (now obsolete) color coding system. If you come across these capacitors, try looking up a capacitor color code guide like the one here to decipher the codes for capacitance, breakdown voltage, and other values.

Other Capacitor Values

Other optional data may include values such as:

  • Operating temperatures
  • Temperature coefficients
  • Date of manufacture
  • Tolerance

Component manufacturers indicate tolerance with a letter code that refers to variances as small as +/- 0.5pF (indicated as A) up to -20/+80% (written as Z). The capacitor tolerance chart below shows some common tolerance letter codes:

Capacitor Code

Capacitor Tolerance

B

± 0.1%

C

± 0.25%

D

± 0.5%

F

± 1%

G

± 2%

J

± 5%

K

± 10%

M

± 20%

With these guidelines, you should be able to quickly check the specs of any capacitor you are using. If you’re unsure about an unusual marking’s meaning, if the capacitor doesn’t indicate a crucial piece of info (such as the breakdown voltage), or if you’re designing a new project and specifying capacitors, check the complete datasheet to be sure you have what you need to proceed safely.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.