Arduino PWM: Pulse Width Modulation in Arduino

게시자

Many Arduino boards, such as the Uno and Nano, don't have the capability to output different voltages―as we discussed in our Arduino digital to analog converter (DAC) article . They can, however, rapidly cycle outputs in the form of pulse-width modulation (PWM) to simulate a varying output.

We can use two characteristics to describe an Arduino PWM (or any PWM) signal:

1. Frequency: how often pulses occur in a given period of time.

2. Duty cycle: what percentage of time the signal is on.

A 50% duty cycle signal, for instance, would have the same repeating on time and off time. Frequency tends to stay constant in a control signal. Check out our article, All About PWM, for more information on this technique.

For now, we'll address PWM as it relates directly to Arduino boards, especially in the context of the Arduino Uno with its ATmega328P microcontroller. Fortunately, we can apply these concepts to any dev board.

Image: Jeremy S. Cook

Arduino PWM LED Control

To get started with Arduino PWM LED, you can use "Fade," the PWM example that comes built into the Arduino IDE. To access this example, which you can see in the screencap above, follow these steps:

1. Navigate to the IDE and look for the name under "basics."

2. Load the example onto your board.

3. Hook up an LED, plus the appropriate resistor in series, to pin 9. You'll see your LED brighten and darken over time.

4. If you prefer, you can change the output pin number around (to 3, 5, 6, 10, and 11).

You'll also be able to modify the brightness and fade amount, and you can use this code as a template for more advanced designs.

Arduino PWM Motor Control

You can also use PWM with a DC motor. This method uses the same pulsing voltage concept, but you'll need a motor driver/transistor setup to handle a motor's higher current needs.

If you want to control a servo via PWM, stick to the Arduino environment and use one or more servo objects, such as:

- Sweep example, as seen on Arduino's website.

Controlling a servo using an ATtiny85 under the Arduino framework.

Arduino PWM Frequency and Duty Cycle

In basic PWM discussions, frequency tends to take a back seat to the duty cycle. And in many cases, once you're above a certain point, it doesn't make much of a difference. At other times, however, frequency matters. For example, the six hardware PWM pins on an Uno run at two different default frequencies via three individual timers. These are divided up into:

- D3/D11, with a speed of 490.20 Hz.

- D5/D6, with a speed of 976.56 Hz.

- D9/D10, with a speed of 490.20 Hz.

Conveniently, you can change these frequency values as sets in code. Here's an example: TCCR2B = TCCR2B & B11111000 | B00000001 gives D3/D11 a frequency of 31,372.55Hz. You can set D5/D6 even higher with TCCR0B = TCCR0B & B11111000 | B00000001, yielding a speed of 62500.00 Hz. Values into the sub-100 Hz levels are available for all PWM pins as needed.

Whether you use it to control motors, lights, or another application, Arduino PWM is a great tool to have at your disposal. With this technique, you can do much more than power a device on and off; you can simulate a more nuanced output with a minimum of hardware.

 

Shop All Arduino Products Here

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.