High-voltage DC to low-voltage DC conversion is the voltage adaptation hub for 800VDC data centers
In 800VDC data center architectures, high-voltage DC to low-voltage DC (HVDC to LVDC) conversion plays the critical role of a "voltage adaptation hub." It is responsible for efficiently converting the high voltage from the 800V DC busway distribution system into the low voltages (such as 48V, 12V, or even below 1V) required by compute chips like GPUs and CPUs. It serves as the bridging link connecting "high-voltage distribution" and "chip power delivery."
HVDC to LVDC conversion enables the step-down from high voltage to ultra-low voltage. AI chips operate at very low voltages (typically <1V) but demand extremely high currents. The HVDC to LVDC conversion stage must achieve an ultra-high step-down ratio from 800V to below 1V within a very compact space, while maintaining extremely high efficiency. HVDC to LVDC conversion is also a key factor determining system energy efficiency; the efficiency of this conversion stage directly impacts the overall Power Usage Effectiveness (PUE) of the data center. Traditional multi-stage conversion solutions achieve an end-to-end efficiency of only about 85%-88%, while next-generation HVDC to LVDC solutions can boost link efficiency to over 93%. Furthermore, HVDC to LVDC conversion frees up space for high-density computing. By reducing the number of conversion stages from 6 to 3, it significantly reduces the footprint of power supply equipment, freeing up more rack space for compute cores like GPUs.
The key technologies of HVDC to LVDC conversion lie in achieving ultra-high conversion efficiency, employing advanced topologies and wide-bandgap semiconductors (such as GaN) to achieve peak efficiencies above 97%, and delivering high power density, enabling kilowatt-level power conversion within minimal space. Advanced Intermediate Bus Converters (IBC) can achieve power densities exceeding 2000W/in³, making it possible to power high-density racks.
On the other hand, HVDC to LVDC conversion features a streamlined number of conversion stages. From 800V to the GPU core voltage, only two conversion stages are needed: first, an isolated IBC steps down 800V to 6V or 48V, and then a multi-phase buck solution steps it down to below 1V, significantly reducing losses. It also provides fast dynamic response. To cope with the severe load fluctuations of GPUs (millisecond-level current transients), HVDC to LVDC solutions must possess extremely fast transient response capabilities to ensure stable supply voltage.
HVDC to LVDC conversion: efficiently converting to the low voltages required by servers and chips
HVDC to LVDC conversion can efficiently convert 800V to the low voltages required by servers and chips. For example, the architecture co-developed by Texas Instruments (TI) and NVIDIA requires only two conversion stages: first, a compact 800V-to-6V isolated bus converter (with extremely high peak efficiency), followed by a multi-phase buck solution from 6V to below 1V. This streamlined architecture fully supports NVIDIA's reference design. HVDC to LVDC conversion serves as the critical bridge from "power transmission" to "chip power delivery" in 800VDC architectures, and its efficiency and power density directly determine the upper limit of compute capacity that an AI factory can unleash.
The 5.5kW AI Server ORv3 Power Supply (PSU) is a reference design developed by the Arrow Electronics and STMicroelectronics (ST) joint lab. Yageo, as the passive component supplier for this reference design, provides key components such as MLCCs, power inductors, and resistors. This PSU strictly follows the OCP (Open Compute Project) ORv3-HPR specification, serving as a foundational building block for standardized, interoperable AI server racks. A single PSU delivers 5.5kW of output power and is the standard power module supporting high-power GPU clusters such as NVIDIA Blackwell Ultra and Rubin. It supports N+1 or N+N redundancy configurations, with multiple PSUs capable of being paralleled into a power shelf. Its design is also prepared for the future evolution toward 800V HVDC directly entering the rack, enabling seamless integration into 800VDC architectures.
Click here to view related information
In 800VDC data center architectures, onsemi's AI server power solutions play the core role of a "full-link power enabler." It does not merely provide a single power product, but rather offers a complete intelligent power portfolio from grid to processor, delivering efficient, high-density power conversion for AI factories. onsemi's solutions achieve this role through a series of innovative technologies, primarily covering a comprehensive wide-bandgap (WBG) technology portfolio, including SiC (EliteSiC series) and vertical GaN (vGaN). Additionally, there are key components optimized for AI, such as the 650V EliteSiC M3S MOSFET and PowerTrench T10 MOSFET, providing efficient, high-density solutions for the entire power chain from grid to chip.
Click here to watch the related video
In 800VDC data center architectures, Molex's PowerPlane Busbar Clip connectors are responsible for reliably transmitting high-voltage, high-current power from the 800V DC busway distribution system to critical equipment such as Power Supply Units (PSUs), Battery Backup Units (BBUs), and Power Distribution Boards (PDBs). They serve as a key node connecting the "power artery" to the "power delivery terminals." As PCB-to-busbar connectors, they can carry high currents from 130.0A to 320.0A, and through low voltage drop and high-conductivity copper alloy design, ensure efficient power transmission with low heat generation. These connectors support the Open Compute Project (OCP) standard and are fundamental building blocks for standardized, interoperable AI server racks. The product's voltage rating reaches 1000V, fully covering and exceeding the requirements of current 800VDC architectures, providing ample margin for future system upgrades.
Click here to view related information
In 800VDC data center architectures, Yageo's C4AQ series DC-Link capacitors play the core role of a "high-voltage power stabilizer" and "noise filter." Positioned between the 800V DC busway and the downstream power conversion modules (such as PSUs and DC-DC converters), they are responsible for smoothing the DC voltage, filtering high-frequency ripple, and providing energy buffering for instantaneous power demands of loads like GPUs. They are key passive components ensuring the stability and cleanliness of the entire high-voltage power supply chain. The C4AQ series capacitors are specifically designed for high-voltage DC-Link applications, featuring extremely low Equivalent Series Resistance (ESR), metallized polypropylene film dielectric, automotive-grade high reliability, and compact modular packaging, ensuring stability and efficiency throughout the power supply chain from the high-voltage DC busway distribution system to core loads like GPUs.
Click here to download related information
In 800VDC data center architectures, Yageo's PM9525NL 3.6kW LLC transformer is typically located within the Intermediate Bus Converter (IBC) or DC-DC conversion stage, responsible for efficiently and safely converting the stable 800V DC busway distribution system voltage to the low voltage required by downstream circuits. It serves as a bridge connecting the high-voltage distribution and low-voltage loads. In a typical 800VDC power supply chain, the PM9525NL transformer primarily undertakes efficient voltage conversion, safe electrical isolation, and achieving high power density. Through a series of innovative designs, the PM9525NL integrates leakage inductance to simplify design, and features high reliability and a wide operating temperature range, providing critical technical support for the efficient power supply of next-generation AI servers and data centers.
Click here to view related information
Yageo's PHV225 and PHS225 series capacitors are rated at 63VDC and are primarily used in the 48V distribution network at the end of the architecture in 800VDC architectures. In an 800VDC architecture, after front-end equipment like SST converts the high voltage to an intermediate bus voltage of 48V, the PHV225/PHS225 capacitors take on the critical task of stabilizing this key voltage. To fulfill this role in the demanding AI server environment, the PHV225/PHS225 series, with their ultra-high ripple current capability, extremely low ESR, and automotive-grade high reliability, ensure the stability and efficiency of the power supply chain from the 48V bus to the GPU core, serving as a solid backbone supporting the stable operation of AI servers.
Click here to view related information
In 800VDC data center architectures, onsemi's 12kW AI PSU reference design is a high-density power module compliant with the OCP ORV3 standard, specifically designed for AI servers. It efficiently converts power from the grid or 800V DC busway into the 48~50V DC required by AI servers. Within the power chain from grid to chip, this PSU serves as the "last mile" connecting upstream distribution and downstream GPU servers. Featuring a high power density output of 12kW and peak efficiency up to 98%, it effectively reduces energy loss and cooling costs. It complies with the OCP ORV3 specification, ensuring compatibility with standard racks and power architectures, and acts as an efficient and reliable "power hub" connecting the distribution network to AI compute chips.
Click here to view related information
Article tags