Arrow Electronic Components Online

The 800V DC busway distribution system acting as the power aorta

PCIM17 Aug 2026
alt-image
View all articles

In the "grid-to-chip" power supply chain, the 800V DC busway distribution system plays the core role of the "power aorta." It receives 800V high-voltage DC power from front-end power sources such as solid-state transformers (SSTs) and efficiently and safely "pumps" it to every cabinet in the data center. If the SST solves the "source" issue, then the DC busway distribution system is the "highway" carrying megawatt-level power and is the key infrastructure determining whether AI factories can be deployed at scale.

Before discussing the role of the 800V DC busway distribution system, it is necessary to understand why the 800V architecture adopts "busway" rather than traditional cables. Traditional data centers use 54V low-voltage DC distribution. When facing high power density exceeding 100kW per cabinet, they encounter serious bottlenecks, such as huge copper losses and space occupation, and large currents lead to enormous line losses (I²R losses). In addition, complex wiring and heat dissipation dead zones are another important issue. Traditional cable wiring is complex and prone to creating heat dissipation dead zones, increasing operational costs. The 800V DC busway distribution system, by "stepping up voltage and reducing current," becomes an ideal solution to these pain points.
 
When transmitting the same power, the current at 800V is much lower than at 54V, thereby reducing I²R losses by 45% to 70%, and the conductor volume is significantly reduced, freeing up more space for computing devices such as GPUs. In addition, the modular design enables faster installation, simplifies deployment, and significantly reduces long-term total cost of ownership (TCO).
 
As the "aorta," the 800V DC busway distribution system undertakes the critical task of linking the upper and lower levels. It features efficient power transmission and distribution, delivering high-voltage DC power from the SST to the distribution boards of each cabinet with extremely low losses. Compared with traditional solutions, end-to-end efficiency can be improved from 85%-88% to over 93%. In addition, it can simplify the power supply chain. Through "integrated DC busway distribution system design," the number of conversion stages from grid to chip can be reduced from 6 to 3, significantly reducing system complexity and failure points. On the other hand, by reducing the size of power supply equipment, more cabinet space is freed up for core computing devices such as GPUs and switches, directly improving computing density per unit area.

PCIM 2026-Page 2 Busway-Demo 1

In the 800VDC architecture, Molex's 18-channel industrial battery management system (BMS) connector solution plays the role of the "interconnection foundation for system nerves and bones." It is not the core computing or sampling component of the BMS, but rather the key physical layer device that reliably connects the BMS motherboard to sensors, acquisition boards, and communication modules within the battery pack. These connectors cover the complete link from signal acquisition inside the battery pack to external communication of the BMS. They are mainly based on the following common advantages, including the space efficiency of the Mini50 series, 2.00mm compact pitch, -40°C to +105°C wide temperature range, latching and anti-mismating  design, and other design features that enable the BMS to operate stably in 1500V high-voltage systems.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 2

In 800VDC data center architectures, Nexperia's 10kW solar inverter reference design plays the core role of a "green energy access gateway." It efficiently converts DC power generated by photovoltaic panels into 800V DC power, integrating it into the data center's DC bus. This is a critical link for AI factories to achieve green power supply and reduce operating costs. This reference design is a complete 10kW hybrid photovoltaic inverter system, directly serving the green energy strategy of AI factories. It supports clean energy grid integration, enables peak shaving and valley filling, and maximizes power generation efficiency. To achieve efficient, high-density green energy access, it supports high power and high voltage, efficient topologies with fanless design, and comprehensive digital control. Through advanced semiconductor technologies such as SiC and GaN, it achieves efficient, high-power-density energy conversion, helping to achieve sustainable, energy-efficient operational goals.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 3.

In 800VDC data center architectures, Nexperia's 10kW three-phase T-type inverter reference design plays the core role of a "high-efficiency bidirectional power router." It is responsible for efficiently converting DC power from photovoltaic arrays or energy storage batteries into three-phase 380Vac AC power. When working in coordination with the 800V DC busway, it becomes a key hub connecting green DC energy sources and the data center's AC infrastructure. As the core of the 10kW hybrid photovoltaic inverter system, this T-type inverter serves as a bidirectional bridge connecting the DC bus to AC loads and the grid. It can supply power to AC loads, enable grid interaction, and improve power quality. Through its advanced T-type topology and Nexperia's 1200V SiC MOSFETs, it achieves efficient, bidirectional, high-quality energy conversion, helping to achieve sustainable, energy-efficient operational goals.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 4.

In the 800VDC architecture, the 1500V BESS (Battery Energy Storage System) reference platform jointly launched by NXP and eInfochips is a complete, mass-producible high-voltage battery management system (BMS) development platform, providing AI data centers with intelligent management capabilities for megawatt-level energy storage, backup power, and grid interaction. In the 800VDC data center power supply ecosystem, this 1500V BESS platform undertakes three key tasks, including the "central brain" of the energy storage system (ESS), the "execution hub" for grid interaction and peak shaving, and the "first line of defense" for thermal runaway and safety protection. Through high-precision cell monitoring, redundant current detection, thermal runaway early warning, functional safety compliance, and modular and scalable hardware and software architecture, it provides AI factories with safe, reliable, and intelligent energy storage and backup management capabilities.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 5

In the 800VDC data center architecture, onsemi's 1000V auxiliary power reference design plays the key role of the "low-voltage power supply cornerstone on the high-voltage DC busway side." It provides stable, isolated low-voltage DC power (12V) for auxiliary systems such as control circuits, drive circuits, sensors, fans, and BMS monitoring boards on the 800V DC busway side, and is the foundation for ensuring the normal operation of the "brain" and "nerves" of the entire high-voltage power supply system. onsemi's 1000V auxiliary power reference design, through 1700V SiC MOSFET for high-voltage input, flyback topology for isolated conversion, and synchronous rectification for efficiency improvement, provides reliable 12V control power for high-voltage equipment such as SSTs, DC busways, and energy storage BMSs, and is the behind-the-scenes hero ensuring the "safe, stable, and intelligent" operation of the entire high-voltage power supply system.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 6.

In the 800VDC data center architecture, this human-machine interface (HMI) reference design for photovoltaic inverters and energy storage systems plays the core role of a "local monitoring and intelligent operation and maintenance terminal." It does not directly participate in power conversion, but rather provides real-time status display, parameter configuration, cloud data upload, and local interactive control capabilities for key equipment in the 800VDC power supply chain, such as photovoltaic inverters, MPPT converters, and energy storage systems (ESS), through multiple communication interfaces including CAN-FD, RS485, Ethernet, and Wi-Fi/BT. It is the "visualization window" connecting operation and maintenance personnel with the high-voltage power system. In a typical green power supply ecosystem for 800VDC AI data centers, this HMI plays the roles of local real-time monitoring, intelligent operation and maintenance interaction, and cloud data bridge.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 8

In the 800VDC data center architecture, NXP's AFCI (Arc Fault Circuit Interrupter) solution plays the important role of a "safety sentinel." It uses edge AI technology to specifically detect dangerous arc faults in DC circuits and quickly disconnects the circuit before they cause fires or equipment damage. It is a key component providing active safety protection for high-voltage DC distribution systems. Unlike traditional protection methods that rely on manual inspection or post-event handling, NXP's AI AFCI solution undertakes tasks in the 800V high-voltage DC system such as actively preventing electrical fires, protecting critical equipment safety, and ensuring operator safety. It is not a single chip, but a complete solution combining high-performance hardware, advanced AI algorithms, and an easy-to-use toolchain.
 
Click here to view related information

PCIM 2026-Page 2 Busway-Demo 23

In the 800VDC data center architecture, Molex's heavy-duty connectors (HDC) play the key role of a "high-reliability modular power interface." They are the physical-layer links for the "last few meters" connecting core equipment such as power distribution units, energy storage systems, and server cabinets. Facing the challenge of surging power density in AI data centers, Molex HDC's roles are mainly reflected in high-density power transmission hubs, all-in-one "universal sockets," and "reliable guardians" in harsh environments. Molex's heavy-duty connectors, through features such as high voltage/current carrying capacity, extreme environmental adaptability, and modular flexible design, reliably connect core equipment such as SSTs, busways, and energy storage into an integrated whole.
 
Click here to view related information

Article tags

Global
Article
Articles and Videos

Related Content