Comprehensive healthcare solutions for precise protection of life
As the global population ages, the prevalence of chronic diseases continues to rise, and awareness of telemedicine and home care grows, medical and healthcare devices are accelerating their evolution toward four key directions: miniaturization, portability, intelligence, and high reliability. From continuous glucose monitors (CGM) and smart injection pens to life-support equipment such as ventilators and defibrillators, every innovation relies on the precision, stability, and safety of underlying electronic components. This article will systematically introduce Littelfuse's key technologies and products from two main application axes - therapeutic devices and personal monitoring devices - and provide an in-depth analysis of the unique value of TMR magnetic sensors, tactile switches, and circuit protection and power management product lines.
Comprehensive solutions for therapeutic devices and personal monitoring devices
In the field of healthcare equipment, devices must operate uninterrupted for extended periods in harsh environments, and any malfunction can directly impact patient safety. Littelfuse offers comprehensive solutions in the healthcare field, ranging from circuit protection and power control to precision sensing, and plays a critical role especially in two high-growth areas: therapeutic devices and personal monitoring devices.
In terms of therapeutic devices, Littelfuse provides core components that ensure uninterrupted operation for ventilators and defibrillators. Because ventilators require stable power supplies and motor control, PolySwitch® resettable devices are needed for battery overcurrent protection to prevent thermal runaway caused by short circuits; Schottky diodes prevent battery reverse connection and ensure correct system polarity. In defibrillator applications, the high-voltage discharge circuit inside the defibrillator must be protected against electrostatic damage; ESD suppressors and TVS diode arrays can absorb transient surges, while tactile switches are used on the control panel to ensure medical staff can issue commands precisely, protecting both the circuit and personnel safety.
In addition, for smart injection pens, which require precise control of drug dosage, Littelfuse's miniature detection switches (such as the HDT series) can detect the rotational position of the dose dial, while TMR magnetic sensors (such as the LF21173) are used for linear displacement measurement of the push rod, converting mechanical position into electrical signals sent back to the microcontroller, enabling precise monitoring of drug delivery. These sensor components are extremely small and consume only about 200 nA, making them highly suitable for battery-powered wearable devices.
Furthermore, due to the limited space within the ear canal, hearing aids impose extremely high requirements on component size. The NanoT series tactile switches, with their compact 2.1 mm x 1.65 mm package, provide reliable tactile feedback for volume adjustment and power on/off; while eFuse integrated protection ICs (such as the LS0504EDD12) provide overcurrent and overvoltage protection at USB-C charging ports, preventing safety issues caused by abnormal lithium battery charging.
For personal monitoring devices, particular emphasis is placed on prolonged continuous use, comfort, and data accuracy, with power consumption being a primary design consideration. For example, continuous glucose monitors (CGM) must be attached to the skin for days to weeks; internally, they can use TMR switches (1.5 mm square) as system wake-up triggers. When the user approaches the reader, the sensor responds in real time with an ultra-low power consumption of 160 nA, significantly saving battery life. At the same time, NTC thermistors (such as the KR series) monitor ambient temperature to provide temperature compensation for glucose readings, ensuring that measurements are not affected by body temperature changes. Additionally, ESD/TVS diodes and thin-film fuses are integrated on the circuit board to protect the sensor chip from electrostatic discharge or charging abnormalities.
Moreover, for wearable injectors (such as insulin pumps), these devices also employ TMR technology for push-rod position sensing to achieve precise control of micro-dose drug delivery; while Reed Switches in the system consume zero power in the static state, further extending battery life and meeting the demands of nighttime or prolonged infusion needs.
Littelfuse ventilator system solution
Providing comprehensive technology products for healthcare applications
When classified by core technology products, Littelfuse offers, in circuit protection, PolySwitch® resettable fuses, TVS diode arrays (such as the SPxx series), ESD suppressors, and more. PolySwitch® resettable PPTC fuses can sharply increase impedance during overcurrent or overtemperature conditions to cut off current, and automatically recover after the fault is cleared, eliminating the need to replace fuses. They are available in various packages including surface-mount and Battery Strap types, providing over-temperature, overcurrent, overvoltage, and ESD protection for ventilator battery packs, USB charging ports, motor winding protection, and rechargeable batteries.
TVS diode arrays (such as the SPxx series) and varistors (MLA) feature extremely low capacitance, protecting high-speed data ports (USB, Ethernet) from ESD and lightning surge damage, with response times reaching the picosecond level, ensuring signal integrity in defibrillators and portable ultrasound devices. In addition, polymer ESD suppressors (PGB series) are suitable for antenna or high-frequency interfaces that are sensitive to capacitance, providing ESD protection without adding signal attenuation.
In power control, Littelfuse offers power semiconductors (such as MOSFETs and Schottky diodes) for AC-DC power conversion, DC-DC buck-boost circuits, and BLDC motor drives (such as in ventilator BLDC motors). Their low on-resistance and fast switching characteristics reduce power dissipation and system heat generation, which is especially critical for medical instruments that operate for long periods. Furthermore, Littelfuse's gate drivers provide sufficient drive current to ensure power transistors operate within safe operating areas and integrate protection features such as under-voltage lockout (UVLO) and over-temperature shutdown.
In sensing and switching applications, Littelfuse offers TMR sensors (LF21173), tactile switches (NanoT, KSC2 series), and detection switches (HDT, FDSD series). TMR sensors are primarily used for position detection and non-contact wake-up. Tactile switches (NanoT, KSC2 series) are available in various operating forces and size options to meet different tactile feel requirements, suitable for operation keys on handheld diagnostic devices. Detection switches (HDT, FDSD series) can be used for pen cap removal detection, skin contact sensing, and user interface control activity detection, helping the system determine whether the device is in use and switch operating modes to save power.
In healthcare applications, the design priority is the safety and reliability of medical equipment. Medical devices must comply with safety standards such as IEC 60601, which impose strict requirements on leakage current, dielectric withstand voltage, and fault risks. Littelfuse's protection devices undergo rigorous AEC-Q or medical-grade certifications (such as FDA requirements), effectively preventing system crashes or fires caused by overloads, short circuits, and ESD events, providing an extra layer of protection for patients and operators.
In the trend toward miniaturization and low power consumption, wearable and implantable devices continuously challenge space limitations. Littelfuse's TMR sensors and NanoT switches, with wafer-level packaging or ultra-thin designs, deliver full functionality within millimeter-scale spaces; at the same time, their nA-level quiescent current allows devices to operate continuously for weeks or even months without frequent recharging, greatly enhancing user experience, making them key to meeting the stringent space and battery life requirements of wearable and portable devices.
In terms of connectivity and data security, with the booming growth of the Internet of Medical Things (IoMT), devices must have wireless capabilities such as Bluetooth and Wi-Fi. Littelfuse provides ESD protection devices suitable for antenna ports, ensuring RF performance is not compromised while protecting communication chips from electrostatic damage and maintaining data transmission stability.
Littelfuse solution for Continuous Glucose Monitors (CGM)
TMR magnetic sensors and switches for precision sensing
Littelfuse's product portfolio is quite extensive, and the following will provide an in-depth introduction to several key products for medical applications. First are the TMR magnetic sensors and switches for precision sensing, whose core technology employs Tunnel Magnetoresistance (TMR) technology, operating by changing resistance in a magnetic field. Compared with traditional Hall-effect sensors, the advantages in power consumption and sensitivity are very significant. Key products include the LF21173TMR and LF21177TMR ultra-low-power omnipolar TMR magnetic switches.
The LF21173TMR and LF21177TMR feature ultra-low power consumption, drawing only 160 nA in low-power mode, which is crucial for battery-dependent wearable devices such as CGM and smart injection pens that must operate continuously for days, maximizing battery life. In addition, these two products offer high sensitivity, capable of detecting magnetic field changes as low as 9 gauss. In healthcare applications, this allows the use of smaller, less expensive magnets to achieve reliable non-contact "wake-up" or position detection, simplifying mechanical design.
On the other hand, these two products support omnipolar detection, responding to both south and north poles of a magnet. This simplifies the placement of magnets within the device, providing engineers with greater design flexibility. Additionally, the LF21173TMR and LF21177TMR come in a compact LGA-4 package, meeting the stringent PCB space requirements of portable medical devices. These products also support non-contact operation, sensing through sealed housings without mechanical contacts, which enhances the device's water and dust resistance (IP67), eliminates mechanical wear, and significantly improves long-term reliability.
Littelfuse defibrillator solution
Tactile switches for user interface and interaction in healthcare devices
For user interface and interaction applications in healthcare devices, the NanoT tactile switch can be used, providing reliable tactile feedback and IP67 protection rating in an extremely small footprint. The NanoT series features an ultra-compact design, with top-actuated models measuring only 2.1 x 1.65 x 0.55 mm, making it one of the smallest tactile switches on the market, significantly saving PCB area and suitable for space-constrained devices such as hearing aids and smart wearables. Additionally, the NanoT series supports IP67 water and dust protection, resisting sweat, liquids, and dust, ensuring long-term reliability in complex usage environments.
On the other hand, the NanoT series offers excellent design flexibility, with options for 100gf, 160gf, and 240gf operating forces, as well as top- or side-actuated models. Engineers can flexibly choose based on the desired tactile feel of the product (such as preventing accidental activation or providing a light touch) to optimize user experience. Furthermore, the NanoT series features high durability, with an operating life of up to 200,000 to 300,000 cycles, ensuring stable and reliable switch function throughout the device's lifecycle and reducing maintenance costs.
Auto-injector or infusion pen block diagram
Circuit protection and power management product lines ensuring safe and stable operation of medical devices
In circuit protection and power management, this product line is very extensive, ensuring safe and stable operation of medical devices. For resettable overcurrent protection, Littelfuse's PolySwitch® resettable PPTC devices can trip during overcurrent or overtemperature conditions and automatically recover after the fault is cleared, without the need for replacement. Available in various forms including surface-mount and Battery Strap types, they can be used for ventilator battery protection, portable device USB ports, motor and transformer protection, and rechargeable battery packs.
For ESD/surge protection, Littelfuse offers TVS diode arrays, varistors (MLA), and polymer ESD suppressors (PGB series). With ultra-low capacitance, they can protect high-speed data ports, quickly respond to electrostatic discharge, and protect sensitive circuits from damage. They are widely used in defibrillators, portable ultrasound devices, device data ports (USB, Ethernet), and user interface interfaces.
In power control, Littelfuse provides product lines including MOSFETs, Schottky diodes, and gate drivers, supporting efficient power conversion, motor drive, and reverse polarity protection while reducing system heat generation. They can be used in ventilator motor drives, portable device power management, and defibrillator power rectification.
For temperature monitoring applications, Littelfuse's NTC thermistors (such as the 0803-KR and 0603-RB series) provide precise temperature measurement for equipment thermal safety monitoring and sensor temperature compensation, such as temperature compensation for glucose measurements in CGM, ventilator overheat protection, and ensuring that device surfaces in contact with patients are at safe temperatures.
Conclusion
With a comprehensive product portfolio spanning circuit protection, power management, and precision sensing, Littelfuse has successfully embedded itself in everything from life-support equipment to daily health monitoring. Whether it is the reliable protection of PolySwitch® resettable fuses, the ultra-low-power precise positioning of TMR sensors, or the miniaturized interactive design of NanoT tactile switches, all reflect the core value of "protecting life through technology." As medical devices continue to move toward greater intelligence and personalization, Littelfuse will continue to provide high-quality, highly integrated solutions to help developers worldwide create the next generation of safer, more user-centric healthcare electronic systems.
Article tags