Capacitive rotary encoders enhance energy efficiency in mobile robotics
With the rapid advancement of smart manufacturing and logistics automation, mobile robotics have found widespread applications in warehouse handling, inspection, and smart factory environments. In these applications, both the efficiency of drive systems and positioning accuracy directly impact overall operational energy consumption and work performance. Rotary encoders, serving as critical sensing components in motor control and feedback systems, deliver precise velocity and position information that enables controllers to make real-time adjustments. This article examines the most common encoder technologies and their expanding role in the autonomous mobile robotics market, while highlighting the features and capabilities of Same Sky's AMT series rotary encoders.
High-efficiency encoders enable energy savings and enhance robotic mobility
Commercial mobile robotics are generating substantial markets for both equipment and related services. According to recent research projections, the aerial drone segment alone is expected to exceed $50 billion by 2030. On the ground, mobile robots are being deployed across industrial, commercial, and domestic settings to perform tasks with greater speed and cost-effectiveness than human workers, to function in environments unsuitable for people, or to collaborate with humans by handling repetitive or physically demanding jobs.
The mobility requirement drives the need for battery-powered operation, making overall vehicle energy efficiency critically important for maximizing operational range. Careful management of limited power resources proves essential for enabling robots to work longer or travel farther on a single charge. This holds true whether considering a drone needing maximum flight distance for food delivery, a warehouse assistant requiring maximum uptime to improve operator profitability, or a domestic robot like a vacuum cleaner or lawnmower whose market appeal directly correlates with how much work it can accomplish between charges. Greater efficiency also provides designers additional flexibility in managing cost, size, and weight by allowing robots to achieve greater range with smaller batteries.
Achieving these objectives makes encoder selection particularly important, as these devices capture the position information controllers need to execute motor vector-control algorithms, and this choice significantly influences system energy efficiency. In multi-motor configurations, the energy savings achievable by selecting efficient encoders can substantially reduce overall power requirements. Among currently available encoder technologies, capacitive models not only boost efficiency but also enhance reliability, reduce maintenance needs, lower development expenses, and accelerate time-to-market.
Distinctive characteristics of optical and magnetic encoders
Meaningful improvements in flight range or operating time require accumulating numerous small power savings across all onboard subsystems. Since mobile robots often incorporate multiple electric motors to drive actuators or positioning mechanisms such as camera gimbals, even modest efficiency gains in motor controllers can yield substantial overall benefits. Motor control and commutation critically depend on knowing the rotor's angular displacement at any given moment. Optical and magnetic encoders represent two popular approaches for accomplishing this task, though each comes with certain drawbacks.
Optical encoders combine an LED light source with an optical sensor arrangement that detects light transmitted through or reflecting from a code wheel mounted on the motor shaft. Two LEDs positioned in quadrature enable simultaneous detection of both motor speed and direction. A third LED may monitor a single marking on the code wheel to provide an indexing pulse to the motor control system.
Optical encoders consist of an LED light source, receiver, and code wheel
Encoder resolution, expressed in pulses per revolution (PPR), depends on the number of precisely spaced markings on the code wheel. While optical encoders can achieve very high resolution, they also suffer from several vulnerabilities. These include susceptibility to dust, grease, or condensation accumulating on the code wheel, which can cause missed or false readings. Additionally, LED brightness diminishes over time and ultimately fails, creating encoder failure that requires replacement as the only remedy.
Regarding energy efficiency, optical encoders do draw relatively high current, which increases at higher resolution settings and with more complex output signal formats. In fact, current consumption can more than double when moving from the lowest to highest resolution. Some optical encoders draw as much as 85 mA at maximum resolution. While this may seem insignificant compared to motor power consumption, at 5 V and 85 mA the encoder consumes 0.425 watts. In a four-motor system, the encoders alone account for 1.7 watts. Reducing this drain on battery energy could allow the application to power other systems such as onboard cameras, sensors, or small actuators for extended periods.
Magnetic encoders offer an alternative that requires no line-of-sight operation and therefore resists contamination-related errors. Furthermore, magnetic encoders can function even when submerged in non-conductive fluids like gear oil. On the downside, positional resolution and accuracy typically fall below those of optical encoders. Depending on the magnetic encoder type, maximum current can range from 20 mA to 160 mA or higher.
Capacitive-based rotary encoders deliver superior energy efficiency
Same Sky's AMT rotary encoders, built on capacitive technology, provide an energy-efficient alternative solution. Operating on the same principle as digital Vernier calipers, the sensor consists of a fixed body and a moving element that together form a variable capacitor. As the encoder rotates, this capacitor generates a unique yet predictable signal that can determine shaft position and rotation direction. With onboard processing, the ASIC and a microprocessor can work together to produce more complex outputs, such as commutation pulses required for brushless DC (BLDC) motors or serial outputs for absolute encoders.
Capacitive encoders operate on the same principle as digital Vernier calipers
Image sensors designed for exceptional depth sensing and imaging
The capacitive operating principle allows the encoder to maintain accuracy in dusty or dirty environments, such as warehouses, factory floors, or outdoor equipment deployments. Like magnetic technology, capacitive encoders can also be submerged in non-conductive fluids such as gear oils, eliminating expensive code wheel enclosure sealing and minimizing routine cleaning or disk replacement needs often required with optical encoders. Meanwhile, capacitive encoders deliver equivalent or superior accuracy compared to other encoder technologies, with typical accuracy of 0.2 degrees.
Regarding energy efficiency, AMT capacitive encoders offer substantial advantages. For example, the AMT10 and AMT10E encoders draw less than one-tenth the current of comparable optical encoders, yielding significant system power savings. Specifically, the AMT10 and AMT10E consume only 0.12W when operating at 5V and 6mA in a four-motor system. As mentioned earlier, certain optical encoders consume as much as 1.7W in a similar four-motor system, while magnetic encoders can consume as much as 3.2W, making the AMT10 and AMT10E clearly superior in overall efficiency. Beyond the AMT10 and AMT10E series, Same Sky's other AMT series incremental, absolute, and commutation capacitive encoders require only 5V and 16mA, still delivering substantial power savings compared to optical and magnetic alternatives.
Capacitive rotary encoders not only save enough power to meet all requirements of other onboard subsystems, but also need less maintenance than optical encoders, which may require cleaning to restore accuracy. Magnetic encoders, though rugged, typically offer lower accuracy than optical or capacitive types and consume nearly twice the power of an optical encoder.
When robots incorporate multiple motors for various tasks, replacing all optical or magnetic rotor position encoders with capacitive versions can significantly reduce overall power consumption, freeing up capacity for subsystems like GPS modules, wireless communications, or sensing, allowing more battery energy to extend the vehicle's operational range.
Capacitive absolute encoders are also gaining popularity in robotics applications, exemplified by Same Sky's AMT21, AMT22, and AMT24 series. While both incremental and absolute encoders can measure rotating shaft speed, direction, and position, absolute encoders offer the additional capability of outputting shaft position at any time, including at power-on, eliminating the homing sequence required for incremental encoders. Furthermore, absolute encoders deliver true real-time position with minimal latency, making them ideal for autonomous mobile robotics applications requiring precise position data.
The AMT series modular encoders feature rugged construction, operating across -40°C to 125°C temperature ranges while resisting dust, dirt, and oil without requiring additional covers, lids, or seals for protection, making them suitable for vacuum and high-pressure environments. Functionally, they offer flexibility and convenience, supporting up to 22 programmable resolutions, with sleeve bore options ranging from 1 to 15.875 mm (5/8 inch), simple assembly, and multiple line driver and connector choices. Additionally, AMT encoders provide energy-efficient operation with low current draw, minimal rotation power requirements thanks to low-mass internal rotors, and compact packaging. These benefits of the AMT series modular encoders combine to give engineers greater flexibility during prototyping without requiring additional units, while enabling purchasing managers to significantly reduce production SKU counts.
Same Sky AMT modular encoder
Capacitive rotary encoders play a vital role in mobile robotics
As mobile robotics become increasingly prevalent, the demand for battery-powered operation grows accordingly. With market evolution and rising end-user expectations, every milliampere-hour of battery energy grows increasingly valuable. Moreover, current mobile and aerial platforms integrate numerous electric motors, not only for driving wheels or rotors but also for various positioning mechanisms and actuators requiring multi-axis motion control. Motor power consumption ranges from several watts in small positioning mechanisms to tens of watts or considerably more for traction or lifting applications. Each motor pairs with a driver/controller unit that also dissipates significant power. Reducing power consumption in each motor system frees more battery energy for productive work, and the cumulative effect across multiple motors delivers meaningful advantages for building robots that travel farther on smaller batteries.
Affordable automation through small mobile robots and civilian drones will continue transforming manufacturing, distribution, and asset management operations. Capacitive-based rotary encoders stand to make meaningful contributions to this exciting mobile robotics revolution, unlocking energy savings beyond what many might expect. More broadly, they help manufacturers across diverse application areas meet efficiency regulations such as the EU's IEC 60034-30-1 standard defining efficiency levels for three-phase induction motors. Thanks to these compact, energy-efficient devices, motor-driven equipment worldwide can operate longer while consuming less energy than ever before.
Conclusion
Against the backdrop of increasing demands for high efficiency, extended battery life, and precise control in mobile robotics, rotary encoders have evolved beyond simple position feedback devices into components critically influencing overall energy performance. By incorporating higher-resolution sensing technology, low-power signal processing architectures, and more reliable digital communication interfaces, capacitive rotary encoders enable motor control systems to achieve more accurate speed and position regulation while reducing unnecessary energy consumption and mechanical losses. Same Sky's AMT series rotary encoders will play increasingly important roles in efficient drive systems and energy management for mobile robots, further advancing the development of energy-efficient and intelligent mobile robotics platforms.
Article tags