Rapidly evolving high voltage hot swap protection and telemetry technologies for AI servers
As GPU power consumption continues to rise, the power demands in AI server environments are growing relentlessly, driving the transition of power delivery architectures from 48 V toward 800 V and propelling the evolution of AI data center infrastructure. This high-voltage architecture introduces new challenges for system protection and monitoring, particularly during live tray insertion and removal. This article will introduce the future development trends of data center hot swap controllers, as well as Analog Devices' continuous innovations in high voltage hot swap protection.
The future of hot swap controllers in data centers
As AI workloads intensify, GPUs in server environments are driving unprecedented power demands, pushing rack-level power delivery architectures toward 800 V, which imposes stringent challenges on system protection and monitoring for servers. To address these challenges, a next-generation hot swap controller is required - one that is not only capable of managing high voltage inrush currents but also provides robust telemetry for system diagnostics and safety.
In AI server infrastructure, two key trends are driving the transition to higher voltage power delivery at the rack level. The first is rising GPU power consumption: as GPUs continue to scale in compute performance, their power requirements are increasing significantly. The second is higher compute density per rack: to maximize performance and minimize interconnect latency for large-scale AI training and inference, more GPUs are being consolidated within a single rack. This co-location improves bandwidth efficiency and reduces communication overhead by shortening data paths between accelerators.
To meet the resulting surge in rack-level power demand, the industry is moving toward a disaggregated power architecture. In this model, traditional power components such as power distribution units (PDUs), battery backup units (BBUs), and capacitor units (CUs) are relocated from the main IT rack to an adjacent power sidecar. This separation not only supports higher voltage delivery, such as 800 V, but also frees up valuable space within the rack for additional compute resources.
Existing AI racks operate with a 48 V busbar for power delivery. AC is converted to 48 VDC using in-rack power supply units (PSUs). The 48 V bus feeds IT equipment (server PSUs, GPU nodes, switches), BBUs with their own bidirectional DC-to-DC converters, and supercapacitor units (SCUs) for fast ride-through and transient handling.
Each node on a rack (for example, a server tray) requires the capability to be switched in and out during live operation. Imagine a service technician arriving on site to replace a server. It's not practical to shut the entire rack down just to replace a single server. Doing so would be hugely intrusive to the operation of the data center, not to mention enormously expensive due to server downtime. The only time a rack would be taken offline is for a major electrical issue, related to the busbar or facility feed, etc. Instead, nodes are hot swapped, allowing the technician to remove the node, swap it, and push it back in without shutting anything else off.
During this event, the node's hot swap controller disconnects power internally, allowing the node to be removed safely. The rack's busbar stays energized and continues feeding all other nodes, BBUs, and SCUs. Once a replacement node is inserted, precharge circuits limit inrush before full connection, a key function of the hot swap controller. The node then boots and rejoins the AI cluster automatically (often with orchestration tools handling rebalancing).
48 V AI server
Rising power demand drives the transition to higher rack-level voltages
The primary driver for transitioning to higher rack-level voltages is the escalating power demand per rack. As power increases, so does the current flowing through the busbars. This rise in current necessitates larger and heavier busbars to maintain acceptable thermal and electrical performance - posing significant challenges in terms of mechanical practicality and system design. By increasing the delivery voltage, the required current can be proportionally reduced, enabling the use of more compact and manageable busbar dimensions and interconnects. This shift to higher voltage is essential for maintaining scalable, efficient, and mechanically feasible power distribution in next-generation AI server racks.
It's worth noting there can exist intermediary steps in this architecture evolution where a 48 V busbar is used in the rack. In this case, PSUs are scaled to higher powers, accepting ±400 V/800 V at the rack and down converting to 48 V to marry with existing busbars. However, this is not a longer-term state as power will be limited (maybe up to 250 kW per rack) and the goal is to allow for maximum compute capability in a single rack, driving power to 1 MW per rack by the end of the decade. PSUs and BBUs are therefore best positioned outside of the IT compute rack. In the future, solid-state transformers are likely to be used to distribute high voltage directly to each IT compute rack without the need for these sidecars.
To achieve high voltage hot swap, many design considerations must be understood and technical challenges overcome to create the optimum solution. First, power density is a critical factor, as the ±400 V/800 V hot swap circuitry ultimately resides on the server card within the IT rack. Space on these cards is highly valuable and will face growing constraints as rack densities increase, fitting more servers into each rack. As a result, high voltage hot swap solutions must be designed to occupy the smallest possible footprint.
In addition, high voltage control and protection is another key factor, as the transition to ±400 V and 800 V in data centers introduces significant safety challenges. While 48 V poses minimal shock risk, these higher voltages can be life-threatening. Consequently, hot swap circuitry must handle large current surges within microseconds, making precise control essential. Managing the inrush current ramp is critical to avoid damage to the rack or harm to technicians. The system must also coordinate timing, detect overcurrent or undervoltage events, and shut down gracefully when required.
Furthermore, telemetry is an important application requirement for high voltage control. As the first component in the node's power path, hot swap controllers are ideally positioned for data acquisition. They must precisely measure voltage, current, and power to meet system specifications, while also logging events such as overcurrent, undervoltage, and thermal shutdowns. In addition, they should report temperatures from the power switch (MOSFET) or nearby PCB areas. Accurate hot swap telemetry delivers significant system value by enabling real-time load current profiling, which improves energy demand forecasting. Historical current data collected at the hot swap supports predictive maintenance, such as identifying a failing PSU before it trips, and feeds into rack-level capacity planning models for power distribution.
Data center ±400 V/800 V rack power delivery architecture
ADI develops next-generation rack-level high voltage power delivery solutions
ADI has extensive expertise across the data center power domain and is collaborating with cloud service providers and semiconductor manufacturers to develop next-generation rack-level high voltage power delivery solutions. ADI is a recognized leader in hot swap technology at 12 V and 48 V, and is now extending its expertise to support the industry's transition to 800 V.
A new voltage distribution domain is defined to the rack - ±400 V or 800 V - fed from a sidecar directly to the IT rack. ADI is actively developing new high voltage hot swap controller solutions to support emerging rack-level power architectures. By leveraging its proven intellectual property in power protection and telemetry, ADI is extending its capabilities into the ±400 V and 800 V domain. In collaboration with leading data center OEMs and power switch vendors, ADI's next-generation solutions are engineered to meet the evolving requirements of hot swap systems - including compact form factors, precise high power control, and enhanced data acquisition accuracy. These innovations are critical for enabling safe and efficient operation in high voltage AI server environments.
LTC4286 circuit diagram
ADI offers multiple product families supporting hot swap technology
ADI has a deep portfolio of 48 V hot swap controllers with PMBus® power monitoring, such as the LTC4286 and LTC4287, which are pin-to-pin 7 mm × 7 mm QFN hot swap controllers with single and dual gate architecture. Most recently, the LTC4284 dual gate solution in a 5 mm × 8 mm QFN package was added to this portfolio.
The ADI LTC4286 and LTC4287 are integrated solutions for hot swap applications that allow a board to be safely inserted and removed from a live backplane. The LTC4286 uses a circuit breaker timer to limit MOSFET temperature, while the LTC4287's dual-gate drivers coupled with configurable multimode startup sequencing and operation optimize the MOSFET safe operating area (SOA) for a variety of power levels. Both provide reliable protection against MOSFET overheating and overstress.
Both the LTC4286 and LTC4287 support the SMBus 3.1 interface, PMBus command structure, and onboard ADCs with selectable averaging and speed, allowing monitoring of board current, voltage, power, temperature, and fault status. The LTC4286 has additional features to respond to input undervoltage (UV) and overvoltage (OV): it interrupts the host when a fault occurs, notifies when output power is good, detects insertion of a board, and auto-reboots after a programmable delay following a host commanded turn-off. The LTC4287 features an optional external EEPROM for part configuration and BlackBox capturing of past fault conditions, along with multiple additional features including response to input UV/OV, host interrupt on fault, power-good notification, board insertion detection, MOSFET turn-off if an external supply monitor fails to indicate power-good within a timeout period, and auto-reboot after a programmable delay following a host commanded turn-off.
The ADI LTC4284 is a negative voltage hot swap controller that drives external N-channel MOSFETs to allow a board to be safely inserted and removed from a live backplane. The dual-gate, multi-mode drivers optimize the MOSFET safe operating area (SOA) for a variety of power levels. The SOA timer limits MOSFET temperature rise for reliable protection against overstresses, and it supports an I²C interface and onboard gear-shift ADC for monitoring board current, voltage, power, energy, and fault status. An available single-wire broadcast mode simplifies the interface by eliminating two isolators, and the included EEPROM provides black-box capturing and nonvolatile configuration of fault behavior.
Additional LTC4284 features include response to input UV/OV, host interrupt on fault, power-good notification, board insertion detection, MOSFET turn-off if an external supply monitor fails to indicate power-good within a timeout period, and auto-reboot after a programmable delay following a host commanded turn-off.
Conclusion
As AI server racks undergo a critical shift toward 800 V power delivery architectures - a transition aimed at meeting the growing power demands of advanced GPUs and supporting higher compute density - the new architecture moves power components to a separate sidecar, thereby optimizing space for compute resources in the main rack. ADI is at the forefront of this development, creating next-generation high voltage hot swap controllers that effectively manage inrush currents, offer comprehensive telemetry for system diagnostics and safety, and ensure reliable operation. By taking a system view to the evolution of rack power, developers can enable cloud server providers and system integrators to generate new insights and revenue savings.
Article tags