Arrow Electronic Components Online

The role of passive and magnetic components in ADAS applications

Arrow Times10 Jun 2026
Illustration of an Advanced Driver Assistance System (ADAS) around a top-view car.
View all articles

The rapid development of Advanced Driver Assistance Systems (ADAS) and autonomous driving technology is reshaping every layer of automotive electronic architecture. From multi-sensor fusion and high-computing-power decision-making units to stable and reliable actuators, modern intelligent vehicles impose unprecedented stringent requirements on the performance, reliability, and integration density of electronic components. Especially in key areas such as power management, signal transmission, electromagnetic compatibility, and high-frequency filtering, the failure of any tiny component could lead to system collapse or even endanger driving safety. This article introduces YAGEO's complete product portfolio, including polymer capacitors, MLCCs, wired communication components, and standard power magnetic components under its brands such as KEMET and Pulse, and discusses the roles, technical characteristics, and synergistic value of these four core product categories in ADAS and autonomous driving applications.

Polymer capacitors provide an energy buffer for high-power processors

The core function of polymer capacitors is to provide an "energy buffer" for high-power processors, ensuring that computing cores do not lose power. When GPUs or SoCs in ADAS domain controllers operate, current demand fluctuates dramatically within very short periods. With their extremely low equivalent series resistance (ESR), polymer capacitors can respond at nanosecond speeds, instantly releasing or absorbing large currents and effectively preventing processor crashes caused by sudden voltage drops. This characteristic is critical for meeting the ASIL-D requirement of the ISO 26262 functional safety standard.
 
YAGEO, through its KEMET brand, offers the T59x series of automotive-grade polymer tantalum capacitors (KO-CAP®), which play a key role as "power system stabilizers" and "performance enablers" in ADAS and autonomous driving applications. YAGEO/KEMET has built four core polymer capacitor series - T591, T597, T598, and T599 - to cover diverse needs ranging from high humidity resistance and small size to high temperature and long life.
 
Among them, the T598 series, with its ultra-low ESR of 6 mΩ, high ripple current capability of 8.7A, withstand voltage up to 75V, and maximum capacitance of 680µF, has become the most core component in ADAS/autonomous driving domain controller power systems.
 
YAGEO/KEMET's polymer tantalum capacitors (KO-CAP®) adopt a solid structure of "tantalum anode + Ta₂O₅ dielectric layer + conductive polymer cathode," and their technical advantages precisely address the stringent power requirements of ADAS systems: high-current, low-ripple, and highly reliable power supply for high-performance computing chips.
 
The T597 ultra-small product (3216-12) from the T59x series is already in mass production, compatible with MLCC 1206 package, providing engineers with a seamless replacement solution. Furthermore, YAGEO continues to expand its polymer capacitor product line, introducing hybrid polymer radial capacitors such as the A7C0/A7C5 series, with maximum operating temperatures up to 150°C, further covering high-temperature ADAS auxiliary applications like powertrains.
 
With core advantages such as ultra-low ESR, high capacitance, high volumetric efficiency, no DC bias or acoustic noise, and AEC-Q200 automotive qualification, YAGEO/KEMET's polymer capacitors are deeply embedded in key nodes of ADAS systems, including domain controller core power supply, sensor modules, and communication interface power filtering, providing a solid foundation for the stable and safe operation of L2+ to L4/L5 autonomous driving.

A sleek white concept car is shown in three-quarter front view with multiple labeled technology zones around the vehicle.

MLCCs play the role of mainstream high-frequency decoupling and filtering in power systems

As the most common passive components, MLCCs act as "ubiquitous guardians" in power systems, serving as the main high-frequency decoupling and filtering components. Placed near the power pins of digital chips such as SoCs, ASICs, and FPGAs, MLCCs use their extremely low equivalent series inductance (ESL) and excellent high-frequency characteristics to filter out power supply noise caused by high-speed switching of chips, providing a clean and stable power source.
 
YAGEO, as a global leading passive component supplier, offers a comprehensive range of automotive-grade MLCCs designed specifically for automotive electronics. These products have passed the stringent AEC-Q200 automotive qualification, and some models have even passed the more rigorous VW80808 automotive qualification, ensuring their long-term reliable operation under harsh automotive environments such as high temperature, high humidity, and strong vibration.
 
YAGEO's MLCCs are represented by four core product series in ADAS systems: The AC series is the "general-purpose workhorse," providing reliable power filtering and decoupling, covering a wide range of products including NPO (C0G), X7R, and other Class I and Class II dielectrics, with X6S and X5R high-capacitance series expanded to meet miniaturization needs. For example, the AC0603 series NPO capacitor features an ESL as low as 0.05nH at 1GHz and a self-resonant frequency (SRF) as high as 11.4GHz, making it ideal for high-frequency signal processing.
 
The AS/FT series acts as a "flexible guardian" for safety, mainly used in high-vibration areas to prevent capacitors from cracking due to mechanical stress. It features a flexible lead-free terminal design, providing up to 5mm of PCB bending withstand capability, effectively avoiding cracks caused by board bending or thermo-mechanical stress in traditional MLCCs, significantly improving reliability.
 
The AQ series serves as a "purifier" for high-frequency signals, mainly ensuring the purity and integrity of high-frequency signal chains. It uses NPO dielectric and features an extremely high Q factor (low dielectric loss) and very low ESR/ESL, making it an ideal choice for precision RF applications. Its product line covers 0402 (0.1pF ~ 100pF) and 0603 (0.2pF ~ 100pF) packages.
 
The High Voltage series (AC High Voltage) acts as a "solid backbone" for high-voltage platforms, mainly used in 800V high-voltage architectures to provide reliable filtering, snubbing, and protection for high-voltage circuits, offering DC voltage ratings up to 3000V and operating temperatures up to 150°C.
 
YAGEO's MLCC product line, through the universality of the AC series, the flexible reliability of the AS series, the high-frequency performance of the AQ series, and the voltage withstand capability of the High Voltage series, precisely covers every critical node in ADAS systems - from core computing power to front-end sensing, from low-voltage logic to high-voltage power grids - building a solid foundation for the stable and safe operation of autonomous driving.

Infographic illustrating various technology applications across consumer, networking, industrial, power, automotive, and medical sectors.

Wired communication components enable the fusion of power and data

Wired communication components are a key link in ADAS's move toward central computing combined with zonal architecture, with the core contribution being the fusion of power and data. They simplify sensor connections. Using Power over Data Line (PoDL) technology, the power and high-speed data of a single camera can be transmitted over a single pair of Ethernet wires (SPE), eliminating the need for separate power lines, greatly simplifying the vehicle's wiring network and reducing overall vehicle weight.
 
In the high-speed development of ADAS and autonomous driving, the real-time, reliable transmission of massive sensor data (e.g., from cameras and radar) to high-computing-power decision-making units is just as important as stable power supply. YAGEO Group's Pulse Electronics brand plays the role of a "nervous system builder," providing key wired communication components (including Ethernet transformers and common mode chokes) designed to ensure the smooth flow of data on the in-vehicle data highway.
 
Pulse's wired communication components feature automotive-grade qualification and high-standard manufacturing, passing AEC-Q200 certification - a "passport" for entry into the automotive supply chain - ensuring the long-term reliability of components under extreme temperature, humidity, vibration, and other environmental conditions.
 
Pulse's AE series of automotive Ethernet common mode chokes (CMC) have the core function of filtering common mode noise on differential signal lines, ensuring signal integrity, and are key filters for guaranteeing the reliability of high-speed data transmission links. Key selection parameters include common mode impedance, inductance, DC resistance (DCR), and rated current.
 
Pulse's HM series of automotive Ethernet transformers serve two main purposes: providing electrical isolation to prevent potential damage between different voltage domains, and signal coupling to ensure efficient, low-loss signal transmission. Key selection parameters include isolation voltage, turns ratio, insertion loss, and return loss.
 
Pulse's PE-1210ACC / PE-1812ACC series of CAN/CAN-FD common mode chokes are mainly used to filter common mode electromagnetic interference (EMI) on low-speed in-vehicle buses, especially suitable for protocols such as CAN, CAN-FD, A2B, and isoSPI, ensuring reliable communication. Key selection parameters include common mode impedance, DC resistance, and rated current, providing effective filtering without attenuating the differential signal.
 
YAGEO/Pulse's wired communication components, through the three major series AE, HM, and PE-ACC, precisely cover in-vehicle networks from 100M to Gigabit automotive Ethernet, CAN/CAN-FD, etc., supporting every key link from sensor fusion, backbone network transmission, to computing interconnect. When designing ADAS systems, you can select from the AE (choke), HM (transformer), and PE-ACC (CAN choke) series based on communication speed (e.g., 100M/1000M Ethernet vs CAN-FD) and functional requirements (common mode filtering vs electrical isolation) to ensure the performance and safety of the data link.

Technical infographic shows a blue wireframe car surrounded by labeled automotive electronic systems.

Standard Power Architecture Enables Efficient Power Delivery for ADAS Systems

In ADAS and autonomous driving systems, stable and highly efficient power delivery is critical to ensure reliable system operation. As a leading provider of magnetic components, YAGEO supports power management ICs (PMICs) and power modules with high-performance inductors and filtering products, enabling efficient power conversion and signal stability. These magnetic components help convert raw battery power into stable and regulated voltages required by electronic components, contributing to overall system efficiency (up to 97% at system level) while reducing power loss and thermal burden.
 
In power management, inductors are key components that directly impact conversion efficiency and system stability. High-performance inductors can ensure stable power supply and are the core of the power system. Taking the ADCC series as an example, its ultra-low RDC (down to 6.3 mΩ) and high saturation current (Isat up to 14A) make it well-suited for core power delivery in ADAS domain controllers, especially for GPU/SoC applications. Under high transient current conditions reaching tens of amperes, it effectively suppresses voltage drops and maintains stable output.
 
For camera and radar modules, compact package sizes (such as 2.0 × 1.6 mm) are available to meet space-constrained designs. On the high-current input side, the AMMx series molded power inductors (with Isat up to 118A) provide robust current handling capability and serve as critical components in the power conversion stage.
 
With the increasing demand for high-frequency and high-voltage applications, the widespread adoption of 48V architectures, and the increasing use of wide bandgap semiconductors such as SiC and GaN, switching frequencies in power systems are rising to MHz levels. This places higher demands on inductors in terms of core loss, thermal performance, and high-frequency characteristics. YAGEO addresses these challenges with product portfolios such as the APCA series, offering wide operating temperature ranges and low core loss characteristics, helping systems maintain stable operation in high-frequency and high-temperature environments.
 
In PoC (Power over Coax) applications, inductors play a key role in enabling simultaneous transmission of power and high-frequency data over a single coaxial cable. YAGEO’s APOC and AWCS series feature high Q factor and high self-resonant frequency (SRF > 2.45 GHz), helping minimize signal loss and maintain signal integrity (actual performance may vary depending on system design and configuration).
 
In ADAS systems, DC-DC converters are major sources of electromagnetic interference (EMI). YAGEO provides a comprehensive filtering portfolio, including APPM series common mode filters for power lines, AWCU series for CAN/CAN-FD and automotive Ethernet applications, and ABSY / ABUP ferrite beads for signal and power line noise suppression. These components effectively suppress common-mode noise and EMI interference, ensuring stable power delivery and reliable signal transmission in complex automotive environments and maintaining system stability.

Conclusion

Through this systematic review of YAGEO's four major product lines - polymer capacitors, MLCCs, wired communication components, and standard power magnetic components - it is clear that YAGEO's passive and magnetic components, though "invisible" in various corners of the circuit board, remain indispensable "enablers" and "guardians." For every engineer dedicated to building safe, reliable, and high-performance intelligent vehicles, deeply understanding and properly selecting YAGEO's complete product portfolio will undoubtedly provide solid foundational support and greater room for innovation in system design.

Article tags

Articles and Videos
Arrow Times
APAC
YAGEO

Related Content