Melexis MeLiBu® and The Engineering Behind Automotive LED Display Panels
For the past decade, automotive LED adoption has largely followed a substitution philosophy. Early designs were essentially technological updates to the halogen era; whereby highly concentrated clusters of high-power light sources were designed to project a beam from a fixed point. While efficient, these designs remained constrained by the legacy concept of a “headlight” or “taillight” – a static functional device rooted in the limitations of incandescent bulbs.
While dynamic indicators and some full-width units have pushed the boundaries of luminary design further, we are arguably now seeing the emergence of a new generation of LED-centric design. Automotive lighting is moving away from concentrated high-power points toward display panels – dynamic, pixelated surfaces that span the width of the vehicle. This shift transforms the vehicle’s exterior from a passive reflector into an active digital canvas. In this new paradigm, the “light” is no longer a beam; it is a programmable surface capable of displaying symbols, animations, and high-resolution patterns, both externally and also within the cabin.
Nevertheless, this evolution requires a fundamental architectural rethink, shifting the engineering focus from simply powering a load to managing a complex, high-speed display peripheral.
Demand for Communicative Surfaces
Why are OEMs and businesses driving this shift toward complex matrix panels? The motivation is rooted in functional necessity and brand differentiation within a rapidly changing mobility landscape.
As automotive designers prioritize aerodynamic efficiency to maximize electric vehicle (EV) range, traditional internal combustion engine (ICE) design cues such as air intakes, cooling grilles, and exhaust pipes are rendered obsolete. Consequently, creating a unique visual identity in increasingly competitive automotive markets has become a significant challenge.
The lighting signature has therefore emerged as the primary vector for brand differentiation. Dynamic and animated panels, including RGB internal deployments and distinctive full-width Matrixdisplay panels, can create distinct aesthetic appeal. They also allow OEMs to deploy over-the-air (OTA) updates that refresh the vehicle’s aesthetic identity post-sale, offering new animations or lighting-based functionality that extend the lifecycle and relevance of the platform.
Pedestrian Safety
Apart from aesthetics, there is also a functional drive aligned with emerging autonomous vehicles. In the absence of a human driver to signal intent, the vehicle itself must bridge the communication gap. For example, front-facing display bars capable of projecting “Safe to Cross” symbols or warning colors to vulnerable road users will probably become a critical safety requirement for Level 3 and beyond autonomy.
In this context, exterior lighting serves as the primary interface between the autonomous vehicle’s central intelligence and its immediate environment, while internal lighting can communicate autonomous operations back to passengers.
The “Robotaxi” Economy
There is also a commercial push for display panels from fleet operators as autonomous fleets expand, particularly in markets like China. In these applications, vehicles require a new modality for customer communication, as it is essential for the commercial viability of shared mobility.
Matrix panels integrated into doors or grilles can display status messages such as “Occupied,” “Free,” or “Reserved” – effectively replacing manual signals or eye contact. This capability enables commercial operators to enhance the end-user experience through clear, instant communication.
Realizing the Rear Matrix Display with MeLiBu® 2.0
To meet the demands of the next generation of automotive lighting, Melexis introduced MeLiBu®. The latest iteration, MeLiBu® 2.0, builds on the strengths of its predecessor while significantly expanding its capabilities. This allows for expansive and intricate lighting designs, ensuring that arrays, such as rear display panels, can cover entire vehicle surfaces without compromise.
However, deploying a high-resolution, full-width rear display panel presents a specific set of engineering hurdles. By utilizing MeLiBu® 2.0 and its compatible ICs, engineers can systematically address each of these zonal challenges.
Overcoming the Data Bottleneck
Operating a rear lighting array as a coherent matrix surface demands near video-grade data throughput. Attempting to drive fluid animations across a full-width light bar using standard CAN or LIN protocols is architecturally unviable; the bus throughput is simply insufficient to carry the frame data required for smooth, high-frame-rate animation, creating a hard limit on visual complexity.
MeLiBu® 2.0 utilizes a UART-over-CAN physical layer to deliver data speeds of up to 4 Mbit/s. This high bandwidth allows the central controller to “stream” complex lighting patterns to the edge nodes without latency or visual artifacts. Furthermore, the protocol supports 251 nodes on a single bus, allowing engineers to implement projects with over 4,000 RGB LEDs (or 24,000 single-color LEDs) on a single interface. Crucially, this bandwidth supports 16-bit PWM resolution (up to 1kHz), enabling deep dimming and precise gamma correction required for high-end visual performance.
Streamlining Zonal Integration
With the centralization of compute power inherent to zonal architectures, the physical separation between the central high-performance computer (HPC) and the lighting edge nodes introduces synchronization challenges. Furthermore, OEMs need to avoid burdening the architecture with complex local software management at every node.
MeLiBu® 2.0 is designed for seamless integration into software-defined vehicles (SDVs) with dedicated Code-Free driver variants allowing intelligence to be shifted to the system master. Equipped with validated firmware and 768 Bytes of user non-volatile memory (NVM) for configuration storage, Code-Free removes the need for custom firmware development at the edge. To further simplify physical integration, the drivers support auto-addressing via integrated shunt resistors, streamlining the assembly of complex daisy-chained modules.
Mastering Thermal and Physical Density
High-density matrices generate significant heat distributed across thousands of sources, which cannot be managed by traditional bulky heatsinks in ultra-thin designs. Furthermore, achieving pixel-to-pixel uniformity across such a large array is difficult when mixing LEDs from different production bins or suppliers.
Melexis drivers are engineered for high efficiency to prevent localized hotspots, and housed in compact QFN 5x5 packages to minimize footprint. To achieve maximum pixel density with minimal component count, the drivers feature stackable multiplexing—allowing, for example, just two stacked MLX80134 ICs to drive 384 LEDs, or three ICs to drive 864 LEDs. To ensure visual quality, MeLiBu® 2.0 offers flexible calibration options, allowing LED calibration data to be stored either locally within each driver IC or centrally at the ECU. This ensures perfect color uniformity regardless of the system architecture. With the stackable multiplexing feature, applications requiring a very high LED count, like rear combination lamps and illuminated grills, can be designed with very few LED driver ICs.
Ensuring Functional Safety
Rear lighting components are not merely aesthetic; brake lights and turn signals are safety critical and must adhere to rigorous industry standards to ensure operation under all conditions.
To support these critical applications, all MeLiBu® 2.0 drivers facilitate ASIL B Safety Element out of Context (SEooC) compliance. This includes configurable fail-safe scenarios stored directly on the IC, ensuring that warning signals and emergency lights remain operational even under challenging conditions or loss of communication, making the drivers suitable for applications where reliability is non-negotiable.
Conclusion: The Expanding Role of Communicative Light
The transition from static lamps to dynamic display panels represents a fundamental shift in automotive design. By solving the critical challenges of data bandwidth, thermal density, and integration complexity, the Melexis ecosystem enables OEMs to transform the vehicle exterior into a versatile communication surface.
To support the future of automotive lighting design, including display panels, Melexis is expanding the MeLiBu® ecosystem with a next-generation product family designed specifically for high-density display applications. This includes the MLX80132 and MLX81132 (24-channel, 2-fold multiplexing) for mid-range density, and the MLX80134 and MLX81134 (24-channel, 4-fold multiplexing) for high-density arrays.
Crucially, this family offers designers architectural flexibility through two distinct variants:
- Code-Free (MLX80132/MLX80134): For rapid deployment and simplified validation in standard zonal nodes.
- User Programmable (MLX81132/MLX81134): For specialized nodes requiring custom edge logic while maintaining MeLiBu® 2.0 connectivity.
By combining these advanced drivers with the high-speed data backbone of MeLiBu® 2.0, OEMs can deploy futuristic, software-defined lighting designs today, confident that the underlying hardware is robust, scalable, and fully aligned with the evolution of the autonomous vehicle.
Article tags