New from Bourns, high voltage LC kit for buck/boost and double pulse applications

0223-Wolfspeed-SpeedVal-Multi-Supplier-Article-Image-Bourns

Bourns Inc. has partnered with Wolfspeed to develop magnetic components optimized for the SpeedVal evaluation platform.

Included in the Buck/Boost Filter module section of the platform, Bourns introduces two custom designed inductors for use as the inductive element in the LC power filter stage as an add on accessory board.

0123-Wolfspeed-SpeedVal-Multi-Supplier-Figure1-Bourns

This LC filter enables the half-bridge portion of the main SpeedVAL half-bridge motherboard to be tested as either a buck or boost configuration mode.

To accomplish this, chokes were designed with two different inductance ranges per Wolfspeed’s project requirements.

Bourns offers the following two components integrated into the following Wolfspeed modules:

Bourns Part Number

Wolfspeed Module Number

BS501143T

MOD-ACC-BUCKBOOST-190uH

BS501144T

MOD-ACC-BUCKBOOST-400uH

The Bourns inductors were optimized for the total range of the 15kW current SpeedVAL kit parameters for both range of frequency (20-300kHz) but also a nominal peak operating current of 42A DC.

Features:

  • Litz wire for reduced skin effect and over all AC coil loss
  • Powder core material core loss over the total operating frequency of the SpeedVal kit
  • Toroidal core shape for best magnetic flux path
  • Powder core material for distributed gap advantages over discrete gap to reduce EMC
  • Considerations of core and wire density for lowest total weight of the component

Bourns has also developed with Wolfspeed an inductor, BS501145T, for use in dynamic double pulse testing of the SpeedVAL kit. In order to provide the inductive load necessary for turn on/turn off energy and reverse recovery characteristics for switching measurements, not only does the choke need to provide an inductive reactance but also be “invisible” enough for the fast turn on and turn off rates of the FET.

To accomplish this for a minimum to no necessary compensation for the inductor, the choke needed to provide:

  • Best possible magnetic flux path and lowest core loss for best switching energy measurement of the DUT (Device Under Test)
  • Very high operating frequency (GHz)
  • Lowest parasitic and shunt capacitance to limit extra FET ringing
  • Nominal temperature rise in the inductor windings for maximum current needs of SpeedVAL
  • Different inductance value combinations necessary to complete double pulse testing requirements

BS501145T dynamic double pulse testing

An air core inductor was developed and produced to fulfill these requirements.

Bourns BS501145T features:

  • 3 sets of stacked windings to produce 6 different inductance values
  • Spaced windings for minimal shunt and distributed capacitance
  • Screw connectors for spade, banana, and bifurcated terminals

Bourns BS501145T inductor


See related product

BS501143T-04

Bourns Inductor Leaded View

See related product

BS501144T-04

Bourns Inductor Leaded View

See related product

BS501145T-04

Bourns Inductor Leaded View


Wolfspeed SpeedVal Kit Banner


Related news articles

Latest News

Sorry, your filter selection returned no results.

We've updated our privacy policy. Please take a moment to review these changes. By clicking I Agree to Arrow Electronics Terms Of Use  and have read and understand the Privacy Policy and Cookie Policy.

Our website places cookies on your device to improve your experience and to improve our site. Read more about the cookies we use and how to disable them here. Cookies and tracking technologies may be used for marketing purposes.
By clicking “Accept”, you are consenting to placement of cookies on your device and to our use of tracking technologies. Click “Read More” below for more information and instructions on how to disable cookies and tracking technologies. While acceptance of cookies and tracking technologies is voluntary, disabling them may result in the website not working properly, and certain advertisements may be less relevant to you.
We respect your privacy. Read our privacy policy here