Micron Technology is at the Forefront of the DDR5 Revolution

With the continued industry migration to things like E-commerce, remote work, and cloud computing, the demands on data centers continue to grow exponentially.

DDR4-standard DRAM has seen widespread adoption since it was adopted in 2014. However, increased customer demands for reliability, availability, and serviceability over the past few years have made it apparent that a new generation of DRAM is needed. Recently, Micron Technology, Inc announced a comprehensive Technology Enablement Program (TEP) to aid in the design, development, and qualification of next-generation computing platforms utilizing DDR5 DRAM, the most advanced currently available. 

In January 2020, Micron announced its roll-out of DDR5 RDIMM samples. In July 2020, JEDEC (the global standards organization for the electronics industry) published its widely-anticipated JESD79-5 DDR5 SDRAM standard. Because of their experience with the technicalities of the new DRAM and their engagement with the new standards, companies like Micron, Cadence, Montage, Rambus, Renesas and Synopsys exist at the nexus of market demands and technical development. With the TEP, this group of businesses will work hand-in-hand with channel partners like distributors, value-added resellers, and OEMs as they develop new products using this new tech. 

DDR5 is the most technologically advanced DRAM to date. Built off of Micron’s industry-leading 1znm process technology, DDR5 delivers an over 85% increase in memory performance. The key to this advancement is memory density - DDR5 has double that of its predecessor DDR4. In this infographic, see how DRAM has experienced exponential increases in speed over time, and how DDR5 is the best yet. 

0820 micron_ddr5_infographic

This evolution in speed allows for the increased memory bandwidth and capacity needed to power cutting-edge data centers with rapidly expanding processor core counts. The below table gives an overview of the advantages of DDR5:

Feature/Opinion    DDR4    DDR5    DDR5 Advantage 
Data Rates    1600-3200 MT/s    3200-6400 MT/s    Increases performance and bandwidth 
VDD/VDDQ/VPP   1.2/1.2/2.5    1.1/1.1/1.8    Lowers power 
Internal VREF    VREFDQ   VREFDQ, VREFCA, VREFCS   Improves voltage margins, reduces BOM costs 
Device densities    2Gb-16Gb    8Gb-64Gb    Enables larger monolithic devices 
Prefetch    8n    16n    Keeps the internal core clock low 
DQ receiver equalization     CTLE    DFE    Improves opening of the received DQ data eyes inside the DRAM
Duty cycle adjustment (DCA)     None    DQS and DQ    Improves signaling on the transmitted DQ/DQS pins 
Internal DQS delay
 monitoring 
   None    DQS interval oscillator    Increases robustness against environmental changes 
On-die ECC     None    128b+8b SEC, error check and scrub    Strengthens on-chip RAS 
CRC     Write    Read/Write    Strengthens system RAS by protecting read data 
Bank groups (BG)/banks     4 BG x 4 banks (x4/x8)
 2 BG x 4 banks (x16) 
  8 BG x 2 banks (8Gb x4/x8)
 4 BG x 2 banks (8Gb x16)
 8 BG x 4 banks (16-64Gb x4/x8)
 4 BG x 4 banks (16-64Gb x16) 
  Improves bandwidth/performance 
Command/address interface    ODT, CKE, ACT, RAS,
 CAS, WE, A<X:0> 
  CA<13:0>    Dramatically reduces the CA pin count 
ODT    DQ, DQS, DM/DBI    DQ, DQS, DM, CA bus    Improves signal integrity, reduces  BOM costs 
Burst length    BL8 (and BL4)    BL16, BL32
 (and BC8 OTF, BL32 OTF) 
  Allows 64B cache line fetch with only 1 DIMM subchannel. 
MIR (“mirror” pin)    None    Yes    Improves DIMM signaling 
Bus inversion    Data bus inversion (DBI)    Command/address inversion (CAI)    Reduces VDDQ noise on modules 
CA training, CS training    None    CA training, CS training    Improves timing margin on CA and CS pins 
Write leveling training modes    Yes    Improved    Compensates for unmatched DQ-DQS path 
Read training patterns    Possible with the MPR    Dedicated MRs for serial
 (userdefined), clock and LFSR
 -generated training patterns
  Makes read timing margin more robust  
Mode registers    7 x 17 bits    Up to 256 x 8 bits
 (LPDDR type read/write)  
  Provides room to expand 
PRECHARGE commands    All bank and per bank    All bank, per bank, and same bank    PREsb enables precharging-specific bank in each BG 
REFRESH commands    All bank    All bank and same bank    REFsb enables refreshing of specific bank in each BG 
Loopback mode    None     Yes    Enables testing of the DQ and DQS signaling  

Micron DDR5 Technical Engagement Program (TEP) Benefits:

Approved partners can get access to:

- Technical resources such as data sheets, electrical, thermal and simulation models to aid in product development and platform bring-up.
- Select DDR5 component and module samples as they become available.
- Connection with other ecosystem partners that can aid in the design and bring up of DDR5 enabled platforms.
- Technical support and training materials.

Apply Now

Get the White Paper

Download Press Release

 

Related news articles

Latest News

Sorry, your filter selection returned no results.

We've updated our privacy policy. Please take a moment to review these changes. By clicking I Agree to Arrow Electronics Terms Of Use  and have read and understand the Privacy Policy and Cookie Policy.

Our website places cookies on your device to improve your experience and to improve our site. Read more about the cookies we use and how to disable them here. Cookies and tracking technologies may be used for marketing purposes.
By clicking “Accept”, you are consenting to placement of cookies on your device and to our use of tracking technologies. Click “Read More” below for more information and instructions on how to disable cookies and tracking technologies. While acceptance of cookies and tracking technologies is voluntary, disabling them may result in the website not working properly, and certain advertisements may be less relevant to you.
We respect your privacy. Read our privacy policy here