Arrow Electronics Components Online

完整电源解决方案赋能AI服务器算力跃升

Arrow Times20 7月 2026
Illustration of an Advanced Driver Assistance System (ADAS) around a top-view car.
View all articles

随着生成式AI与大模型的爆发式增长,AI服务器的算力需求正呈指数级攀升。作为算力的物理承载,AI服务器不仅需要更强大的GPU/CPU,更迫切需要一套稳定、优效且高密度的供电系统来支撑其运转。然而,动辄数十千瓦的机柜功耗、急剧缩短的产品迭代周期,以及日益严格的能效法规,正让传统电源架构捉襟见肘。本文将为您剖析AI服务器在电源架构上的需求,以及由Murata(村田制作所)所推出的电源方案核心产品与应用特色,揭示其如何赋能AI服务器实现算力跃升。

为AI服务器打造高密度电源基座

针对AI服务器高算力、高功耗的需求,Murata推出了符合OCP标准的集中式电源管理解决方案,其核心产品如MWOCES-191/211系列(像是MWOCES-191-P-D和MWOCES-211-P-D)电源机柜(Power Shelf),旨在解决AI数据中心面临的大电流供应挑战和机柜功率密度飙升问题。
 
由于AI服务器功耗很大,研究显示机柜平均功率密度预计在2027年将突破30kW,为应对高功率密度,Murata推出的电源机柜,将是应对这一趋势的关键基础设施。此外,Murata的电源机柜支持主流AI架构,方案可灵活支持OCP、NVIDIA MGX等主流AI服务器架构,能适配19英寸和21英寸机架,并已成功应用于实际部署,并提供完整电源链条,Murata提供从机柜级(Power Shelf)到板端(DC-DC转换器)的完整电源方案,周全支持高负载计算。
 
以MWOCES-191-P-D(19英寸)和MWOCES-211-P-D(21英寸)为例,两款产品核心参数基本相同,其主要特色包括具有很高功率密度,可在紧凑的1U(约4.45cm)高度内,可提供高至33kW的总输出功率,并具有灵活冗余架构,最多容纳6个热插拔电源模块(PSU)和1个远程管理单元(RMU),可支持N+1或N+N冗余,保障系统高可靠性。
 
此外,这两款产品还支持智能远程管理,搭配MWOC-RMU-3模块,便可实现远程ON/OFF控制、状态监测和故障信息上报,并拥有宽广的输入兼容性,支持三相Δ型、三相Y型、单相AC及HVDC(192-400 Vdc)等多种输入,适应不同数据中心电力环境。
 
另一方面,MWOCES-191-P-D和MWOCES-211-P-D均拥有很高的能源效率,配套的电源模块(如MWOCP67-5500-B-RM)峰值效率大于97.5%,符合80Plus Titanium(钛金)甚至更高级别的80Plus Ruby(红宝石)能效标准,且具有高规格安全与可靠性,产品符合UL、CSA、TUV、CQC、CB等多项国际安全认证,并具备2年保修。
 
Murata的OCP电源解决方案,凭借其高功率密度、灵活的模块化设计、智能管理能力和优等能效,准确地满足了AI服务器对电源系统的严格要求,是构建和扩展AI数据中心基础设施的理想选择。

A slim rackmount server chassis is shown from a front angle, highlighting its metal construction. The front panel features multiple perforated fan modules arranged in a row for efficient airflow. Blue latches and visible ports on the left side suggest hot-swappable components and network connectivity. The clean, minimal background emphasizes the hardware design and industrial aesthetic.

MWOCES-191-P-D支持OCP系统电源机柜

提供关键底层供能支持的前端电源模块

针对AI服务器对功率和效率的严格需求,Murata还推出D1UXXX系列(例如D1U74T-W-3200)等前端电源模块,提供了关键的底层供能支持。以D1U74T-W-3200-54-HB3C为例,这款模块的输出功率达3200W,输出电压为54 Vdc主输出 + 12 Vdc辅助输出,能效等级达到80 Plus Titanium(钛金级),在50%负载下效率高至96%以上,可显着降低数据中心的能源损耗和散热成本,并具有支持热插拔、主动均流、PMBus™数字管理接口等关键特性,采用紧凑的1U设计,在极小的1U空间内实现了3200W的高功率输出,有效节省了机架空间。
 
这款3200W的高功率模块是构建高密度计算集群的理想选择,可适配主流AI服务器架构,该模块符合Intel CRPS标准,可灵活适配OCP、NVIDIA MGX等主流AI服务器架构,并支持GPU加速计算,专为满足AI训练和推理中GPU服务器的高负载需求而设计。
 
D1U74T-W-3200-54-HB3C具有高可用性与灵活性,支持N+1冗余和热插拔功能,并支持多个模块并联运行,便于在线维护和功率扩展,并配备PMBus™/I2C数字接口,可实现对电源的实时控制、编程和远程监控等智能管理功能。此外,该产品还具有宽输入电压范围,支持全球通用的宽交流输入电压,适应不同地区的电网环境。
 
Murata的D1U74T-W-3200-54-HB3C前端电源模块,凭借其3200W的高功率、钛金级的能效、智能化的管理能力和高可靠性设计,准确地满足了AI服务器对电源的严格要求。它是应对AI算力带来的高功耗挑战,构建稳定、优效、可扩展的AI数据中心的关键组件。

Rectangular metal power supply module shown in closeup on a white background. The unit features a black cooling fan at the rear with a clear plastic handle for insertion and removal. A teal pull tab and standard power connector are visible, emphasizing its hot-swappable server or network equipment design. The overall appearance is industrial and functional, with a neutral metallic color palette.

D1U74T-W-3200-54-HB3C前端电源模块

中间总线转换器是连接前端电源和后端负载的关键一环

在典型的AI服务器电源架构中,中间总线转换器(IBC)是连接前端电源和后端负载的关键一环。在AI服务器电源架构中,AC-DC电源架(Power Shelf)中的电源模块(PSU)负责将交流电转换为48V或54V的直流电,DC-DC则由IBC接手工作,将48V/54V的电压有效地转换为12V的中间总线电压,接着板上的电压调节模块(VRM)再将12V电压转换为CPU、GPU等核心芯片所需的低微电压(如1V以下)。
 
针对AI服务器高算力带来的电力需求,Murata推出了MPQXXX系列(例如MPQ800-12V67-L48NBMC)等IBC产品,它们在板级电源转换架构中扮演着关键角色。以MPQ800-12V67-L48NBMC为例,它支持800W输出功率,输入电压为40V - 60Vdc,输出电压为12Vdc,输出电流最大125A,效率高至97%,外形尺寸仅有1/4砖(58.42 x 36.83 x 15.0 mm),可在-40℃至+125℃温度范围工作,并通过UL62368-1安全认证。
 
MPQ800-12V67-L48NBMC拥有97%的较高转换效率,能有效降低能量损耗和发热,对高密度AI服务器至关重要,并具有高功率密度,在紧凑的1/4砖封装内实现800W输出,可节省宝贵的PCB空间,且支持数字控制与智能管理,并可选配PMBus™接口实现实时监控、故障管理和输出电压微调,支持完整的保护机制,集成过流、过温、过压保护,确保系统在异常情况下的安全,并具备高可靠性,2250V的隔离电压提供了出众的系统安全性和抗干扰能力。
 
Murata的MPQ800 IBC模块凭借97%的较高效率、800W的高功率密度、智能化的数字控制和完整的保护功能,准确满足了AI服务器对板级电源转换的严格要求。

An isolated DC DC power converter module is shown in close-up against a plain white background. The green printed circuit board features multiple electronic components, including capacitors, resistors, and integrated circuits. A large black central block covers part of the board, while metal pins and connectors are visible on one side for electrical interfacing. A white identification label with technical markings and barcodes is attached to the top surface.

MPQ800-12V67-L48NBMC数字控制隔离式中间总线变换器

扮演关键“48V至12V”电压转换环节角色的充电泵

在AI服务器的板级电源转换架构中,充电泵(Charge Pump)产品在关键的“48V至12V”电压转换环节扮演着至关重要的角色。它们与传统的中间总线转换器(IBC)功能相似,但凭借其特别的“无损”技术,在特定场景下能实现更高的效率和功率密度。
 
Murata的充电泵产品主要分为两类:一类是独立的充电泵模块,如MYCXXXX系列(像是MYC0409-NA);另一类是集成了充电泵技术的POL(负载点)稳压器模块,如MYTXX系列(像是MYTNA1R84RELA2RA)。它们在AI服务器中分工合作,共同构成了从48V母线到核心芯片的完整优效供电链路。
 
MYC0409-NA是Murata UltraCP™系列的一款效率较高的48V至12V独立充电泵模块,采用专有的无损充电泵技术,专门用于将48V总线电压有效地转换为12V中间总线电压,其输入电压为20V - 60V(支持48V总线架构),输出电压为Vin/4(例如48V输入时输出12V),输出电流最大6A,输出功率最高72W,峰值效率高至96.5%,外形尺寸为11.5 x 9.5 x 2.0 mm,可在-40℃至+105℃温度范围工作。
 
MYC0409-NA具有特高效率与低发热,其无损充电泵技术可将转换器损耗降低约一半,从而使产品温度降低50℃或更多,通过高度集成,其封装尺寸远小于传统的砖块式IBC模块,有助于在紧凑的AI服务器板卡上实现分布式供电架构,并支持并联运行,通过简单地增加模块数量,即可灵活构建从低功率到高电流的系统。此外,MYC0409-NA还拥有完善的保护功能,集成使能控制、Power Good指示、频率同步、过流保护、过温保护、欠压锁定等功能。
 
在AI服务器中,MYC0409-NA可在AI加速卡或主板中,直接替代体积较大的传统IBC模块,将48V电压转换为12V,为后级的GPU、CPU、内存等负载供电,并可将多个MYC0409模块分散布置在靠近负载(如GPU)的位置,形成分布式供电架构,这能将布线损耗降低约60%,从而提高整体系统效率,且可通过并联多个MYC0409模块,构建一个大电流、优效的12V供电阵列,满足AI服务器中高功耗加速卡的需求。
 
另一方面,MYTNA1R84RELA2RA则是一款集成充电泵的POL稳压器,是Murata UltraBK™系列的一款两级DC-DC转换器,它巧妙地将充电泵技术与后续的降压稳压器结合,直接从12V母线为AI核心芯片提供超低压大电流供电。MYTNA1R84RELA2RA的输入电压为6V - 14.4V(适用于12V母线),输出电压为0.7V - 1.8V(可调),最大输出电流为4A,输出功率为7.2W,可在-40℃至+105℃温度范围工作。
 
MYTNA1R84RELA2RA还内建很高集成度的“Ultra Block”,在一个很薄的封装内集成了包括电感在内的所有无源器件,并采用两级优效架构,内部采用双相充电泵作为第一级,再配合第二级稳压器,实现了非常高的转换效率,其纤薄设计,典型高度仅为2.1mm,非常适合放置在AI加速卡背面等对高度有严格限制的区域,并具有完备的保护机制,集成输出过流保护、短路保护和过温保护,确保在负载故障等异常情况下的系统安全。
 
MYTNA1R84RELA2RA在AI服务器中可为核心芯片供电,作为最后一公里的POL稳压器,直接放置在GPU、CPU、AI ASIC等核心芯片附近,将其所需的12V电压有效转换为1V以下的特低压核心电压,并可解决高密度布局难题,凭借其微小尺寸和纤薄高度,可以便利地集成在AI加速卡日益紧凑的布局中,为高密度计算提供支持。

结语

在AI算力竞赛进入白热化的今天,供电能力已成为制约系统性能释放的关键瓶颈之一。Murata所提供的并非单一器件,而是一套经过验证、协同优化且覆盖全链路的完整电源解决方案。从机柜级的MWOCES电源机架,到板载的MPQ800 IBC模块,再到紧贴芯片的MYC系列充电泵与POL转换器,Murata通过其出众的工程能力,将优效、高功率密度和高可靠性融为一体,这不仅帮助数据中心运营者显着降低了电力损耗和散热成本,更在有限的物理空间内释放了AI服务器的最大计算潜能。对于寻求构建稳定、优效且可扩展AI基础设施的开发者与企业而言,Murata的完整电源方案无疑是一个值得深入评估与信赖的选择。

文章标签

文章和视频
Arrow Times
亚太地区
Murata Power Solutions

Related Content