文章
查看我们全新且快速增长的应用专用简报库、实用文章、精选制造商、网络研讨会内容、框图等更多内容。
体验 InfineonSpice,这款免费的模拟电路仿真器融合了速度、可靠性和高级功能,可轻松增强您的设计流程。
探索由 AI 驱动的 PPE 合规监控系统的开发。通过对防护装备的实时检测,确保工业环境中的安全。
学习使用 Qualcomm 的 IM SDK 构建适用于受限区域的高效 AI 监控系统。通过实时检测和可视化警报确保安全。
了解 Molex 技术如何为 LEO 卫星星座提供强健的互连解决方案,确保在极端太空条件下的可靠性。
蓬勃发展的电动汽车(EV)市场带动了包括电动汽车充电器在内的各行各业的发展,为了满足日益增长的电动汽车需求并实现低碳目标,必须通过高效的电动汽车充电系统设计来建立更完善的充电基础设施,
As electric vehicles (EVs) gain more and more market share and will eventually replace internal combustion engine vehicles, DC fast charging stations will replace or integrate with petrol stations, powered by renewable energies such as solar and wind.
随着电动汽车(EV)市场的迅猛发展,快速充电技术已成为缓解“里程焦虑”、推动电动汽车普及的核心驱动力。然而,快速充电系统的普及也带来了严峻的技术挑战:更高的功率等级(22kW至350kW+)、更高的电压平台(800V及以上)、严苛的户外工作环境,以及日益严格的电磁兼容(EMC)与安全标准。本文将为您介绍电动汽车快速充电应用中所面临的挑战,
当电动车的充电功率从50kW向350kW甚至更高迈进时,充电时间正从“小时”级向“分钟”级缩短。然而,在这场与时间赛跑的过程中,一个非常关键却常被忽略的幕后功臣,正是默默提供“心跳”的时序器件(Timing Devices)。
了解 Arrow 的 2026 年第三季度 IP&E 新闻,包含有关电源、管理、电路保护、磁性元件和热解决方案的专家见解。
探索一份适用于 AI 支持的心电图电路设计的综合在线框图,并了解如何将其集成到您的下一款医疗设备中。
In 800VDC data center architectures, Power to GPU solutions play a critical "last-mile" role. They are responsible for precisely and efficiently stepping down the intermediate voltage (such as 48V or 12V) from the high-voltage DC-to-low-voltage DC conversion stage to the ultra-low voltage (typically below 1V) required by the GPU core, while delivering currents up to thousands of amperes to the chip.
In 800VDC data center architectures, high-voltage DC to low-voltage DC (HVDC to LVDC) conversion plays the critical role of a "voltage adaptation hub." It is responsible for efficiently converting the high voltage from the 800V DC busway distribution system into the low voltages (such as 48V, 12V, or even below 1V) required by compute chips like GPUs and CPUs.