Weigh-in-Motion Tech Makes Trains Safer and More Cost-Effective

Heavily loaded freight trains can operate more safley and cost efficiently thanks to innovations in sensor technology.
게시자

Moving thousands of tons of freight on trains more than 2,000 meters long is a tricky business. Derailments can be caused by unbalanced weight distribution between the front and rear of the train. If heavier cars are positioned at the rear and braking is too sudden or forceful, compression forces can derail the lighter cars in front. For almost as long as there have been freight trains, the problem of weight distribution has received a lot of attention.

To further complicate the challenge, freight trains are constantly being reconfigured at depots along the route. Cars are removed and replaced by other cars of different weights. In short—over the long haul—it’s a major challenge to know how the train is loaded. The traditional solution has been to weigh each car individually on a static scale, which is time consuming, inefficient and costly.

Sensors the size of a postage stamp are now being used to solve the load distribution problem more efficiently. Piezoelectric strain gauge sensors welded to the side of a rail are a critical component of weigh-in-motion (WIM) technology. The strain gauges sense minute changes in the rail’s electrical properties when a train car’s wheel passes over it, and the railcar’s weight can be accurately derived from this data. 

The aggregated information for the entire train gives the railroad operator two corrective options: 
1) Adjust the brake settings to accommodate and control how much pressure is applied; and/or, 
2) Reconfigure a precariously loaded train. 

It all sounds simple enough but engineering the solution involves a number of technologies including: 

• Sensors that may be based on several technologies. Piezoelectric sensors using quartz crystals are common and produce an electric charge proportional to the force. Since the signal has very high impedance, it is not sensitive to electrical interference.
• A MOSFET-based charge amplifier is used to convert the signal to a voltage output.
• Inductive loops to identify and timestamp the rail car’s entry and exit from the WIM station.
• The WIM software, which has to take into account the railcar’s weight, speed and other variables. It is not uncommon to include a GPS-synchronized time stamp as a means of tracking the data.
• Wireless communications, which is often Wi-Fi although cellular technology or modems can also be used. 

Sensors that use quartz have a sensitivity of about 4.3 pC/N (i.e., the force of one Newton applied to the sensor produces a charge of 4.3 Picocoulombs). Quartz is being replaced with gallium phosphate (GaPO4) as the piezoelectric crystal in many applications such as WIM. GaPO4 can achieve twice the sensitivity because twice as much charge is produced by the same force. 

The sensitivity of the sensor remains the same regardless of the nominal (rated) force and very large sensors can also be used to measure a very small force. Another advantage is that charges can be physically set to zero. A short circuit can be used to produce a charge of zero pC on the input when the sensor is loaded by a force such as a pre-stress. 


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.