Top motor control driver considerations for DC motors

Given the rapidly growing interest in electrification across numerous major applications, DC electric motors are becoming increasingly commonplace. In this article, get an overview of the three main DC motor types as well as appropriate motor control drivers (MCDs) for each.

Brushed DC Motors
For simpler applications, brushed DC motors are a great choice. Power is provided simply by applying DC voltage to the terminals of the motor. Speed control is achieved through the precision control of the applied voltage, and most brushed DC motors can operate with pulse-width-modulated (PWM) signals.

Brushless Motors
Brushless DC (BLDC) motors are typically used in more high-performance applications. Due to their construction, they also are more efficient than brushed motors and release less EMI as well. These benefits require more sophisticated controls, however, with ICs or motor-controller microcomputers being required.

DC Stepper/Stepping Motors
Stepper motors are so-called because they rotate in discrete “steps”. Depending on the application requirements, the motor can be programmed to rotate through varying numbers of radial locations. The most common is about 200 steps per revolution, meaning that, out of 360 total degrees, the motor will move through 1.8 degrees then stop for a desired amount of time before continuing to the next step.

Motor Control Driver Types
Brushed motors can be used in close quarters with other brushed motors, necessitating a need for a controller with numerous channels to handle different motors. The Toshiba TB67H452FTG is a great example of a controller that can handle many brushed motors at once.

The control of brushless motors is a bit more complex, usually requiring varying combinations of sensors and MCDs. Intelligent phase control and closed-loop speed control are two important features of MCDs for brushless motors.

Stepper motor controllers need to have an appropriate level of support for the amount of step resolution required by the application. It’s not uncommon to find stepper MCDs that support 1/64 or even 1/128 resolutions. A downfall to increasing the number of steps is a corresponding decrease in torque. This, however, can be remedied through the use of an MCD with active gain control measures, such as the Toshiba TB67S249FTG.

The right DC electric motor coupled with the right MCD can be a powerful combination. Toshiba offers numerous options for motor control, from simple to cutting-edge. Click through to the article to learn more about motor technology and available controller choices.


READ MORE


관련 상품 참조

TB67H452FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TB67S249FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78H653FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78H660FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78B009FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78B016FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78B027FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78B042FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78B025FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TC78H670FTG,EL

Toshiba Motor Controller and Driver ICs 보기

관련 상품 참조

TB67S128FTG, EL | Stepper Motor Controller

Toshiba Motor Controller and Driver ICs 보기


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.