The complete guide to banana plugs

Banana plugs are single-wire electrical connectors used for joining wires to equipment with a cylindrical pin/plug that has sprung metal “leaves” that bulge outward, though variations on this exist for different applications. The springs produce a snug fit and good connectivity in a socket as well as preventing the pin from falling out.

Banana plugs are used at the ends of patch cords for electronic test equipment, speaker wires, and probe leads. The wire can exit the rear at a right angle (90 degrees), a 45-degree angle, or straight back. The diameter of the pin is usually 4 mm (which is why it’s also often referred to as a 4 mm plug). The back of the pin is connected to a wire which is screwed, soldered, or crimped into place. Often there is insulating plastic over part of the connector.

Read this article to learn more about the different styles, features, and options of banana plugs from Mueller Electric.


Banana Connector Guide

This guide to bananas covers different types of banana plugs, connectors and jacks.


Body Image 1-Mueller-Electronic-Banana-Plugs

Banana Plugs

Banana plugs are a single-wire electrical connector used for joining wires to equipment.

In Europe, Banana plugs are sometimes called 4 mm connectors, but not all bananas will connect with 4 mm parts.

A banana plug is a cylindrical pin/plug that has sprung metal “leaves” that bulge outward, though variations on this exist for different applications. The springs produce a snug fit and good connectivity in a socket as well as preventing the pin from falling out. The diameter of the pin is usually 4 mm (which is why it’s also referred to as a 4 mm plug).

The back of the pin is connected to a wire which is screwed, soldered, or crimped into place. Often there is insulating plastic over part of the connector. These are used at the ends of patch cords for electronic test equipment, speaker wires, and probe leads. The wire can exit the rear at a right angle (90 degrees), a 45 degree angle, or straight back.

Body Image 2-Mueller-Electronic-Banana-Plugs

Leaves

Body Image 3-Mueller-Electronic-Banana-Plugs

Banana plugs are called bananas because of the metal leaves which bulge out. Each leaf is curved like a banana. These are most commonly either 4 leaves or 9 leaves. The 9 leaf bananas have a stronger “grip” on the socket and are preferable for heavier wires or in high voltage uses where safety is a concern.


Stackable or Stacking Plugs

A stackable plug has a 4 mm hole in the back, either on the side, the back, or both, to accept the pin of another 4 mm plug.


Body Image 4-Mueller-Electronic-Banana-Plugs

Shrouded Bananas

Shrouded (also called sheathed) plugs have insulation around both the male and female connectors to avoid accidental contact in high voltage situations.

The shrouded plug will fit into shrouded and unshrouded jacks but not binding posts.


Body Image 5-Mueller-Electronic-Banana-Plugs

Retractable Banana

A retractable Banana has a spring-loaded shroud cover that slides out of the way when the pin is inserted into a shrouded or unshrouded jack.


Body Image 6-Mueller-Electronic-Banana-Plugs

There can be combinations of the above, for example, a stackable retractable banana.


Binding Posts


Body Image 7-Mueller-Electronic-Banana-Plugs

The binding post is called a "5-way" or "universal" post because there are 5 ways to attach a wire to it. They are a type of wire terminal found on speakers, receivers, and amplifiers as well as test and measurement instruments, high-voltage test equipment and various handheld devices.

Binding posts accept bare wire and four different types of connectors: pin connectors, spade connectors, banana plugs, and dual banana plugs. Banana plugs are inserted into a hole in the back of the binding post.


Banana Jacks

A Banana Jack is another word for the female connector that the banana plug is inserted into.

Jacks have different kinds of pins on the front end which allow them to connect or plug into many different electrical items.

A Binding post is one type of jack.


Body Image 8-Mueller-Electronic-Banana-Plugs

Dual Plugs and Posts


Body Image 9-Mueller-Electronic-Banana-Plugs

Dual plugs are simply two plugs together. They are designed for use with amplifiers or speakers that use traditional binding posts.

Dual plugs and posts make it safer to plug in two wires with no chance of stray wire strands creating a short across contacts.


Body Image 10-Mueller-Electronic-Banana-Plugs

Dual Binding posts are two posts together - often what a dual plug will plug into.


Mini Bananas


Body Image 11-Mueller-Electronic-Banana-Plugs

These are 2mm or 3mm banana plugs. Pictured above is a mini banana plug compared to a regular banana plug.


Color Coding

Banana plugs and jacks are commonly color coded. Red and black are the most common. If a Mueller part is available in a color, then the end of the part number will have a dash and a single digit. That digit corresponds to the color of the part. For example, a BU-00243-2 banana plug means the plug is red because the last number is a 2 after the dash.

This naming system is followed by many other banana plug manufacturers, as well.


Body Image 12-Mueller-Electronic-Banana-Plugs


관련 상품 참조

BU-P1825-1

Mueller Electric 보기

관련 상품 참조

BU-P1825-2

Mueller Electric 보기

관련 상품 참조

BU-P1825-3

Mueller Electric 보기

관련 상품 참조

BU-P1825-4

Mueller Electric 보기

관련 상품 참조

BU-P1825-5

Mueller Electric 보기

관련 상품 참조

BU-P1825-6

Mueller Electric 보기

관련 상품 참조

BU-P1825-7

Mueller Electric 보기

관련 상품 참조

BU-P1825-8

Mueller Electric 보기

관련 상품 참조

BU-P1825-9

Mueller Electric 보기


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.