Digital Sensors, the Path Forward

For years, the sensor products industry has been primarily analog focused. Sensors operated using analog circuits and components, due in part to the analog front ends found in almost all electronic measurement devices. Analog sensors have been fairly straightforward devices, sometimes providing basic analog outputs, and in some cases adding amplification or gain, and signal conditioning before the output is sent to a measurement or control system. Today, these systems are becoming more sophisticated, and as a result, demand additional signal processing to achieve the desired system performance.

In the past, sensor system engineers were reluctant to move to digital products due to the challenges presented by adding digitization to existing analog sensor signal paths. The R&D costs of making these changes were out of reach for many small sensor companies that focused on single product types, applications, and markets. Over the past couple decades, a few digital sensors have entered the market, but the lack of any standard interface or communication protocols made the effort expensive and risky. Needless to say, digital adoption was slow.

Due to the increased availability of low cost electronic components that can process and convert analog signals to digital formats, the migration of analog sensors into the digital world is now underway in earnest. Over the past few years, sensor manufacturers have been starting to integrate sensor elements, A/D conversion, processing capability, memory, power management, and digital communications capability into just a few chips that easily fit into the sensor package. In addition, the proliferation of standard communication protocols like I2C and SPI have made it easy to integrate sensors fitted with these capabilities into electronic monitoring and control systems.

The digitization of sensor products has benefits far beyond the ability to easily communicate with digital control systems. As an example, most digital sensors include a “sleep mode” feature that turns the sensor off when it’s not needed for system functions. By reducing the power required, the battery life improves for remote and mobile systems that rely on energy harvesting or battery power. Digital sensors can also take advantage of software optimization routines that are not available in the analog mode. Techniques like oversampling and digital filtering can dramatically improve sensor resolution and frequency discrimination. Best of all, these performance improvements come with no cost increase. It’s all in the software. 

There are a number of more subtle benefits that come with digital sensor products.  Because a digital sensor has on-board memory, information can be stored.  Nonvolatile information such as the device part number, revision level, serial number, and calibration factors can be included and easily accessed.  Dynamic information such as number of interrogations, error logs, and hours of operation can be programmed in the senor software.  This data can support a robust reliability and quality assurance program for the systems utilizing these sensors.

Digital sensor technology has enabled sensor manufacturers to create products that meet the unique needs of a customer’s system.  Many digital sensor products today contain more than one sensing element.  For example, a digital humidity sensor can also contain a temperature sensor, and by accessing the data from both and doing a little bit of math in the system host processor, the dew point can be generated.  Three pieces of information are created (relative humidity, temperature, dew point) using the data from only two sensing elements, both in the same low cost sensor package.

Today’s complex systems are driven by the demand for “smart” capabilities.  This has increased the need for additional digital sensors in system designs.  Systems and products require more information to increase their capabilities.  Products are required to be aware of their surrounding environment, its own health and uptime, received human inputs as well as other system interaction, all of which require the use of additional sensors.  These sensors send that critical data to the microcontrollers through seamless interfaces, enabling them to make decisions based on the data received from the sensors.  The more data provided, the more intelligent the decisions. Smarter systems require more sensors.

Digital sensors are now able to provide low cost solutions with increased performance and capability.  The migration to digital sensors has enabled smarter systems by providing better performance, all while being built and integrated at very attractive price points and meeting customer design requirements. 

관련 상품 참조

HPP845E031R5

TE Connectivity Temperature and Humidity Sensors 보기



관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.