TDK Launches New Thyristor Module for Power Factor Correction

게시자

TDK Corp. and its EPCOS division have introduced to the market a fast, electronically controlled, self-monitoring thyristor switch for capacitive loads. The company’s new TSM-LC-N690 is capable of connecting power capacitors within a few milliseconds, and as often and long as requested to the grid without any wear off.

The module performs two-phase switching of the capacitors, so that a neutral conductor is not needed.

The new TDK/EPCOS thyristor module features an expanded operating voltage range up to 690 VAC. Depending on the operating voltage, the new module can switch currents of up to 60 A, and is designed for a reactive power of 40 kvar (kilovolt ampere reactive) to 75 kvar.

Reactive power occurs when the current and voltage is out of phase, caused by loads imposed, for example, by electric motors and transformers. Reactive power can be almost completely compensated for by switching power factor correction capacitors. PFC reduces energy costs and relieves the load on the environment.

The new TDK/EPCOS module helps to increase the operating life of capacitors by switching at the zero crossing of the current—the instantaneous point at which there is no voltage present. Dangerous over-currents are avoided and the grid is not exposed to transients, those momentary surges of energy that are induced upon power, data, or communication lines.

The module continuously monitors voltage, phase and its own temperature, and is thus very reliable. Like all EPCOS thyristor modules, the TSM-LC-N690 operates silently and is wear- and maintenance-free, with a short switching time of only 5 milliseconds (ms).

The EPCOS TSM-LC-N690 thyristor module can be triggered by EPCOS’ dynamic power factor controllers, programmable logic controllers (PLC), or directly from the processor. It is suited for dynamic PFC applications with presses, welding machines, elevators, cranes and wind turbines.

TDK is a leading electronics company established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK’s portfolio today includes electronic components, modules and systems marketed under the product brands TDK and EPCOS. The company also manufactures power supplies, magnetic application products, energy devices, and flash memory application devices.

TDK’s EPCOS division, based in Munich, Germany, offers capacitors, ceramic components, EMC filters, inductors, non-linear resistors, RF modules, surface acoustic wave components, surge arresters and ferrites.

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.