Power on Your PCB

게시자

Most of the basic rules of thumb for printed circuit board layout are aimed at high-density, high-frequency boards. While keeping trace angles under 45 degrees and minimizing board size are good things to keep in mind, there are higher priorities when it comes to high power board design.

Spread Out

There will always be components that generate more heat than others on your board. The best thing you can do for heat dissipation is to get those components as far away from each other as possible. On an LED board, all the LEDs will be generating heat and should be as evenly dispersed as possible. On a power conversion board the culprits may not be so obvious. The main switching component in a power supply is often at risk for overheating and any components that are in line with the main current flow should be distanced at least somewhat from the main switcher. These components should already be selected and rated to high wattages, so they should be fairly obvious. Typically, a designer needs to keep an eye on thermals for the main IC, any external FETs, and any high-current inductors. These are often very close together in the schematic, but should be given room to breathe on the PCB. Components tend to be rated to a maximum current or power dissipation given a minimum copper area beneath them, so check the datasheet if you are worried your parts are too close. If you are creating a double sided board, keep in mind that the distance should be regarded 3-dimensionally. Putting the IC and FET back to back on a double layer board isn’t doing you any favors.  

Go Deep and Wide

Copper has a very low resistance, but it isn’t perfect. If large amounts of current are moving around on your board, you need to calculate trace resistance both to manage any thermal effects and predict any voltage drops from one end of a trace to the other. There are numerous online calculators that can help you out, or you can do the math yourself. A 1oz copper trace has a height of 1.4mils, which means you can see a huge performance jump just by moving to 2oz copper. This upgrade is far from free, but may make the difference between a functional board and a molten mess in extreme cases. Once you have gone as deep as you can, go wide. Special consideration needs to be given to internal traces in a 4+ layer board, as they cannot dissipate heat into the air. They should generally be twice as wide as an external trace carrying the same current. Copper pours are great for distributing heat evenly through a board, but exposed copper and external heat sinks are key for actually removing that heat from a board. If you use pours to carry large amounts of current, watch closely for any choke points that may limit your thermal efficiency. Current choke points tend to show up where a pour shrinks to fit between two mounting holes or around the edge of a component.  Current can only flow throughout your board as well as it can through the narrowest point.

Punch Air Holes

Many high power chips, especially those with an internal FET, have a large pad on the bottom that aids in heat dissipation. At a minimum, these pads should be in contact with an equally large and exposed copper pad on the PCB. If you have room, thermal vias are a great way to draw heat away from the chip. Thermal vias are smaller than normal current-conducting vias, using an 8mil to 10mil diameter drill bit. The vias are arranged in a grid such that their annular rings are touching and no soldermask is between them. Soldermask should also be removed on the back side of the via array to give the copper direct access to air. The amount of heat that can be dissipated into the air is directly related to how much surface area is available for dissipation, so thermal vias are literally piping the heat to the outside of the board rather than dumping heat into a copper plane isolated by soldermask.     

With these three design priorities in mind, you can make sure your build stays high-functioning and stable when under high-power operating conditions. 


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.