Molex Microminiature Connector Solutions

Previously and most commonly used in consumer handheld devices, microminiature connectors are now increasingly used in devices across a variety of applications, including household appliances, surgical equipment, home security devices, vehicle infotainment systems and more. Discover the trends that are increasing the use of microminiature connectors across multiple industries and learn more about Molex’s super-fine pitch and small-size Easy-On FFC FPC connectors.

Good things come in small packages

More innovative device features become available as IoT evolves. This evolution has also created an opportunity for increased modularity and an increased demand for flexible printed assemblies for the new features. 

Microminiature connectors were originally created for handheld devices in the consumer market and are now increasingly designed into devices across a variety of industries. But why are applications across industries using more microminiature connectors? To answer that question, it’s important to examine the following three reasons.

Intuitive user interface

A transformation in user interface design goes hand-in-hand with the advances of technology and innovative smartware. The evolution of user interfaces (UI) is now changing the way we work, shop, drive and communicate. This increased UI interaction has created an opportunity for microminiature connectors to be designed into devices such as cooking appliances, surgical equipment, home security devices, vehicle infotainment systems and more.

A great example of this can be found in the growing Connected Vehicle market. Automobile designers are striving to offer the optimal in-vehicle experience for drivers and passengers alike. As interior LCD panels become a standard in steering wheels, center consoles, and seats, new opportunities arise for designing with Molex’s Easy-On FFC/FPC portfolio. Featuring a variety of options, the Easy-On family offers superior connectivity for these applications.

Feature-rich options

The time we spend using mobile devices is growing each year, as new capabilities are developed and released to the industry. As our devices become more important in our daily lives, manufacturers are constantly competing to provide the most desirable features. Consumers are searching for the lowest profile devices, with the largest screen size and highest resolution.

Increased UI and feature-rich options can result in an increased requirement for flexible printed assemblies and modular design. For example, features such as touch screen, touch buttons and displays are all key microminiature connection points requiring flex assemblies.

The requirement for new and exciting features is present regardless of design parameters, and Molex FFC FPC super-fine pitch products provide a solution with an offering that ranges from just 0.20mm pitch.

Profile changes

As the development of applications for smaller and higher performing technologies increases, the demand for the products to meet these requirements is growing. This can sometimes mean that higher performance in a smaller space is demanded for products including micro wire-to-board, FFC/FPC and memory card connectors.

The mobile device market has evolved from the sliding form factor introduced in the 90s - consumers are now searching for streamlined devices with decreased profiles.  With phones getting thinner, the products in them need to be even thinner. Molex’s Easy-On family offers low profiles of 0.75mm to satisfy this need.

Molex Easy-On FFC FPC Connectors

Molex is on the frontline, innovating microminiature components for customers and engineers who need space savings, high-density signals and durability in connector designs.

The Easy-On FFC FPC range offers super-fine pitch and small-size FFC/FPC connectors in many circuit sizes to offer superior reliability and speedy data rates. Offering 0.20 to 2.00mm pitches, Easy-On connectors are ideal for tight-packaging applications. They also deliver features such as positive locks and a dual-contact design that ensures a reliable connection.

Additionally, a secure connection between the FFC/FPC connectors and terminals is established through a wide variety of actuator options including ZIF, slider, and flip.

As the evolving market demands smaller more reliable connections, Molex is continually developing lower-profile and higher-density interconnects to meet these needs.

EXPLORE MORE MOLEX PRODUCTS

관련 상품 참조

0541324033

Molex Connector FFC-FPC 보기

관련 상품 참조

2005290170

Molex Connector FFC-FPC 보기

관련 상품 참조

51296-1894

Molex Connector FFC-FPC 보기

관련 상품 참조

2005280070

Molex Connector FFC-FPC 보기

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.