Mesh networking for smart buildings and industrial IoT

Get a better understanding of how onsemi’s RSL10 Mesh Platform enables manufacturers to intuitively realize mesh networking applications by experiencing and developing different real-world use cases. This innovative solution also allows developers to customize their application with source code provided inside the RSL10 Integrated Development Environment (IDE) or any within a Bluetooth SIG-compliant RSL10 Mesh Package.

Unlike traditional point-to-point (P2P) Bluetooth connections, Bluetooth® Low Energy mesh networks implement a many-to-many topology and use managed flooding to send data. As a result, these networks don’t require centralized routing or routing tables like Ethernet networks. Bluetooth Low Energy Mesh specifications also offer built-in security with encryption at multiple layers, so nodes can relay traffic while potential eavesdroppers on the network only see encrypted packets. A properly placed Bluetooth Low Energy Mesh network can span larger distances than traditional P2P Bluetooth communications as nodes can perform message passing by relaying packets to a destination node that is out of range of the transmitting node. This enables a variety of IoT applications, including connected lighting and remote sensor monitoring, previously out of range for Bluetooth technology.

The RSL10 Mesh Platform

The RSL10 Mesh Platform is a versatile, easy to configure kit for developing mesh networking applications based on the RSL10 Bluetooth 5 radio. The platform includes two RSL10-based Mesh Nodes and a Strata Gateway, which enables connectivity to the Strata Developer Studio™ and acts as the network provisioner so that nodes can be securely added and removed.

Alongside the RSL10 System-in-Package (RSL10 SIP), the Mesh Nodes feature multiple environmental sensors for monitoring temperature and ambient light and magnetic field detection. The nodes also include a 2.3 kHz tone indicator, a connector for vibration buzzers and light dimming and alarm capabilities.

The Strata Gateway supports seamless and secure connectivity to the Strata Developer Studio™. This cloud-connected software enables provisioning of additional mesh networks and firmware-over-the-air (FOTA) updates. Using the virtual workspaces for common mesh networking examples, including a smart office and smart home, developers can access sensor data and trigger settings like signal strength, ambient light, battery, temperature and node connections for every node within the network in the Strata basic view. An advanced view allows the user to view several code examples.

The RSL10 Mesh Platform enables manufacturers to realize mesh networking applications in an intuitive way by allowing them to experience and develop different real-world use cases before digging deeper into the advanced examples.

Developers can also customize their own application using the source code for the RSL10 Mesh Platform provided inside the RSL10 Integrated Development Environment (IDE) or any of the examples available in the Bluetooth SIG-compliant RSL10 Mesh Package.

Also provided is the RSL10 Mesh app, available on GooglePlay™. The Mesh app acts as a provisioner to easily deploy new RSL10-based devices in a mesh network and allows control of individual nodes or groups of nodes using Generic OnOff and Light Lightness models.


Learn More from onsemi


관련 상품 참조

관련 상품 참조

관련 상품 참조

관련 상품 참조

관련 상품 참조

관련 상품 참조

관련 상품 참조

관련 상품 참조


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.