Learn about connector termination styles from Amphenol

As devices continue to get more sophisticated, the connection quality of peripherals and other components to the main PCB must evolve. In this article, explore 4 core types of PCB connectors available from Amphenol, including ideal applications, termination type, and more.

There are multiple factors design engineers take into consideration when choosing a connector. This can vary from performance factors like speed and signal integrity to form factors like size and shape. Among the basics of connectors, it is essential to determine what termination method is to be chosen. Most applications require a particular type of termination to match design requirements.

Through-Hole Termination (THT)
Though-hole terminations were very common in the early days, where the connector contacts or leads pass through a hole in the PCB. Through-hole components are best used for high-reliability products that require stronger connections between the PCB layers. Many of Amphenol’s connectors, such as Minitek®, Dubox®, Bergstak®, PV®, Quickie®, BergStik®, and EconoStik™, are offered with through-hole termination.

Surface Mount Termination (SMT)
With this technology, the connectors are mounted directly on top of the PCB. The connectors are either soldered manually in place or a reflow/wave soldering method is used to hold them in place. Some of the board/card edge connector types also come with surface mount terminations. Amphenol ICC offers various products in this mounting style, including Minitek®, Dubox®, Bergstak®, Quickie®, BergStik®, EconoStik™, Rib-Cage®, Conan®, Minitek® MicroSpeed, Griplet®, and Cross-Mate™.

Pin-in-Paste (PiP) Termination
Pin-in-Paste technology, also known as Through-Hole-Reflow technology is a reflow soldering process done with the help of automated machinery, eliminating hand and wave soldering processes. The connectors are loosely held onto the board holes and placed under an assembly machine, which in turn reflows the liquified solder under high temperatures over the board. Due to capillary action, the melted paste sucks the solder onto the board and into the hole, forming a permanent bond between the solder, paste, and connector lead. Amphenol products using PIP connection include Minitek®, Quickie®, BergStik®, DIN 41612 High-Temperature Backplane Connectors, Boltrack™, Modular Jack, OCTIS™ Outdoor, D-sub, and VerIO™ I/O connectors.

Press-fit Termination
Press-fit termination is generally a solderless termination, which helps to reduce the overall cost of the application. These types of connectors are often recommended with specific tooling, and required by the manufacturer to ensure an even insertion and full seating of the item. Amphenol offers Quickie®, BergStik® from wire-to-board and board to board, Metral®, Millipacs®, DIN, HPC from backplane, High-Speed Backplane Connectors like AirMax®, ExaMAX®, ExaMEZZ®, and Paladin®, and Delta-D D-sub Connectors with press-fit termination. Also, most of Amphenol’s power products can be configured with press-fit terminations, including the PwrBlade®series, PwrMAX® series, and EnergyEdge™ card edge series of connectors.


Featured Parts

관련 상품 참조

10147073-2600RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기

관련 상품 참조

10146153-2600RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기

관련 상품 참조

10147075-2600RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기

관련 상품 참조

10150097-3200RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기

관련 상품 참조

10150098-3200RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기

관련 상품 참조

10150095-3200RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기

관련 상품 참조

10150096-3200RLF

Amphenol Communications Solutions Connector Headers and PCB Receptacles 보기


관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.