Introduction to Circular Connector Terminology

Circular connectors are esteemed for their durability and robustness, allowing them to be used in the harshest of industries. Whether they are at work in industrial automation systems, aircraft controls, or commercial lighting, circular connectors reign supreme for their versatility.

Even though they are familiar in industrial settings, circular connectors come in many different variations and types, which can make them confusing and complicated to apply in a design. We'll cover the basics of circular connector terminology to make designing with circular connectors easy. 

Circular Connector Components & Features

  1. Number of Connector Contacts: Contacts are the most crucial part of the connector, as they connect the conductive material in the plug. This plug carries a signal or power to the mating conductive material in the socket. The number of contacts in a circular connector is often dictated by the number of IO that the connector needs to transfer. For example, a circular connector that supplies an RGB signal to an LED will have four contacts for the red, green, blue, and ground IO.
  2. Number of Connector Ports: Think of circular connector ports as how many circles make up the connector. Therefore, most circular connectors only have one port. However, some circular connectors can "split" signals to multiple other ports, which requires using multiple circular sockets for a single plug manifold. For example, this Molex connector has one inlet port and ten outlet ports.  This number of port configurations is notated as "1/10."
  3. Termination Method: The termination method describes how a signal-carrying wire terminates into the connector. One prevalent termination method is crimp terminations, but specific connectors require specific crimps and crimping tools, so check for product compatibility on your connector's datasheet.
  4. Connector Design: Body Orientation: A connector's physical geometry is crucial in physically constrained systems. For example, a television's wall plug is often oriented to lay flat against the wall, since televisions are frequently placed on stands that lay close to the wall, reducing room for wires and plugs. The body orientation of circular connectors allows for flexibility in similar situations and tight spaces.
  5. Contact Gender: One often-confusing point when selecting a circular connect is choosing the correct contact gender. The contact gender is only the gender of the contact, not the connector itself. For example, a standard "barrel jack" connector system may look like male contacts while they are, in fact, female contact genders.
  6. Current and Voltage Ratings: The current and voltage ratings of a connector are dictated by the size and geometry of the conductive materials. When selecting circular connectors, choose a higher voltage and current-rated connector than your application requires, as an overdesigned connector may provide more arc protection or lower impedance.
  7. Temperature Rating: As the name suggests, a connector's temperature rating dictates its recommended operating temperature conditions. In applications that require specific qualifications, such as MIL-spec or automotive temperature ranges, these temperature ranges may be well beyond what the connector could see. For example, the MIL-spec circular connector from Amphenol features a temperature range from -60C to 200C.

To shop all circular connectors from top manufacturers, shop Arrow.com.

관련 상품 참조

D38999/20WH21PD-LC

Amphenol Connector Circular 보기

관련 뉴스 기사

최신 뉴스

Sorry, your filter selection returned no results.

개인정보 보호정책이 업데이트되었습니다. 잠시 시간을 내어 변경사항을 검토하시기 바랍니다. 동의를 클릭하면 Arrow Electronics 개인정보 보호정책 및 이용 조건에 동의하는 것입니다.

당사의 웹사이트에서는 사용자의 경험 향상과 사이트 개선을 위해 사용자의 기기에 쿠키를 저장합니다. 당사에서 사용하는 쿠키 및 쿠키 비활성화 방법에 대해 자세히 알아보십시오. 쿠키와 추적 기술은 마케팅 목적으로 사용될 수 있습니다. '동의'를 클릭하면 기기에 쿠키를 배치하고 추적 기술을 사용하는 데 동의하는 것입니다. 쿠키 및 추적 기술을 해제하는 방법에 대한 자세한 내용과 지침을 알아보려면 아래의 '자세히 알아보기'를 클릭하십시오. 쿠키 및 추적 기술 수락은 사용자의 자발적 선택이지만, 웹사이트가 제대로 작동하지 않을 수 있으며 사용자와 관련이 적은 광고가 표시될 수 있습니다. Arrow는 사용자의 개인정보를 존중합니다. 여기에서 당사의 개인정보 보호정책을 읽을 수 있습니다.